Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Modular Farm Blog: Post 5 - Artificial LED Lighting System
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
  • Author Author: jmbranco76
  • Date Created: 2 Sep 2015 5:53 PM Date Created
  • Views 3179 views
  • Likes 7 likes
  • Comments 17 comments
  • modular_farm
  • grow_light
  • hydroponic
  • net_zero_energy_farming
  • growsharp
Related
Recommended

Modular Farm Blog: Post 5 - Artificial LED Lighting System

jmbranco76
jmbranco76
2 Sep 2015

Hi vertical farmers,

 

In the previous post we presented the key issues of our nutrient doser prototype and showed our magnetic liquid level detector. We are still waiting for the delivery of solenoid valves to complete that prototype.

In this post we will talk about our controllable grow lights tailored to plant needs.

 

Grow Light System

Besides warmth, water and nutrients the light is a key factor for plant growth.

To control this parameter we built an artificial lighting system based on high-power state of the art LEDs able to supplement daylight to plants and control their photoperiod.

An overview of the architecture is shown on the next image:

image

Figure 1. Artificial LED lighting luminaire for plant growth.

 

The built system and design criteria will be detailed during this post.

 

LEDs

We are using LEDs from OSRAM tailored for the plant needs in the wavelengths of deep blue, hyper red and far-red as seen on figure 2.

image

Figure 2. Spectral Power Distribution of plant photoreceptors and LED emissions.

 

Those wavelengths match the peak sensitivity of several photoreceptors in plants (chlorophylls and phytochromes) responsible for the photosynthesis and plant growth control.

The key characteristics of the used LEDs are shown on the next image (extracted from Osram’s LEDs for horticultural lighting brochure):

image

Figure 3. LED characteristics.

 

The LEDs are driven at a constant current of 350 mA and are serialized to share the same current. We use 5 LEDs in series per string attached to a controllable LED driver.

 

Plants are sensitive to different aspects of light namely its spectrum, its intensity and its daylight duration (photoperiod). The proposed system tackles all those variants. The spectrum can be tuned by changing the ratio between blue and red LEDs, while the light intensity can be adjusted by dimming the LEDs and the photoperiod (day/night) can be controlled by switching on and off the light.

We will start with a consensual ratio of 2/3 of red and 1/3 of blue that can be adapted based on the growing experiments or specific requirements of different plants.

 

LED PCBs

The LEDs are assembled in a proper double-sided plated-through PCB with 0.8 mm thickness. Thermal paste is used between the PCB and the heat sink to reduce even further the thermal resistance. An 1% NTC resistor is assembled on the PCB to monitor the temperature.

The example of an assembled PCB can be seen on the following image:

image

Figure 4. LEDs assembled on the PCB.

 

The assembled lit luminaire at 2% dimming is shown on the following picture:

image

Figure 5. Assembled LED luminaire.

 

Driver

We are building the driver around the TPS61500 from Texas Instruments, a boost converter for high brightness LEDs with multiple dimming methods. We will be using a PWM signal to control each LED string. With PWM dimming method LED brightness is controlled by the nominal settled current and the duty cycle of the external PWM signal. This method offer the best color consistency keeping the LED tuned at the correct wavelength.

Our system is supplied by a lithium-ion battery with 4 cells and a voltage ranging from 11.2 V (empty) to 14.6 V (full). The TPS61500 has a wide input range (3-18 V) that makes it suitable for our application. It features as well a high efficiency, programmable overvoltage and open LED protections, with a built-in 3 A, 40 V internal power switch.

We built the complete circuitry following the manufacturer's recommendations and design guides using the Multilayer Ceramic Chip Capacitors (MLCC) and the power inductors supplied by the challenge sponsor Würth Elektronik.

The circuit schematics of the built LED driver can be seen on the following image:

image

Figure 6. LED driver circuit schematic.

 

The PCBs were routed on KiCad, produced at home and hand soldered.

A complete functional driver is shown on the next picture:

image

Figure 7. LED driver assembled PCB.

 

We used the following Würth Elektronik components from the supplied kits:

ReferenceValueKit Part NumberKit
C1,C21uF, 50VX7R1206105K050WCAP-CSGP MLCC 1206
C7,C84.7uF, 50VX7R1206475K050WCAP-CSGP MLCC 1206
L110uH74438336100WE - MAPI

 

We measured 12 V, 0.50 A at input and 15.76 V, 0.36 A at the output with 5 red LEDs what gives a nice LED driver efficiency of 94.5% at nominal condition.

We measured also a good PWM dimming linearity from 2% to 100% using a 5 V square wave with a frequency of 200 Hz as PWM input signal.

To reduce the number of drivers we will adapt the final driver version to supply 10 LEDs in series. This will require minor changes on the components values and ratings.

 

Luminaire Mounting

Due to the limited height of 40 cm between layers and the reduced opening angle of the LEDs (80 degrees) a light gradient is visible on the growing pipes as shown on the following image:

image

Figure 7. Light Effect of the luminaire assembled on the hydroponic setup.

 

To improve the light homogeneity, increase the photosynthetic active radiation and reduce the effect of shading when the plants grow we will use 2 luminaires per layer spaced by 60 cm.

We will probably use some reflective materials to keep the light contained in the hydroponic setup footprint avoiding light pollution to the surroundings.

 

On the next week we will be describing our image acquisition system to monitor and control plant growth and introduce our database that will store all the valuable collected information.

 

And that's it for now. If you have any questions or comments please feel free to reply to this post.

 

Thanks for following and keep connected!

  • Sign in to reply

Top Comments

  • sleuz
    sleuz over 11 years ago +3
    Hey José Very informative post. We also have coloured high power ceramic LEDs in our portfolio. WL-SMDC Ceramic mono-color High Power LED waterclear - Product Catalog LEDs You may also check out our LED…
  • jmbranco76
    jmbranco76 over 11 years ago in reply to RWReynolds +2
    Hi Rick, I think the plants will be happy with your light setup . Dimming can be useful if you use the Leds to supplement day light with a certain photon flux. When there is enough daylight the Leds will…
  • shabaz
    shabaz over 11 years ago +1
    Thank you for the very detailed post - excellent information!! Your project looks fantastic.
Parents
  • RWReynolds
    RWReynolds over 11 years ago

    Great blog post Jose!

     

    I'm learning a lot from your team. Are you using any of the Wurth LEDs. I have purchased a number of Red/Blue LED grow bars. But I had planned on creating additional lighting using the Wurth Re/Blue LEDs.

     

    Your spectral power distribution chart is great. Now I will have to go back after the fact and see how my lighting stacks up. image

     

    Great looking system folks!

     

    Cheers,

    Rick

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jmbranco76
    jmbranco76 over 11 years ago in reply to RWReynolds

    Hi Rick,

     

    Thanks. I didn´t consider to use the LEDs supplied in the kit as they are Low-Power LEDs  intended mainly for backlighting or as LED indicators. Also the standard wavelengths are not optimized to the absorption peaks of most of the plants (there could be exceptions;)). This means you would need hundreds of those LEDs to reach the same radiant power and this power would be less effectively absorbed by the plants.

     

    I considered 1W to 3W LEDs from suppliers like Lumileds, Osram or Edison that have the most efficient wavelengths for plant growing like deep blue, hyper red or far red. But I will probably give it a try to the High-Power LEDs from Wurth presented by Simon.

     

    Cheers,

    José

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to jmbranco76

    Thanks for the great info Jose. It made me go back and re-examine my lighting choices.

     

    I think the main LED arrays I purchased will be sufficient @ a total output of 100W for the entire array. Each 2.5m strip is made up of 27 red and 9 blue LEDs at a total power output of 10W. I have 10 strips of these that I will arrange for the best coverage. They are marketed specifically as grow lighting, but I can't say I looked so closely at the specific spectral output of the lights until I read your last blog post. I now know that they provide wavelengths of 660nm (red) and 445nm (blue) light. It looks like I have the deep blue (445nm) and hyper red (660nm) covered. In looking through the LEDs provided in the kit I can see that far red is not provided. Possibly I can get some far red (730nm) samples from Wurth and have the spectrum covered.

     

    The LED arrays I have are not dimmable and will run from a simple 12V supply. What is the benefit of the lights being dimmable?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • RWReynolds
    RWReynolds over 11 years ago in reply to jmbranco76

    Thanks for the great info Jose. It made me go back and re-examine my lighting choices.

     

    I think the main LED arrays I purchased will be sufficient @ a total output of 100W for the entire array. Each 2.5m strip is made up of 27 red and 9 blue LEDs at a total power output of 10W. I have 10 strips of these that I will arrange for the best coverage. They are marketed specifically as grow lighting, but I can't say I looked so closely at the specific spectral output of the lights until I read your last blog post. I now know that they provide wavelengths of 660nm (red) and 445nm (blue) light. It looks like I have the deep blue (445nm) and hyper red (660nm) covered. In looking through the LEDs provided in the kit I can see that far red is not provided. Possibly I can get some far red (730nm) samples from Wurth and have the spectrum covered.

     

    The LED arrays I have are not dimmable and will run from a simple 12V supply. What is the benefit of the lights being dimmable?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jmbranco76
    jmbranco76 over 11 years ago in reply to RWReynolds

    Hi Rick,

    I think the plants will be happy with your light setup Relaxed.

    Dimming can be useful if you use the Leds to supplement day light with  a certain photon flux. When there is enough daylight the Leds will be almost off allowing some energy savings.

    Also some plants need only a small amount of light after sunny hours to increase the photoperiod and avoid dormancy. For this purpose you can also dim the light to the required plant light levels.

    Cheers,

    José

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to jmbranco76

    Thanks again for the info Jose.

     

    I will be using some natural light so the reduced artificial light may be significant.