• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Morning update :)
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
  • Author Author: sftwrngnr
  • Date Created: 19 Sep 2015 2:25 PM Date Created
  • Views 556 views
  • Likes 1 like
  • Comments 2 comments
  • ambient_growth
Related
Recommended

Morning update :)

sftwrngnr
sftwrngnr
19 Sep 2015

Wow! A lot can change when a small-scale prototype fails.image My daughter's rather whimsical design idea for configuring the vertical farm, and having a pump run off of gravity and rotation of the growing system was a non-starter after trying to just get part of it assembled.  So... scrapping that, and going with a much simpler design. The growing system will be a "stair-stepped" series of PVC pipes with conventional top fed hydroponics.  However... I hate the idea of using power on the recirculation of the nutrients.  So, I'm going to build a small hydraulic ram pump today. I believe I can capture the waste water that normally would just spill off, and feed it through a "Wye" connector, and use the venturi effect to be able to effectively siphon the water (in my case the nutrients) that would normally be discarded.  If this works as I think it will, the recirculation of the nutrients will occur without any electrical power used, other than to periodically open the valve for releasing the nutrients.

 

If that doesn't work, I'll go with an "air-lift" pumping system, using a low voltage (12V), low wattage air pump so that the solution can be aerated at the same time that it is being recirculated.

 

With all that said, I'm going to have a cigar, feed my horses and then head off to Home Depot to get more PVC pipe, a couple of check valves and see if I can't make this work image.

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    Love the way you go for as less energy-consumption as possible!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Yes, sometimes early designs soon prove themselves not appropriate for implementation.

     

    Luckily the design process gives you plenty of alternative ideas to consider when you are faced with needing to change a few things.

     

    DAB