• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog New growing surface
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
  • Author Author: ochikov
  • Date Created: 4 Sep 2015 2:17 PM Date Created
  • Views 1388 views
  • Likes 6 likes
  • Comments 9 comments
Related
Recommended

New growing surface

ochikov
ochikov
4 Sep 2015

Hello Everybody,

Yesterday I just finished my conception for new growing surface. I'm not very good carpenter and I live in a city that is hard to find wooden material. That's why I use my imagination. You can see the pictures bellow. This is just the first phase of my project. The difficult phases are to make the whole process of growing plants - automated. More information will be provided soon!

 

imageimageimageimage

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 11 years ago in reply to ochikov +2
    About this problem, I have almost all the walls of my home the same, so I was worrying about how it was possible that the entire kitchen and the 70litres hot water tank was on the wall. Then a friend that…
  • ochikov
    ochikov over 11 years ago in reply to RWReynolds +1
    Hello! Thank you! First I want to try it without mounting on the wall. The reason is that my light source is from another direction. This week I will mount LED light emitted about 6000K. Then I will try…
Parents
  • RWReynolds
    RWReynolds over 11 years ago

    Great repurpose of a shipping pallet Ognyan. Are you going to mount this on a wall? I can see many of these mounted on the wall, taking up very little space and producing a lot of food.

     

    Great work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ochikov
    ochikov over 11 years ago in reply to RWReynolds

    Hello! Thank you! First I want to try it without mounting on the wall. The reason is that my light source is from another direction. This week I will mount LED light emitted about 6000K. Then I will try to mount it. Here there is another problem. It is a little bit heavy and the wall is made of isolation materials, not a concrete. I don't know how to deal with it. But as soon as I have new information I will post it.

     

    image

    Thank you!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to ochikov

    About this problem, I have almost all the walls of my home the same, so I was worrying about how it was possible that the entire kitchen and the 70litres hot water tank was on the wall. Then a friend that makes this kind of installations explained me that there are special Fisher wall plugs (or other brands I think) special for this kind of walls that has to be placed and glued with a special polymer. After about 15 minutes you can put there almost everything.

     

    I have no idea what is the correct name in English, but try to search "tasselli per cartongesso" in google.com and you see something like the following image. Hope this is helpful.

     

    Enrico

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to ochikov

    About this problem, I have almost all the walls of my home the same, so I was worrying about how it was possible that the entire kitchen and the 70litres hot water tank was on the wall. Then a friend that makes this kind of installations explained me that there are special Fisher wall plugs (or other brands I think) special for this kind of walls that has to be placed and glued with a special polymer. After about 15 minutes you can put there almost everything.

     

    I have no idea what is the correct name in English, but try to search "tasselli per cartongesso" in google.com and you see something like the following image. Hope this is helpful.

     

    Enrico