Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog The Almost Completed Small Model's Fish Feeder and a few Updates
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
  • Author Author: e14 Contributor
  • Date Created: 4 Sep 2015 1:18 AM Date Created
  • Views 622 views
  • Likes 4 likes
  • Comments 4 comments
  • solar_farm
Related
Recommended

The Almost Completed Small Model's Fish Feeder and a few Updates

e14 Contributor
e14 Contributor
4 Sep 2015

Update on Big Project: Buying some bigger motors for making full-scale fish feeders(See Below), and probably ordering LEDs/the PH and Nitrogen Sensors/Solar Panels by next week.

So, I cleaned up the gravel for the 30 gallon water part, and in the end had to buy a timer outlet instead of making one with a relay due to electrical fire concerns for the water pump. It can pump over 100 gallons of water an hour, more than enough for a small 30 gallon model. I plan to finish it by the end of this week, and begin the biofilter and developing a bigger model, which I am looking for at the local rubbermaid trashcan store. (They can be bought at around 100-300 dollars). I was working on a previous Servo fish feeder design(a fish food bottle with a hole at the bottom and a servo connected to a cover that occassionally rotated, allowing a hole in the cover to match with the hole at the bottom of the can and stuff come out) , whose code I will show here. However, I had a few problems with spreading food throughout the model and  controlling the servo. So I decided to use a method similar to deer feeders, with a rotating plate using the centrifugal force to send the food pellets around the pool. Probably, I will be working on this for the rest of today and tommorrow and will try to have pictures and code uploaded with the completed product.

(Below is the old code that did not work this is in Arduino)

#include <Servo.h>

Servo myservo;

void setup()

{

  myservo.attach(9);

myservo.write(0);

  delay(500);

  Serial.begin(9600);

 

 

while (! Serial);

 

 

Serial.println("TIME");

}

/*************************************************/

void loop()

{ 

  if (Serial.available())

 

 

{ int time = Serial.parseInt();

 

 

if (time >=1000)

 

 

{

 

  myservo.write(90);//goes to 15 degrees

  delay(time);//wait for a second

 

  myservo.write(0);//back to 0 degrees

  delay(time);//wait for a second

}

}

}

/**************************************************/

  • Sign in to reply
Parents
  • m.ratcliffe
    m.ratcliffe over 10 years ago

    Got any Pictures/Video of the Feeder in action?

    I'm interested to see what you made.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • m.ratcliffe
    m.ratcliffe over 10 years ago

    Got any Pictures/Video of the Feeder in action?

    I'm interested to see what you made.