Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Vertical Hydroponics - Blog 8: Physical Wiring
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
  • Author Author: jamesod
  • Date Created: 16 Oct 2015 12:24 AM Date Created
  • Views 874 views
  • Likes 3 likes
  • Comments 2 comments
  • vertical_hydroponics
  • wiring
  • vertical_farming
Related
Recommended

Vertical Hydroponics - Blog 8: Physical Wiring

jamesod
jamesod
16 Oct 2015

I have most of the wiring completed for the controls of the system. The relays have been wired to outlets, and all of the sensors have been wired to an interface board. Here is my dirt cheap homemade woden control cabinet. It was the best I could do with the stuff I have laying and basically zero budget. It's not pretty, but it will work. The outside has all of the outlets that are connected to relays, plus a GFCI outlet that is always on. When the programming is complete, it will have the EZR32WG board mounted to it for a cheap HMI.

 

image

Here is the inside. It is complete except for the Adruino that will directly interface with the sensors and relays.

 

image

Next step will be to complete the Arduino code, wire it into the panel, and test the EZR32WG feeding commands to it via UART. 

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 10 years ago +1
    Looks pro
  • DAB
    DAB over 10 years ago +1
    Nice start and use of simple materials. DAB
Parents
  • DAB
    DAB over 10 years ago

    Nice start and use of simple materials.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 10 years ago

    Nice start and use of simple materials.

     

    DAB