Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Documents Vertical Farming Design Challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 29 May 2015 11:07 AM Date Created
  • Last Updated Last Updated: 15 Jun 2015 3:50 PM
  • Views 8982 views
  • Likes 11 likes
  • Comments 51 comments
Related
Recommended

Vertical Farming Design Challenge

image
Vertical Farming Design Challenge

image  All About Vertical Farming

image  Overview Video

image  Prizes

image  Terms and Conditions

image  Kit List

 

Background

 

From Wikipedia

According to current projections of population growth, the world population of humans will continue to grow until at least 2050, with the estimated population, based on current growth trends, to reach 9 billion in 2040,and some predictions putting the population in 2050 as high as 11 billion. World population passed the 7 billion mark on October 31, 2011.

 

From the World Wildlife Organization

Soil is the earth’s fragile skin that anchors all life on Earth. It is comprised of countless species that create a dynamic and complex ecosystem and is among the most precious resources to humans. Increased demand for agriculture commodities generates incentives to convert forests and grasslands to farm fields and pastures. The transition to agriculture from natural vegetation often cannot hold onto the soil and many of these plants, such as coffee, cotton, palm oil, soybean and wheat, can actually increase soil erosion beyond the soil’s ability to maintain itself.

Half of the topsoil on the planet has been lost in the last 150 years. In addition to erosion, soil quality is affected by other aspects of agriculture. These impacts include compaction, loss of soil structure, nutrient degradation, and soil salinity. These are very real and at times severe issues.

 

From VerticalFarm.com

By the year 2050, nearly 80% of the earth’s population will reside in urban centers. Applying the most conservative estimates to current demographic trends, the human population will increase by about 3 billion people during the interim. An estimated 109 hectares of new land (about 20% more land than is represented by the country of Brazil) will be needed to grow enough food to feed them, if traditional farming practices continue as they are practiced today. At present, throughout the world, over 80% of the land that is suitable for raising crops is in use (sources: FAO and NASA). Historically, some 15% of that has been laid waste by poor management practices. What can be done to avoid this impending disaster?”

 

The confluence of these observations and forecasts points to the need to increase our ability to grow fresh food in urban areas – closer to the populations that will consume them.  This means shifting from traditional outdoor gardens to indoor systems for food production.  Electronic Engineers are uniquely suited to provide systems based on a technology infrastructure that can lessen required energy consumption in production and improve the output of a smaller space.

 

Vertical Farming is a developing industry growing to meet these demands.  The main areas for measuring their success – and focus for improvement - are the production output per square foot, monitoring and lessening the energy and water consumption, and efficiencies around harvesting.

  

The Challenge

We will select 15 challengers from all entries received to build indoor, vertical farms that are true IoT solutions. The projects should include:

  • Environmental monitoring (light, temperature and humidity)
  • A watering and feeding system
  • A greater growing surface than just the overall footprint of the build
  • Energy monitoring to collect data on the overall consumption of power and water by the system


Help Along the Way

In addition to the great Kit that Challengers will receive, we also have support for those of you without a green thumb.  We’re going to be recommending the types of seeds to buy, the types of fertilizer and ranges to be aware of when you’re monitoring moisture, light and humidity.  We’ll announce a point in time about six weeks out when all Challengers should start their seedlings.  After a 7-10 day germination period, your seedlings should be transferred to your Vertical Farm.  Then after about a month of growing we’ll ask you to harvest your crop.  Submitting information about the overall weight of the harvest and the average height of the plants will help the Judges determine the best developed solutions.

And if your seedlings start looking sickly, then post a question on the Design Challenge site and someone from the Vertical Farming Association will give you tips and suggestions to help you nurse your plants back to life.

 

More details coming soon.

  • vertical
  • vertical_farming
  • Design
  • challenge
  • farming
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +3
    Questions are a good thing! They inspire thought and conversation. Never be sorry you asked a question, and never feel stupid for asking a question that is considered 'basic'. I ask basic questions all…
  • jkutzsch
    jkutzsch over 10 years ago in reply to shabaz +3
    I will definitely have to check those groups out, I went through last night and just started following a variety of interesting groups but was noticing a bunch have not been updated in years. :-) The specifics…
  • mcb1
    mcb1 over 11 years ago in reply to clem57 +2
    clem57 Clem Yes it did strike me that in very hot climates it could be an issue with water transvapouration putting them at a disadvantage. Even her in summer we lose 4-5mm per day, which many won't realise…
  • jkutzsch
    jkutzsch over 10 years ago in reply to shabaz

    I will definitely have to check those groups out, I went through last night and just started following a variety of interesting groups but was noticing a bunch have not been updated in years.  :-)

     

    The specifics of IoT and farming is very intriguing from what I have seen of some of these challengers some pretty cool ideas were looked into!  Makes you wonder if a new group for IoT Farming might not get some interest.  Especially with some of the cool information being applied to aquaponics and automated feeding/monitoring.

     

    I can imagine implementing many of the same frameworks across the board for chickens, rabbits, etc... all that are applicable for urban farming as well as larger rural implementations.

     

    Good stuff!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to jkutzsch

    Hi John,

     

    It was a great design challenge, wasn't it : )

    You possibly want to join (if you haven't already done so) the Internet of Things group, Single Board Computers and Industrial Automation and Power and Energy groups, this design challenge covered quite a few topics but a strong trend in the challenge entries was that ways were found of improving urban food growth through IoT. I think it is a unique resource on the topic - I've not seen so much on the Internet elsewhere in this subject area with such a software/hardware mix and urban farming ideas.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 10 years ago

    It is awesome Design Challenges such as this one that makes me wish I had come across Element 14 much earlier!

     

    I can't find any groups or other areas that would continue the discussion of Vertical Farming or similar that seems very promising with the assorted technology options available from E14.  Am I just missing them?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    So would a start and stop pump be better than a continuous one because the start/stop gives control but degrades the pump any suggestions?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to e14 Contributor

    This is the budget one part count:

     

    >20mm SDS auger bit [length isnt that important so long as it is longer than the pvc tee]          £4

    >20mm PVC inspection tee                                                                                                         £2

    >25MM WHITE PLASTIC SPACER BAR SADDLES FOR CONDUIT [4 units]                                         £2

    >Electric 2 Pin Connector DC12V 40-50mA 10RPM DC Geared                                                       £4

    >Flexiable coupling [4mmto 12] these are a hard to find and I had to make my own from a 4-6mm [recommend moving to a 919D 6mm motor and getting a 6-12mm coupling  [check sds is indeed 12mm, Im running from memory here]


    The key here is that everything is the correct size to not need major alignment or work, the fitting process is:

     

    >Secure Tee in vise and run the 20mm auger bit thru it by drill power [it isnt quite 20mm at some points]

    >Mount the tee in place on a suitable base plate [I used some wood]

    >connect the drill and motor with the coupling link

    >Push the drill into the pvc tee, and get it is aligned as possible before mounting the motor in the pvc saddles.

    >Test it turns as expected and is not misaligned. If it works remove the saddles and reapply with some decent glue.

    >Find a suitable hopper [a pop bottle should fit nicely].

    image

     

    I made a second one [for feeding chickens] with a 919D motor and mounting plate [20mm auger, 6- coupling] and it does increase the feed rate and look like a more professional job. I have never had a blockage in either of them, but that is using very small diameter food. I would recommend building a slightly larger version [25mm sds auger, 919d or similar motor, 25mm inspection tee, 32 mm clamps] but I cannot confirm all of these parts work together yet.

     

    After some reading it seems that fish like being fed regularly and the amount based on fish weight and water temperature, the micro controller feeds on the hour every hour during daylight, the amount a function of water temperature and it works ok for now.

     

    The Ph probe kit looks fancy, maybe I will invest in one after seeing your competition review of it. hopefully the competition judges will allow a late entry.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hello Michael,

     

    I would love to see your fish feeder project. I would like to add a fish-feeder to this set-up and you could save me some time with a proven design. As far as measuring PH, yes I will be measuring PH. I have an industrial PH meter that's meant to be submerged and operated, I think, 100% duty-cycle. PH can be tricky, and expensive. Sparkfun has a PH kit for $130 that includes a sensor, interface PCB, and calibration solution. Remember that PH, as well as other measurements, are temperature dependent. The sparkfun kit has a temp comp method.

     

    As far as my set-up. I need to dive into the data sheet for this PH sensor and check the protocol.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to e14 Contributor

    Nicholas,

    I like the look of your setup, do you plan on automating all of the system. I am working on something similar but am unsure if i should automate the PH adjustment and lost compleetly on the addition of iron [It seems wrong to add something without first measuring its deficiency].  I have the plans for a very cheap auger based automatic fish feeder if you want the plans let me know [it has been running flawlesley for 6 months now].

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor

    I would go for it seeing this setup.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sftwrngnr
    sftwrngnr over 11 years ago in reply to e14 Contributor

    Sweet setup!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    I missed the deadline to submit for this one. I had an accident with an angle grinder, im okay buy nearly cut my nose off. image anyway I have a team and all the electronics I need so Im going to do this challenge anyway. I don't care much about winning prizes, but I cant afford to buy new dev kits so I'll use another ARM core device, I have a few mbed platforms laying around and all the hobby stuff like arduino/Raspberry Pi, etc. Unless the officials will allow a late entry?

     

    Our teams goal is to create an off-grid aquaponic farm that will produce enough food for 2 people. Solar powered and rain collection. We will collect as much data as possible and use what we need for automation/monitor. Data will be uploaded to IoT and used accordingly. Alarms, control, monitor will also be available via blutooth, however simple, phone apps can be developed/expanded later.

     

    We have already built an outdoor version and mechanically it works great. Now it's time to add automation and control.

     

    image

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>