Imagine a World Without Cords
  • Challenges & Projects
  • Design Challenges
  • Imagine a World Without Cords
  • More
  • Cancel
Imagine a World Without Cords
Blog It's Alive! Part 009
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 22 Oct 2012 11:26 AM Date Created
  • Views 1259 views
  • Likes 3 likes
  • Comments 5 comments
  • public_wireless_charging
  • tildvavc
  • wireless_power_challenge
  • msp-exp430g2
  • members_featured_project
  • wp_challenge_one
  • wireless_power_consortium
Related
Recommended

It's Alive! Part 009

COMPACT
COMPACT
22 Oct 2012

Alternative Applications for Qi

I conducted a test of the Texas Instruments Transmitter Manager bq500210EVM-689bq500210EVM-689 and Receiver Evaluation Module bq51013AEVM-765bq51013AEVM-765 to check its viability of transmitting power through a Glass door.

 

This unedited video has little dialogue but it shows an MSP430 LaunchPadMSP430 LaunchPad being powered through a Glass Door.

Evidence of successful operation is demonstrated by the faint connection beep and the blinking LEDs on the MSP430 Launchpad.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I am really pleased with the result and now in a position do not have to drill any holes to;

  • power external and outdoor devices such as Christmas or Garden lights from inside
  • or use Outdoor Solar Panels to power and charge indoor devices.

 

Very useful. Very Very useful.

What do you think?

 

Learn more at http://www.element14.com/wireless-power-solution

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Hi all, actually this is the right time to share my experience....with my brother. He is a carpenter, specialized on furnitures. So he doesn't have any clue about electronics, for sure he doesn't know…
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi all,

     

    actually this is the right time to share my experience....with my brother. He is a carpenter, specialized on furnitures.

    So he doesn't have any clue about electronics, for sure he doesn't know what wireless power charging is.

    I love my brother, but i am sure, he would try to find the cable for WLAN if i would ask him to get one.

     

    But back to the topic, i told him about the WPC solutions and integrating a Qi-compatible charger into the desk or sideboard or all the other furnitures. And he did like the idea, even if he didn't understand what he needs from electronical point of view. I told him he'll get a black box with a cable coming out of it, which just needs to be plugged into the wall outlet. And now he can sell the furniture with an more added value.

    The end customer still only sees the wood from the top, but underneath is the coil which transmitts the power to the Rx side.

    Alignment could be done by a nice Qi-logo branded into the wood...or something similar.

     

    So, as we can see in Monte's video, all different materials can be put in between Tx and Rx side, as long as they are diamagnetic (µr equal to approx. 1). This could be any kind of plastic, wood, glas etc.

     

    I am looking forward to see more of your ideas you are coming up with. Wireless doesn't mean "transmission in air", it can be one of the above mentioned materials as well.

    What i need to try is transmitting the power between Tx and Rx having water in between. Maybe a water pump which is installed into a acquarium?!

     

    Oliver

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lfa555
    lfa555 over 13 years ago

    hey Monte, the approach is really genius! I could think of a number of devices and things which could be powered nicely through the window! Go Monte!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 13 years ago

    I like it.

     

    I have been looking for a way to set up a digital camera on the outside of my windows and use either an RF or IR link to trigger the camera for monitoring my birdfeeder and get closeup pictures of the birds feeding.

     

    I could use your approach without having to modify the window or move the bird feeder.

    I could also use this approach to power my lightning photography and thunder recorder without worrying about lightning induced power spikes.

     

    Thanks for a very good idea.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 13 years ago

    Hey Monte, great idea!

    A friend of mine already mentioned his idea to me to make a wireless LED lamp (5W is enough) to be easily replaceable.

    BTW, as an improvement to a Qi-2.0 standard: make it possible to send / receive information through the Qi power link!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ssilberhorn
    ssilberhorn over 13 years ago

    Great idea Monte!!!  MSP430-LaunchpadMSP430-Launchpad powered through glass....

     

    http://www.ti.com/ww/en/launchpad/graphics/byob_images/LaunchPad_Sticker.png

    Hey Monte...

    Build your own wireless power LaunchPad BoosterPack...

     

    How do I build a BoosterPack?

    Building a BoosterPack is easy! Simply follow the BoosterPack pinout/specifications provided in the links below. Each BoosterPack should include hardware design files, software & full documentation. BoosterPacks can be made to support all or some LaunchPad evaluation kits.

    • Learn how to Build Your Own BoosterPack!

     

     

    I designed my BoosterPack! Now what?

    Once your BoosterPack design is done, software is written & documentation is finalized, you can add your BoosterPack design to the BoosterPack wiki list! BoosterPacks that are orderable, listed on the wiki & popular can be promoted to the official www.ti.com/boosterpack page!

    • Add your BoosterPack to the unofficial BoosterPack wiki!

     

    Download Eagle Design Files...

     

    • BoosterPack Design Guide[1]
    • LaunchPad/BoosterPack eagle footprints