Imagine a World Without Cords
  • Challenges & Projects
  • Design Challenges
  • Imagine a World Without Cords
  • More
  • Cancel
Imagine a World Without Cords
Blog It's Alive! Part 016
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 23 Nov 2012 6:58 AM Date Created
  • Views 1167 views
  • Likes 2 likes
  • Comments 5 comments
  • wp_challenge_one
Related
Recommended

It's Alive! Part 016

COMPACT
COMPACT
23 Nov 2012

SMD Soldering Preparation

I've discussed some soldering techniques in previous articles and for this project I will be using manual "hand" assembly and rework for Surface Mount components.

To ensure consistent, reliable, reapeatable quality surface mount soldering and rework I researched a number of different methods and technologies;

  • Conduction
  • Convection
  • Radiation
  • Combinations of the above.

and products that employ these methods.

 

For any new prototype being developed components need to be added in an incremental and progressive manner with frequent testing.

This process is to ensure that each stage is working as desired prior to tackling the next.

This approach discounts the use of an oven where all components are soldered simultaneously. (i.e. Perfect for mass production but not suitable for prototype development.)

 

This project uses non-leaded components so contact conduction soldering alone is not enough. (James Bond?)

The main parts of the design are QFNs (Quad Flat No Leads) with a central thermal pad and a CSP (Chip Scale Package) with solder balls.

Just soldering around the perimeter of these parts does not address the central thermal which needs to be connected to the PCB for heatsinking, mounting and sometimes "grounding" purposes.

("Ground is a good place to grow carrots and potatoes")

CSPs have solder balls as contacts (just like a bga but only smaller) and all should be melted simultaneously to ensure it sinks down into position evenly and correctly.

 

Another consideration are plans to reworking the the prototype in case parts need to be replaced, removed or remounted.

With all these considerations in mind this limits the choice to controlled hot air convection, IR radiation or combination of both and some contact soldering.

I don't possess a suitable IR rework station so this limits my choice to controlled hot air convection.

 

In summary the my plans are;

 

Component TypeSolderingDesoldering
Through holeSoldering IronSoldering Iron or Hot Air
2 ended Chip componentsSoldering Iron, Soldering Iron Tweezers or Hot AirSoldering Iron, Soldering Iron Tweezers or Hot Air
Multi leaded componentsSoldering Iron or Hot AirSoldering Iron, Soldering Iron Tweezers or Hot Air
Non leaded ComponentsHot AirHot Air

 

"A good craftsman never blames his tools"

My response to that is "This is because craftsmen use high quality and perfectly honed tools.".

 

To remove the risk of TORCHING my new project I will be using equipment that will prevent that from happening.

For contact soldering I will use a high quality soldering Iron and tweezers that has its temperature set to as low as possible.

For convection soldering (Hot Air) I will use a Hot air rework station that has computer controlled temperature profiles.

 

"Always - Use flux paste! - I can't stress this more!"

Flux paste improves heat transfer.

 

Here a some photos of my Hot Air rework station and I removing a PLCC.

This is just a practice run on a very old board. No ESD protection measures were taken.

 

Apply flux paste to leads of the component to be removed (this also works for bgas - use specially formulated flux liquid instead)

  image

 

Install heat shield with helping vacuum hand.

The heat shield encapsulates the hot air within its boundaries preventing collateral damage.

  image

 

Click on tool button to run a preprogrammed temperature profile

(This particular temperature profile brings the entire component to an even heat at two different temperatures below the solder's melting point and then peaks quickly to raise the temperature to reflow for just a few seconds before cooling and shutting down.)

image

 

The programmed profile runs through its paces.

I like the way my machine has an animated display to tell me where it is in the process.

image

 

 

Just at the end of the temperature profile peak the component magically pops off the PCB by itself.

  image

 

No damage to the PCB or component at all (except some possible ESD damage because I didn't take the appropriate precautions for this practice run).

I just need to clean off the residual flux and remove and unwanted solder.

  image

 

Just nearing the end of the program and about to shut down.

image

 

Just so easy!

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 13 years ago

    Hey Monte,

     

    I'm using a Atten 858D+ hot air soldering station, which can be bought from ebay for <60 Euros, but I've used more luxureous hot air soldering solutions in the past at my job. Those 'cups' with spring loaded suction system are really useful, could you tell me which brand / type of soldering station you are using?

     

    Greetings,

    Victor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 13 years ago in reply to vsluiter

    Hey Victor

    I've just read an article about an Atten 858D+ not being wired correctly where Mains ACTIVE is connected to the exposed metal parts.

     

    Please have the unit checked and then double checked with a PAT (Portable Appliance Tester to ensure that it is safe.

     

    Regards

    Monte

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • COMPACT
    COMPACT over 13 years ago in reply to vsluiter

    Hey Victor

    I've just read an article about an Atten 858D+ not being wired correctly where Mains ACTIVE is connected to the exposed metal parts.

     

    Please have the unit checked and then double checked with a PAT (Portable Appliance Tester to ensure that it is safe.

     

    Regards

    Monte

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • vsluiter
    vsluiter over 13 years ago in reply to COMPACT

    Thanks for the tip, I'll check it!