Imagine a World Without Cords
  • Challenges & Projects
  • Design Challenges
  • Imagine a World Without Cords
  • More
  • Cancel
Imagine a World Without Cords
Blog OFFICIAL - Qi Lime Pi Rev 1 Completed and Entry with Schematics, Eagle files, Sketchup Files etc...
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: johnsocm
  • Date Created: 7 Dec 2012 3:57 AM Date Created
  • Views 1867 views
  • Likes 2 likes
  • Comments 4 comments
  • public_wireless_charging
  • wireless_power_home
  • wireless_communication
  • wireless_power_challenge
  • power_system
  • wireless_power_charging
  • qi_standard
  • wp_challenge_one
Related
Recommended

OFFICIAL - Qi Lime Pi Rev 1 Completed and Entry with Schematics, Eagle files, Sketchup Files etc...

johnsocm
johnsocm
7 Dec 2012

Hello World,

 

I have completed a sophisticated Highly Efficient Qi Lime Pi ProtoShield. The boards are on their way! The Qi Lime Pi is a Qi/Battery powered and prototyping shield for the Raspberry Pi.

 

Presenting the Qi Lime Pi..In Red, Green, Black and Moldy Purple!

imageimage

Front and Back:

imageimage

My Entry! A Qi Lime Pi - A Qi Powered Raspberry Pi Plate

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Qi Lime Pi Booting up!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Qi Lime Pi mounted on the Raspberry Pi powered via the transmitter and receiver coils!

Fullscreen contentimage_52235.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Voltage is a very good Regulated 5V!

Fullscreen contentimage_52236.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Qi Lime Pi Booting up off a Custom SD Card Image.

Fullscreen contentimage_52237.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

The battery charging circuit works as well but for my purposes I didn't need the battery charging circuit. I wanted the Raspberry Pi to shut off like a light switch when I pull it off the Qi Transmitter. With the battery the Qi Lime Pi keeps charging the battery until full and then powers the Raspberry Pi until the battery is dead when pulled off the transmitter.

 

This Qi Lime Pi shield has the following:

 

Full Evaluation Board Qi Receiver- Has a solder jumper to allow for either a Qi 5V pass through voltage or battery charging functions, comes with lots of test points!

Battery Charger with a GUI Using I2C-A complete charger module for charging compact, flexible, high efficiency, switch-mode charge management for single-cell, Li-ion and Li-polymer batteries.

GUI-Yes this has a GUI. You can download and look at it now right from TI.com! bq2427xEVM_SW_V0001.zip

IC Controlled NexFET Power MOSFET-The NexFET power MOSFET has been designed to minimize losses in power conversion load management applications. The SON 3x3 package offers excellent thermal performance for the size of the package! I had to custom make a SON-8 package for Eagle!

Low Input Voltage Synchronous Boost Converter with 1.3A Switches-More than 90% efficient, Automatic Transition between Boost Mode and Down Conversion Mode, Quiescent Current less than 55 uA. Operating Range from 0.3V to 5.5V, Output short circuit protection under all operating conditions, Power Save Mode, Overtemperature Protection.


I will say it again, It isn't just a battery charger, it is a complete High-Efficiency Switch Mode Charger with Separate Power Path Control!

 

What is Power Path Management,

-It allows the device to power the system from a high efficiency DC to DC converter while simultaneously and independently charging the battery. The charger monitors the battery current at all times and reduces the charge current when the system load requires current above the input current limit. This allows for proper charge termination and timer operation. The system voltage is regulated to the battery voltage and will not drop below 3.5V. This minimum system voltage support enables the system to run with a defective or absent battery pack and enables instant system turn on even with a totally discharged battery or no battery! Try that with your iPhones or Droids! The power path management architecture also permits the battery to supplement the system current requirements when the adapter cannot deliver the peak system currents. This enables the use of a smaller adapter.

 

-The battery is charged in three phases:

---conditioning, constant current, and constant voltage

The charger also offers the a voltage based battery pack thermistor monitoring input (TS) that monitors battery temperature for safe charging.

Here are the details if you want or just skip ahead:

-Instantly Startup the system from a deeply discharged battery or no battery

-Integrated FETs for up to 2.5A charge rate, even though I limited this rate to 1A

-Highly integrated Battery N-Channel MOSFET controller for Power Path Management

-Safe and accurate battery management functions

----0.5% Battery Regulation Accuracy

----10% Charge Current Accuracy

-Voltage based, NTC monitoring input (TS) for measuring the temperature of the battery, I also used a solder jumper for this option to be either enabled or disabled

-Thermal regulation protection for output current control

-Battery Short Circuit Protection

-Soft start feature to reduce inrush current

-Thermal shutdown and protection

-Battery charging status LEDs and signal LEDs

 

Best of all I included the connections for a USB kit from Ti so you can program your own battery charger from the default settings and monitor the battery charging process on a computer. So with this Qi Lime Pi shield you are basically getting a BQ24272 Evaluation Module from Ti embedded on a Pi shield.

This Qi Lime Pi Shield isn't for everyone! This is a kit for the people that want to experiment with different battery types, different charging patterns, different voltages, efficiencies, etc. I wanted to make a kit that includes two of the most efficient, best products that TI has on the market right now. I wanted to include functionality to expand to other devices if needed. This board and design will be easy to transfer over to other designs and boards such as the BeagleBone Cape, in which I will show you in my next post! The Hot Qi Dog Cape officially working!

.

The Qi Lime Pi Slice Shield has arrived and will be put together as soon as I can get my hands on the BQ51050B image that will have just a basic Qi Receiver/battery charger and buck boost for simplicity.

I will post my design files for this Slice version in a later post when I have fully tested this design and have a fully working prototype! Again, The boards have arrived!

 

Thank you TI for most of the hard work on making Great Eval Boards and Great Documentation!

 

Thank You,

 

Chad

Attachments:
QiLimePiRev1.zip
imageQi Lime Pi Rev 1.pdf
  • Sign in to reply

Top Comments

  • DAB
    DAB over 13 years ago +1
    Hi Chad, Good post. I like your purple boards, they are a nice change from the normal colors used. I look forward to your next post. Thanks DAB
Parents
  • DAB
    DAB over 13 years ago

    Hi Chad,

     

    Good post.  I like your purple boards, they are a nice change from the normal colors used.

     

    I look forward to your next post.

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnsocm
    johnsocm over 13 years ago in reply to DAB

    Thank you DAB! I had a blast with the competition and wanted a different color board for everyone to see. I wish I had more time for the competition because I have more items to show off! My Qi Lime Pi Slice and the Hot Qi Dog Cape when I get chance to solder them.

     

    Thank you,

     

    Chad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnsocm
    johnsocm over 13 years ago in reply to johnsocm

    Hello World,

     

    The design files in this post are for Eagle. I would really recommend increasing the traces as much as you can if you are going to order a board. This was the first design and I have already made the rev 2 and shortly soon a rev 3 with the BQ51050B!

     

    Thank you,

     

    Chad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • johnsocm
    johnsocm over 13 years ago in reply to johnsocm

    Hello World,

     

    The design files in this post are for Eagle. I would really recommend increasing the traces as much as you can if you are going to order a board. This was the first design and I have already made the rev 2 and shortly soon a rev 3 with the BQ51050B!

     

    Thank you,

     

    Chad