Imagine a World Without Cords
  • Challenges & Projects
  • Design Challenges
  • Imagine a World Without Cords
  • More
  • Cancel
Imagine a World Without Cords
Blog Raspberry Pi - Pi Qi - Qi Pi- Qiπ - A wireless powered Raspberry Pi 1080P HD VIDEO
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: johnsocm
  • Date Created: 19 Oct 2012 12:20 AM Date Created
  • Views 2199 views
  • Likes 4 likes
  • Comments 15 comments
  • raspberry
  • public_wireless_charging
  • pi
  • wireless_power_home
  • wireless_power_challenge
  • qi
  • members_featured_project
  • wp_challenge_one
  • wireless_power_consortium
Related
Recommended

Raspberry Pi - Pi Qi - Qi Pi- Qiπ - A wireless powered Raspberry Pi 1080P HD VIDEO

johnsocm
johnsocm
19 Oct 2012

Hello World,

 

I have effectively powered the Raspberry Pi by the means of Qi Technology. I would like to present the Pi Qi or the Qiπ (Not sure what I will call it yet...Qi Pi..Qiπ)

 

I was sick and tired of all of the cables that had to go in the Raspberry Pi. So I bluetoothed the Mouse and Keyboard! I plugged in a Wifi USB Dongle. Now the only thing left to make it completely wireless is the Power and HDMI or video ports.

 

I have today taken care of the Power and the only thing left is wireless HDMI or Video! image

 

Here are some photos of the progress.... AND THEN THE VIDEO!!!

 

 

Coil Inside Raspberry Pi Case!

image

Coil Mounted Outside Case to show proof of concept and clarity!

image

Wires strung through case bottom.

image

I am just adding more pictures to create more drama and anticipation of watching the Raspberry Pi Boot up Inductively!

image

Evaluation Board mounted (loosely for now) inside the Raspberry Pi case! Please do not look at the solder job! I was in a hurry to watch this work!

image

Coil on bottom of case!

image

Side View of Coil on Raspberry Pi Case.

image

Raspberry Pi Powered up Wirelessly!

image

Raspberry Pi Powered Up Wirelessly!

image

Raspberry Pi Powered up Wirelessly! Sorry, I cannot say it enough!!! image

image

Final Shot! It is fully booted up wirelessly! Nothing is better than that! An Energizer and Texas Instruments Qi Inductive Charged Raspberry Pi! THE Qiπ! (CHEE-PI)

image

ENJOY!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Thank you,

Chad

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Chad, that is awesome! I love the QiPi. hehe. I am in the process of building the same exact thing, hehe. I'm thinking of putting a battery pack on the bottom of the pi and charging the batteries wirelessly…
  • jealderson1
    jealderson1 over 13 years ago +1
    Cool project Chad - of course there would be Gangnam Style in the video
  • ssilberhorn
    ssilberhorn over 13 years ago in reply to johnsocm +1
    Very cool idea Chad.... Check out our battery management portfolio when you are ready to get this thing mobile... solutions for protecting and prolonging battery life, maintaining state of charge, cell…
Parents
  • Catwell
    Catwell over 13 years ago

    Isn't the wireless charger base still wired to the outlet? Hasn't the R-Pi footprint gotten bigger because of it?

     

    You might want to look into using Magnetic Resonance power transfer, like Witricity uses. http://www.element14.com/community/message/21719#21719/l/teslas-wireless-energy-transfer-a-new-reality-almost-available

     

     

    You could add a $150+ USD wireless HDMI adapter to the Pi.

     

    The price of a tidy room is high.

     

    Cabe

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 13 years ago

    Isn't the wireless charger base still wired to the outlet? Hasn't the R-Pi footprint gotten bigger because of it?

     

    You might want to look into using Magnetic Resonance power transfer, like Witricity uses. http://www.element14.com/community/message/21719#21719/l/teslas-wireless-energy-transfer-a-new-reality-almost-available

     

     

    You could add a $150+ USD wireless HDMI adapter to the Pi.

     

    The price of a tidy room is high.

     

    Cabe

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • johnsocm
    johnsocm over 13 years ago in reply to Catwell

    Hello Cabe,

     

    All very good points! Yes Power transfer from one side of the room to the other and farther will be great when available. It is still very much in the early stages and tests are still being done on the effects of being in the way of the "beam" of the power transfer. There are many technologies being developed and everything as of now still has to be plugged into the wall of some matter. Whether it is a Magnetic Resonance Power Transfer scheme, one side is still plugged into the wall to transmit the power. So yes the Transmitter base is still plugged into the wall as one has to get the power from somewhere.

     

    Telsa's biggest problem was when he made wireless power, there was no way to actually meter that power, so in turn everyone could get the power for free. So quickly the idea and investing was shut down.

     

    A wireless HDMI adapter is still too big to put on the raspberry Pi, I agree. There are options to make the Raspberry Pi have wireless HDMI via dongles, or even through wifi.

     

    I don't see the footprint becoming any bigger with the Qi technology. The main transistor is a BGA package and if you have ever seen that size it is almost impossible to solder by hand. 1mm x 1.5mm floating on six solder balls in which you get one chance to hot air solder it correctly or it will short together.

     

    I would love to be a few years in the future because the main idea of the Qi technology is that I can go anywhere, bathroom, restraunt, home, car and be able to forget my chargers and forget having to buy the special adapter for my phone and just place it on a Qi pad and charge my device.

     

    The Raspberry Pi was made for education and this Qi technology can be built into cases for the Raspberry Pi so the footprint wouldn't have to become any bigger. I feel the Raspberry Pi may come in different versions in the future but I agree the footprint does need to stay the same size or become smaller. I feel if you look at the PCB there are plenty of places the bq51013A (Reciever Chip) and the CSD75205w1015 (Q1 Transistor) can be placed. The rest of the components are needed but could be implemented with the 5V circuitry that the Raspberry Pi has already.

     

    Again, the main idea is that soon we can bring our Raspberry Pi, phone, tablet, computer or any other device to anywhere and forget all of the chargers! This works well for the Raspberry Pi because if you plug in a small 4.3" screen or so a kid or any of us can play anywhere and not have to find a outlet. Yes, outlets are everywhere but sometimes in very inconvienent locations (tripping hazards). The Qi technology or simliar will be everywhere eventually and it will be nice to not have to plug devices in.

     

    Thank you and I agree with all of your statements Cabe, but I am just an Electrical Engineer and a Kid at heart when it comes to electronics! I get excited when I can live the future for even a second!

     

    Chad