Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Blog Waterproofing marine equipment - 07 - Receiver Design Considerations
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ForcisConnect
  • Date Created: 21 Apr 2014 10:46 AM Date Created
  • Views 3088 views
  • Likes 3 likes
  • Comments 13 comments
  • beyond_the_phone
Related
Recommended

Waterproofing marine equipment - 07 - Receiver Design Considerations

ForcisConnect
ForcisConnect
21 Apr 2014

This weeks post will be about my receiver board design. I already published the schematic a few weeks ago, as I wanted to make it available as soon as possible, just in case someone else could use it. But now I want to elaborate a little bit on the decisions I had to make for the receiver.

 

I have very closely based my design on the evaluation board receiver. There are different reasons for it: The first is to start with design that is known to work. This will help troubleshoot problems while assembling and testing these first units. The second reason is the required tuning of the resonant capacitors. In order to properly do it we have to measure the coils inductance at 100kHz and 1Vrms to then calculate with these values the capacitors. I don’t have a LCR meter, and the ones with these characteristics are quite expensive. So it’s best to stay close to the EVM values and coils, at least at first.

 

My goal is to achieve a waterproof enclosure. Because of it there will be no external power adaptor. In this way we reduce the necessary openings in the enclosure to none. All the corresponding circuitry from the evaluation board has been removed.

 

The temperature NTC resistor values were also taken from the bq51013B datasheet. A low temperature threshold of -10ºC on the low side and a value of 100 ºC on the high side seemed reasonable.

 

Another important adjustment is the current limit of the chip. I want to be able to get the maximum current of 1.0A out, so the corresponding resistor has been set to 75Ohm.

 

The chip also has different operating modes that can be selected by pulling high or low the EN1 and EN2 pins. The following table from the data sheet summarizes the possible combinations. In our case both are tied to ground. 

image

 

 

So now I have a wireless power receiver. But for my waterproofing application I need not only a power receiver, but also a way to store the energy. This will be done with a Lipo battery. As mentioned by mcb1 these batteries are quite sensitive to overvoltage and wrong charging. Therefore I need a Lipo battery charger.  The bq51050B has essentially the same pins as the 51013B (the only difference is that OUT is called BAT and EN1 is called TERM, all the other pins are the same) and additional components, but includes a Li-Ion charger in the IC. This chip just seems perfect for my application. After having a look at the evaluation board for the bq51050B and noticing that it’s essentially the same as the one of the bq51013B I decided to make a PCB that could be used with both ICs. In this way I won’t need to order separate PCBs, which will save me some money, and the additional board area will be small. Depending on which IC gets mounted, some components will be left unpopulated, while others may be substituted with 0 Ohm resistors.

 

The only components I had to add to make the board compatible with both IC were two resistors between TERM (EN1 at the bq51013B) and GND. These will determine when charging will be completed. I selected a value of 2400 Ohm, which means loading will finish when current gets below 10% of the maximal value, in my case 1A.

 

I have also added a couple of 0 Ohm resistors in series with  FOD, ILIM, TERM and RECT resistors (R8,R9,R10,R12) in order to be able to add a second one in case I needed to change the resistor values to non standard ones afterwards. I got this suggestion at the TI Wireless Power Forum. (http://e2e.ti.com/support/power_management/wireless_power/f/693/t/333462.aspx)

 

I now finally have a complete receiver design!

 

Here is the BOM

 

Qty

Value

Device

Package

Parts

Description

Farnell Code

1

 

LED0603

0603

LED1

LEDs

1465991

2

  1. 0.01uF

CAP

0603

C5, C6

Capacitor

1817916

3

  1. 0.1uF

CAP

0603

C14, C16, C17

Capacitor

2146610

2

  1. 0.47uF

CAP

0603

C3, C4

Capacitor

2354077

1

  1. 1.0uF

CAP

0805

C15

Capacitor

1833815

1

  1. 1.5k

RESISTOR

0402

R3

Resistor

2072645

1

100pF

CAP

0603

C7

Capacitor

1344349

1

10k NTC

RESISTOR

0402

R7

Resistor

9528067

2

10uF

CAP

1206

C12, C13

Capacitor

2394272

1

1800pF

CAP

0603

C8

Capacitor

1865530

1

196

RESISTOR

0402

R1

Resistor

1802961

1

20k

RESISTOR

0402

R4

Resistor

2072753

2

22nF

CAP

0603

C1, C2

Capacitor

1301890

1

  1. 4.22k

RESISTOR

0402

R5

Resistor

2350371

1

47nF

CAP

0603

C9

Capacitor

2070428

1

  1. 66.5k

RESISTOR

0402

R6

Resistor

2073198

2

68nF

CAP

0603

C10, C11

Capacitor

1414650

1

75

RESISTOR

0402

R2

Resistor

2073246

1

AC Coil

LONGPADS

LONGPADS

JP1

 

2114372

1

BQ51013

BQ51013B

QFN-N20

U1

 

 

1

Vout

LONGPADS

LONGPADS

JP2

Header 2

 

4

0

RESISTOR

0402

R8, R9, R10, R12

Resistor

2072513

1

  1. 2.4k

RESISTOR

0402

R11

Resistor

1358052

 

The schematic:

 

image

And PCB layout:

 

Fullscreen contentimage_52589.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

As always: Comments and suggestions are welcome. Once I send the design to the fab it will be too late!

 

EDIT: I have updated the files. I have corrected some smaller issues I noticed while assembling the first units

Attachments:
WirelessReveiver_v0.2.zip
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 12 years ago in reply to janisalnis +1
    Janis I think the 1 year licence will have expired if you didn't collect it within a certain period. If the design is less than 4 layers, you could use the free version. Mark
Parents
  • janisalnis
    janisalnis over 12 years ago

    Thanks for designing receiver board.

    I downloaded the zip file. Schematic opens Ok.

    But when I click on the brd file it does not open and message comes:

    "Illegal data in file"

     

    May be I have too Eagle version

    Version 4.11 for Windows

     

    and should use the Farnell offer for 1 year free licence?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to janisalnis

    Janis

    I think the 1 year licence will have expired if you didn't collect it within a certain period.

    If the design is less than 4 layers, you could use the free version.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • janisalnis
    janisalnis over 12 years ago in reply to mcb1

    Thanks for help! I downloaded and installed newest Eagle freeware version and it opens your board and I can move the parts around. I will start checking it against the datasheet. It is nice that you made such a good starting point for others. I will modify the placement to fit in my project enclosure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • janisalnis
    janisalnis over 12 years ago in reply to mcb1

    Thanks for help! I downloaded and installed newest Eagle freeware version and it opens your board and I can move the parts around. I will start checking it against the datasheet. It is nice that you made such a good starting point for others. I will modify the placement to fit in my project enclosure.