Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Blog Waterproofing marine equipment - 10 - Buck Boost Converter
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ForcisConnect
  • Date Created: 24 May 2014 11:16 AM Date Created
  • Views 1587 views
  • Likes 0 likes
  • Comments 3 comments
  • buck-boost
  • waterproofing_marine_equipment
  • converter
  • beyond_the_phone
  • tps63001
Related
Recommended

Waterproofing marine equipment - 10 - Buck Boost Converter

ForcisConnect
ForcisConnect
24 May 2014

It has been a while since my last post, and I’m very sorry for it, but a new project where I’m getting involved is absorbing all my time.

Nevertheless during this time all my ordered components have arrived and I will start assembling the receiver board next week.

 

This week I’m going to write a little bit about my battery voltage regulator setup.

 

All my new projects (or most of them) work at 3.3V. This is nice because they draw less current then at 5V, I don’t need level converters to interface new sensors that only work with 3.3V etc.  But when I started looking at battery powering one of these projects with a Li-Po battery I quickly realized that my traditional voltage conversion with a linear regulator approach would not work. The voltage of a Li-Po can range from 2.8 when unloaded to 3.7 when loaded. These numbers vary depending where you look them up, but the important fact here is that the voltage is both above and below my desired 3.3V.

 

One possible solution to this problem is called a Buck-Boost converter. These converters act like a buck converter when the input voltage is above the desired output one, and switch to boost converter mode if the input voltage drops below the output one.

 

I decided to use TI TPS63001 regulator. It comes in a small QFN package, needs only one inductor and a few capacitors and resistors as additional components.

 

Here is the boards schematic:

 

image

 

 

The PCB layout file:

image

And the BOM:

 

Quantity

RefDes

Value

DESCRIPTION

SIZE

1

L1

  1. 2.2uH

Inductor

 

3

C1,C2,C3

10uF

Capacitor, Ceramic, 25V, X5R, 10%

1206

3

R1

1MOhm

Resistor

0603

 

 

Finally, here is the assembled circuit (I still have to improve my reflow soldering skills, as the board looks quite dirty!)

image

The circuit works nicely and will be attached to the battery, so I can now get my desired 3.3V!

  • Sign in to reply
Parents
  • mcb1
    mcb1 over 12 years ago

    Looking good.

     

    For cleaning the board you can use "isopropyl alcohol" or failing that methylated spirits

    I usually use an old toothbrush to scrub it.

     

    There are commercial pcb cleaning products, but both these will work.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 12 years ago

    Looking good.

     

    For cleaning the board you can use "isopropyl alcohol" or failing that methylated spirits

    I usually use an old toothbrush to scrub it.

     

    There are commercial pcb cleaning products, but both these will work.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ForcisConnect
    ForcisConnect over 12 years ago in reply to mcb1

    Thanks a lot! I will try to buy some of these.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to ForcisConnect

    Here in NZ the Denatured alcohol is available in most hardware stores.

    The isopropyl alcohol is sometimes available at a chemist, but is rather expensive that way.


    mark