Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Forum What is the range of the Würth Elektronik GmbH & Co. KG " Wireless Power Transfer Solution To Go" solution ?
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 5 subscribers
  • Views 1506 views
  • Users 0 members are here
  • wpc
  • ic
  • compatible
  • würth
  • integrated
  • manager
  • receiver
  • transmitter
  • beyond_the_phone
  • fully
  • evaluation
  • wireless
  • 1.1
  • power
  • module
Related

What is the range of the Würth Elektronik GmbH & Co. KG " Wireless Power Transfer Solution To Go" solution ?

hemmerling
hemmerling over 12 years ago

Hello,,

 

a)

What is the range of the WÜRTH " Wireless Power Transfer Solution To Go" solution

http://www.we-online.de/web/en/electronic_components/produkte_pb/demoboards/wireless_power/wireless_power_1.php

?

 

It is shipped with


5V, Qi Compliant Wireless Power Transmitter Manager Evaluation Module 

http://www.ti.com/tool/bq500212aevm-550

 

and

BQ51013BEVM-764 WPC 1.1 Compatible Fully Integrated Wireless Power Receiver IC Evaluation Module 

http://www.ti.com/tool/bq51013bevm-764


Must be transmitter and receiver be together as known from "charging stations",

or might the power transmission work for about 100 cm, like known from Enotion powerswitches  ?

My design challenge application needs this distance of 100 cm...


b)

What is the operating RF frequency of the devices ?

I did not find any clues in the TI documents...

I don´t mean the clock speed of of an optional or included microcontroller..

 

c)

If I see right, there is no microcontroller included in the set?!

If so, do you think that it would be a good idea to add a MSP430 board for controlling the application :-)?! ( I am used to program it ).

 

Sincerely

Rolf

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Rolf,

     

    to your questions:

    a)     yes, the coils of the Receiver and Transmitter have to be coupled at a z distance of maximal 10mm as defined in the Qi Standard of the Wireless Power Consortium (WPC). Energy up to 5W will be transferred.

    Enotion power Switches operate differently as they only transfer a signal on energy harvesting Basis and not energy.

    To cover a distance of 100cm you have to use a different transfer technology like magnetic resonance, RF or IR.

     

    b) Operational energy transfer frequency is at 120kHz, as the Qi Standard defines 100-205kHz as frequency range.

    This is published in the Qi Standard of WPC.

     

    c) there is no need for an extra µC as the power Management Controllers of the TI boards can be set according to the parameters of the Qi Standard by the programming Interface of the Evaluation boards or jumpers on the boards. Description on the TI Website you mention in your question a).

     

    Best regards

     

    Joerg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sleuz
    0 sleuz over 12 years ago

    This might be of some help for you:

     

    DE

    Wer misst, misst Mist - or measuring the performance of the wireless demo kit

     

    ENG

    self.clue++ : Measuring the performance of the wireless power demo kit

     

     

    Simon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hlipka
    0 hlipka over 12 years ago in reply to sleuz

    btw: there are updated version of my measurements in english and german available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to hlipka

    You have a great table.

    I wonder if you could add the efficiency when the various coils are NOT displaced.

     

    Its very interesting that the 'ebay' electronic receiver performance is not as good, and something a table isn't go to show.

     

     

    Well done

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hlipka
    0 hlipka over 12 years ago in reply to mcb1

    Actually, these number are already there. I just was not clear about them. When looking at the current draw, the lowest value is the one with no displacement. The larger the displacement, the higher the current consumption. So the first number for the current, and therefore the first number of the efficiency, is the one with no displacement.

    I will update the articles accordingly, to make that clearer.

    Regarding the ebay receiver: with lower loads (and small distances) its efficiency is better. With higher loads it goes to about par. With larger vertical distances it also gets better, also with higher displacement. OTOH its adaptive power management seems not as good, and it needs lower distances to pick up a connection.