Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Forum What is the range of the Würth Elektronik GmbH & Co. KG " Wireless Power Transfer Solution To Go" solution ?
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 5 subscribers
  • Views 1507 views
  • Users 0 members are here
  • wpc
  • ic
  • compatible
  • würth
  • integrated
  • manager
  • receiver
  • transmitter
  • beyond_the_phone
  • fully
  • evaluation
  • wireless
  • 1.1
  • power
  • module
Related

What is the range of the Würth Elektronik GmbH & Co. KG " Wireless Power Transfer Solution To Go" solution ?

hemmerling
hemmerling over 12 years ago

Hello,,

 

a)

What is the range of the WÜRTH " Wireless Power Transfer Solution To Go" solution

http://www.we-online.de/web/en/electronic_components/produkte_pb/demoboards/wireless_power/wireless_power_1.php

?

 

It is shipped with


5V, Qi Compliant Wireless Power Transmitter Manager Evaluation Module 

http://www.ti.com/tool/bq500212aevm-550

 

and

BQ51013BEVM-764 WPC 1.1 Compatible Fully Integrated Wireless Power Receiver IC Evaluation Module 

http://www.ti.com/tool/bq51013bevm-764


Must be transmitter and receiver be together as known from "charging stations",

or might the power transmission work for about 100 cm, like known from Enotion powerswitches  ?

My design challenge application needs this distance of 100 cm...


b)

What is the operating RF frequency of the devices ?

I did not find any clues in the TI documents...

I don´t mean the clock speed of of an optional or included microcontroller..

 

c)

If I see right, there is no microcontroller included in the set?!

If so, do you think that it would be a good idea to add a MSP430 board for controlling the application :-)?! ( I am used to program it ).

 

Sincerely

Rolf

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Rolf,

     

    to your questions:

    a)     yes, the coils of the Receiver and Transmitter have to be coupled at a z distance of maximal 10mm as defined in the Qi Standard of the Wireless Power Consortium (WPC). Energy up to 5W will be transferred.

    Enotion power Switches operate differently as they only transfer a signal on energy harvesting Basis and not energy.

    To cover a distance of 100cm you have to use a different transfer technology like magnetic resonance, RF or IR.

     

    b) Operational energy transfer frequency is at 120kHz, as the Qi Standard defines 100-205kHz as frequency range.

    This is published in the Qi Standard of WPC.

     

    c) there is no need for an extra µC as the power Management Controllers of the TI boards can be set according to the parameters of the Qi Standard by the programming Interface of the Evaluation boards or jumpers on the boards. Description on the TI Website you mention in your question a).

     

    Best regards

     

    Joerg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Rolf,

     

    to your questions:

    a)     yes, the coils of the Receiver and Transmitter have to be coupled at a z distance of maximal 10mm as defined in the Qi Standard of the Wireless Power Consortium (WPC). Energy up to 5W will be transferred.

    Enotion power Switches operate differently as they only transfer a signal on energy harvesting Basis and not energy.

    To cover a distance of 100cm you have to use a different transfer technology like magnetic resonance, RF or IR.

     

    b) Operational energy transfer frequency is at 120kHz, as the Qi Standard defines 100-205kHz as frequency range.

    This is published in the Qi Standard of WPC.

     

    c) there is no need for an extra µC as the power Management Controllers of the TI boards can be set according to the parameters of the Qi Standard by the programming Interface of the Evaluation boards or jumpers on the boards. Description on the TI Website you mention in your question a).

     

    Best regards

     

    Joerg