element14 presents
  • Challenges & Projects
  • More
element14 presents
e14 presents blogs Introducing Solas and the journey of creating my own RGB LED Board
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: lorrainbow
  • Date Created: 1 Mar 2022 11:47 PM Date Created
  • Views 8383 views
  • Likes 14 likes
  • Comments 22 comments
  • makecode
  • pcb
  • 3D Printing
  • led
  • rgb
  • rp2040
  • blocks
  • laser cutting
Related
Recommended

Introducing Solas and the journey of creating my own RGB LED Board

lorrainbow
lorrainbow
1 Mar 2022

Initial Ideas

Over 3 years ago I really wanted a single RGB LED controlled by a microcontroller. I didn't want to add LEDs to a microcontroller, solder them, chain them, wire them up! I just wanted an RGB LED connected a microcontroller. And, as far as I could tell, none existed. Or at least nothing that simple and easy to code. I thought this would be a great project to replace my huge RGB LED cube that I had made the year before in 2018. 

Learn more about Cubert here! 

Cubert

Cubert

Cubert was a 1 metre cube of 8x8x8 RGB LEDs connected together through copper rods using custom PCBs. It was controlled by 1 micro:bit. It was a fantastic and much loved project. I coded it so people could play their favourite old school games like Snake! Or Pacman. But in 3d! And in lights on a metre cubed cube :D What I loved about Cubert, besides how it looked, was how interactive it was. I don't like to create technical art pieces that you just look at. I want you to poke it! And play with it. And shake it. Cubert was interactive, but it was one player. And with one microcontroller it was difficult to have multiple people interact with it. I did have some games where two people had a micro:bit each and using the radio and the accelerometer they would race to fill the cube with their colour by shaking their micro:bit! But what I really wanted was a project where everyone could code their device and add it to a bigger structure, working together to create something. That's where I came up with the idea for Solas. A small programmable RGB LED that could be chained to other RGB LEDs in something like a tree structure. Each light could be a leaf. 

Fun Fact: Solas means light in Irish

Solas Version 1: 2020

A couple of years I did have a go at creating Solas. I'm no PCB designer so my husband created this design for me. The PCB has a chip and electronics to manage the USB and the rechargeable battery on the back. The idea was you added hats to the PCB with RGB LEDs attached. We ordered 5 PCBs for testing and used 3d printing to imagine the case, the lids, etc. 

imageimage

It was a nice start! But this was 2020 and just as we got the PCBs back we entered lockdown in the UK and I was suddenly home schooling 2 kids! So Solas went on the back burner. 

Solas Version 2: 2022

This year is the year of Solas! We started planning and designing it again. The initial design wasn't ideal for connecting the boards together. And how we connected the hat to the board also wasn't clear. This new version would follow the original idea of one board with the chip and the LED together. I've given up on the battery, for now! And am focusing on the connection between the boards. Working with Microsoft Research as part of my day job with Lancaster University gave me insight into a new modular electronics system called Jacdac. It allows the easy connection of modules to microcontrollers and to other microcontrollers. It can also be easily connected to a web browser for coding. One vital aspect of Solas for me is how easy it is to code. I don't want to have to code it in C or even python. I want young children to drag and drop blocks onto their Solas and have it up and running in minutes. Similar to the BBC micro:bit (that I'm really fond of!). 

It's 1st March 2022 and we've designed Solas V1 and sent it off to the PCB manufacturer. We're using the RP2040 chip with the jacdac modular system. Here are the PCB pictures. Each Solas has 3 Jacdac connectors and a micro USB connector on the 4th side for powering on its own. A Solas can be powered through Jacdac but the first Solas in the chain needs to be powered over USB. The LED is on the top and the RP2040 is on the bottom.  The 2 gaps on the side of the top photo are for buttons: boot and reset. We're having the boards assembled as well as created, which is going to take a while especially given the low stock of components lately. 

imageimage

Solas Petal

We ordered 5 of the Solas version 2 board in February 2022. It looks like it won't arrive until April. After some quick testing we'd plan to order a large quantity of the board to build the tree of light, it depends on costs and funding.. maybe 100 or 200. I'd love to make 500 and give them away at festivals! I want to take Solas and the tree to family events. The first possible event is EMF camp which is the 2nd June, which is very close to April given how long the first 5 PCBs took to arrive... So we started to panic a bit about that! We decided to make a single RGB LED petal that would attach to Solas over Jacdac and be codeable, chainable. It's Solas without the PCB. We made the petal in the same shape as Solas, but smaller and without assembly and ordered 200 of them in February. We're going to have to assemble them ourselves, soldering on the RGB LED, resistors, etc. Fingers crossed we can make light (get it?) work of that. We did solder 512 surface mount RGB LEDs onto PCBs for Cubert! Time to brush up on our soldering skills. 

Hopefully the 5 prototype PCBs we've ordered will work and we can use them alongside some other Jacdac microcontrollers to light up the tree with the 200 petals for EMF camp. While waiting on PCBs to arrive, we're working on the tree itself.

Laurelin: the tree of light

Solas is a leaf/light that attaches to branches on a tree. We decided to call the tree Laurelin (LOTR reference). I don't want the tree to be too tall that I would need a ladder to attach lights to it, so we're thinking 2 metres high. It needs to be collapsible and fit inside a car boot. Here are some of the original design files for the branches:

image

There are multiple layers of these of different sizes. 4 layers in total with the top 2 layers being 3mm thick and in frosted acrylic. The bottom 2 layers are thicker in wood with the trunk being maybe 9 or 12mm thick and 3 long pieces that can be screwed together. This is beyond the size of my laser cutter so we're relying on friends to help us with cutting the branches. 

Here's the latest prototype and one quarter scale:

image

I like it! We need to add holes and figure out how each Solas/petal will connect to the branches. We also need to thread the wires through the branches.. possibly spray painting them so they look like roots! And maybe etch the wooden branches with decorations. 

Coming soon to Element14 presents: a video of Solas version 1 in action, RGB LEDs, Jacdac, how we got version 2 to work with Jacdac and Microsoft Makecode and designing the leaf that wraps around Solas to make it glow:

imageimage

I'll keep you updated on Solas and Laurelin's progress!

Comment below and questions or suggestions you have for Solas or Laurelin. 

Maybe one day you'll see it and me at your local electronics' family festival! 

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 4 years ago in reply to lorrainbow +1
    Hi Lorraine, thanks for the clarification. There appears to be an open source padauk chip programmer here which may work out a bit cheaper: https://blog.adafruit.com/2020/09/03/programming-padauk-microcontrollers…
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    "...We decided to make a single RGB LED petal that would attach to Solas over Jacdac and be codeable, chainable. It's Solas without the PCB..."

    Is the Solas Petal more-or-less a 'prototype' Solas and still using a RP2040 as the brains ? or is it an off-the-shelf JM Single RGB LED module stuck onto a Solas PCB template ? Not quite clear if the upstream Solas it is attached to is being coded or the Solas Petal itself.

    Looks like some of the Microsoft reference designs are using the STM32 for basic IO onto Jacdac for the time being, with a few alternative devices for their 'JM Brain' reference modules.

    Is there an intention to use the tree branches as 'Dedicated hubs' at all or will it be a case of daisy chaining each petal back along each branch testing your 'graph theory' maths skills (soon to become known as 'the travelling petal problem').

    I was thinking that the branches would be quite well suited to the filament LED strips which tend to come in predefined lengths as you could adjust the sizes to suit. You could perhaps also have some 'active branches' acting as 'Hub devices' providing both IO and bus routing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lorrainbow
    lorrainbow over 4 years ago in reply to beacon_dave

    Hi Dave!

    A petal is like a jacdac module, not a brain. It's got a PIC as its controller, as unfortunately most STM32s are out of stock. Also the programmer for the padauk chips costs like a £150! This is why we've gone with a PIC. We're confident it will work

    We think a Solas can control up to 16 petals, the max for the current limitation. So one Solas will be on a lower branch and daisy chaining multiple petals in different directions. EMF camp is 2nd June and our 5 prototype Solas' are due in April! So we're worried our 2nd order of Solas' won't arrive in time and we won't have enough brains to make a light up tree. 

    With this plan P, we're planning on using the 5 Solas brains and perhaps 3 micro:bit brains on the lower level (the lowest has 8 branches) daisy chaining 16 petals each to make 128 + 5 lights on the tree. Of course we can always add light strips connected to a pi or arduino if it's looking a bit dim! 

    We had planned this project for a festival in Belgium in August so every person can have their own individual controllable chainable light. (a Solas, not a petal). 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lorrainbow
    lorrainbow over 4 years ago in reply to beacon_dave

    That padauk controller would be really difficult to solder and expensive to get manufacturered. I like that it's open source though. 

    It's a single shared bus, so just 1A between the 3 connectors. There's a micro USB connector on Solas for powering. (The petal doesn't have that, it's purely bus powered) 

    For whole tree control we were thinking of a raspberry pi at the bottom connected to all devices. Not sure how that's going to work yet. I don't want to control the whole tree at once often, as it's meant to be a community tree made up of individual leaves. 

    L

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to lorrainbow

    I'd volunteer to solder up a couple of these if you or element14 could get the parts to me, but the microcontroller has a lead time of 52 weeks : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    Can you solder up a time machine first ? Thinking

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to lorrainbow

    A couple of powered USB hubs hung off of the R-Pi and a bag of USB external hard drive Y-cables might do the trick if you are looking at supplying around 1A to each brain.

    How does the community tree thing work in practice ? Do you start with a bare tree and each participant programs and adds their creation to the tree one-by-one until it is fully loaded ? Or do you start with a tree fully loaded with petals and each petal then gets replaced with a programmed brain ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    There appears to be a low cost discovery kit which contains the STM32F072RBT6 microcontroller (rather than the STM32F072C8T6) which looks like a close match.

    https://uk.farnell.com/stmicroelectronics/stm32f072b-disco/dev-kit-stm32f072b-discovery/dp/2376483

    Shorter lead time of and of April 2022.

    I'm guessing that that one of those plus a simplified PCB / protoboard design for the rest would allow one to use the same programming firmware/software and make it more accessible for a wider audience.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    There appears to be a low cost discovery kit which contains the STM32F072RBT6 microcontroller (rather than the STM32F072C8T6) which looks like a close match.

    https://uk.farnell.com/stmicroelectronics/stm32f072b-disco/dev-kit-stm32f072b-discovery/dp/2376483

    Shorter lead time of and of April 2022.

    I'm guessing that that one of those plus a simplified PCB / protoboard design for the rest would allow one to use the same programming firmware/software and make it more accessible for a wider audience.