element14 presents
  • Challenges & Projects
  • More
element14 presents
e14 presents blogs Small circuits - Ideas needed for my Fidget Cube!
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: hifromkatie
  • Date Created: 25 Oct 2021 3:19 PM Date Created
  • Views 6382 views
  • Likes 4 likes
  • Comments 26 comments
  • tinypcb
  • Cube
  • element14 presents
  • fidget toy
Related
Recommended

Small circuits - Ideas needed for my Fidget Cube!

hifromkatie
hifromkatie
25 Oct 2021

Hi all!
I'm currently working on an element14 presents project, to make a electronics/engineers fidget cube. What do you think, good idea?

My original aim was to make a 1" cube with small circuits on each side, but fairly quickly I realised this was going to be tight on space, I have now upped the size to 50mm cube (approx 2").

 

My design spec is as follows:

  • One side is a power supply, has a LiPo battery input and outputs 5v to 5 Molex PicoBlade connectors.
    • Pin1: +5V
    • Pin2: GND
  • Each side is completely stand-alone, has no dependency on any other side, other than the power connector.
    • All processing must be done on that side's PCB
  • The visible area of each side is 40mmx40mm
  • The PCB is 44mm by 40mm (This has a 2mm edge on 2 sides to slot into a 3D printed framework which will hold all the PCBs in to a cube shape.

 

I currently have the Power supply PCB designed, this also includes a fidget element of a push button which will turn 8 LEDs on and off

Front and Back:

imageimage

 

 

 

The next side I have designed is a logic gates and Binary counter board.
The top half has inputs A and B, and surrounding them the output of the following gates, based on input A and B, OR, XOR, NOR, XNOR, AND & NAND.

The lower half has a 6 bit binary counter, with a button to increase and decrease the counter.

 

Front and Back:

imageimage

 

I am planning on a "sketch side" which will consist of an LCD or OLED display and a joystick which will allow you to draw lines on the screen (Think Etch-a-Sketch).

This is currently proving hard to fit into the space and design requirements, but I think I've got a solution, but I haven't modelled this yet, so you might just have to trust me on this one (and I'm desperately hoping I've done the PCB correctly for it to all work like I've planned!)

 

The framework to hold these into a cube will be 3D printed, and currently looks like this:

The red is the top half and the blue shows the bottom, these will slide over the PCBs due to a groove on the 4 outside faces. The top and the bottom will need some hotmelt glue or other fixing method designed into the 3D print to hold them in place. Potentially an internal framework which will push against the back of the PCB and also securely hold the LiPo battery pack.

image

 

So what do you think of this idea?
Have you got any suggestions for the sides I've already come up with? Improvements, or criticism welcome!

I still need 3 sides, if you have an idea for a side then please let me know and I can design it for the cube. Or if you would like to try designing a side I'd love to see your design.


With the sides being independent and fitting the design criteria, I'm thinking they could be interchangeable and swapped in and out.
We could invent our own swapping system, if someone designed a side and makes a few and swaps them with other people who've made their own, we could all make our own unique fidget cubes!

Please feel free to tell me if I'm getting carried away now...!

  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to thewildotter

    thewildotter  wrote:

     

    Consider "Touch Switches"

    Physical switches tend to be a bit large.    There are lots of "touch switch" examples online using cmos IC's (eg. How to Build a Touch Sensor Circuit with a NAND Gate chip ) which only need a couple of exposed PCB trace "probe points" in the HMI (human machine interface) area.  Such switches might implement "momentary contact", latched, debounced, auto repeat,... functions into these small spots on the PCB. Many cmos MSI (eg., 74HC4011,...) chips have been revived in surface mount versions possibly making them small enough to be located very close to a trace to be touched.  A "crossbar" switch design on your PCB could provide a very large number of switches in a very small area.    Latched switches might be mounted with an LED to show which switches are in which state with either on/off or color either at the switch or elsewhere.   Using such "touch switches" can dramatically shrink the input "human/machine interface" (HMI) footprint on your fidget, thus greatly expanding the range of applications you might implement.  Touch switches can be one finger spanning two traces, one hand on one trace and a finger on another, one hand on a trace and another hand holding a stylus to touch points in an HMI input area.  An HMI input area might map to a separate HMI output "screen" far enough away to be seen without the input finger obstruction.   There is a whole world of cleverness these I/O area shrinking tricks can make accessible since they greatly increase the HMI input resolution.

    _______________

    thewildotter

    Yes, or a bit simpler: capacitive touch pads on the outside that regulate the intensity of a led (mounted on the inside shining out). A dimmable flashlight/torch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 5 years ago in reply to beacon_dave

    Yeah, and fidget cubes are all about feedback and responses, so interacting with a small motor inside the cube would also be cool.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • thewildotter
    thewildotter over 5 years ago

    TV Mute is a "Killer" App

    Another "killer" application might be a "learning" remote control.   Then you could capture your high use remote functions and retain your TV(etc.,...) control without laying down your fidget to pick up the TV remote.  Mute springs to mind as a great button to have it memorize so you could turn down those annoying super-loud commercials they like to blast at you after you have raised the volume to hear whispered dialog.  So, the app would have an infrared detector and an infrared emitter attached to appropriate I/Os on a microprocessor.   One button on your PCB would tell the fidget to record until you release it.  You press that button and then the mute button on the real remote, then release.   Another "playback" button on your fidget PCB would then play back the last recorded remote command.   Since mute is usually a toggle, one remembered remote command is enough to shut up those annoyingly loud advertisements.  You just press the playback button again to unmute once the annoyance passes.  I sure would like to have a smart fidget with that feature.

    ________________

    thewildotter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • thewildotter
    thewildotter over 5 years ago

    "Star Trek Music"

    An interesting specific application might be a GSR Theramin.  Use high impedance inputs to opamps from several finger touch spots.   Use about a 1/4 second sampling clock.  Change your finger pressures on the beat of this slow clock.   Sample the GSR of several fingers to capture the pressure values to use to provide the Theramin parameters for the next slow time slice.   Output the GSR results into a laptop scale speaker behind the (holy to let sound through) PCB.  Learn to play  the intro music to the original "Star Trek" TV series (a Theramin instrumental) and other classic Theramin pieces.   Some of the fingers may be direct analog with no clock to allow live production of the Theramin frequency slides.  With this PCB you will be able to fidget to music of your own creation.   There are microprocessors with AtoD converters and PWM output which might make this application a very simple PCB with wildly customizable software. It could possibly include bars of pre-recorded Theremin music that you can lip-sync with your fingers and appear to be quite the musician.

    ______________

    thewildotter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 5 years ago in reply to cstanton

    I was thinking that you could perhaps have 'input sides' and 'output sides' with an intercommunication bus. There are numerous applications that could use a LCD display but you are only likely to be interested in the one you are looking at any given time, which led me to...

     

    Perhaps only the top-facing side should be active - some sort of orientation sensor at the core that only powers up the top most side. If you have multiple sides with audio outputs then you may not want them all active at the same time, however...

     

    If you have input and output sides, then you need more than one side active at a time, but then...

     

    Trying to use input buttons on the reverse of the cube whilst viewing a screen in front of you could get tricky. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>