Name: akshitagupta15june
Current home town: Kanpur, Uttar Pradesh, India
Did you attend university? Pranveer Singh Institute of Technology Kanpur, Bachelor of Technology in computer Science
Current Job: Undergraduate second year student
Your favorite electronics projects from element14 presents or youtube:
Your project:
Under this lockdown i hope everyone is trapped in there home but due to the opportunity by element 14 i have got a great chance to show my project as a episode . It is first time making this project and recording such a long video so please pardon me if something is done wrong.
MULTIPURPOSE AGROBOT
Problem Statement / Purpose of Project
DESIGN COST EFFECTIVE BUSINESS SOLUTION WITH GOOD USE OF TECHNOLOGY AND MECHANISATION FOR SUSTAINABLE AND COOPERATIVE AGRICULTURE, FARMING.
Full Automatic MULTIPURPOSE AGROBOT using Internet of Things(IOT)
The work is done by robot without any man power.
Automation is used in all fields eg. automobiles , manufacturing fields.
Automation is a illumination of human afford from the working field.
The idea of applying robotic technology in agriculture is very new, the opportunities for robot enhanced productivity immense.
The robots performing agriculture operations such as ploughing , seed sowing and water spraying.
Allowing farmers to reduce the environmental impact, increase precision and efficiency, and manage individual plants in novel ways.
PRINCIPLE AND FEATURES OF AGROBOT
The main impact for our project has been to develop a solar operated digging
machine, which is solar powered. In this machine, we used a solar panel to
capture and convert solar energy into electrical energy which is used to charge a
5v battery. Which gives the necessary power to a DC motor. With the help of
Bluetooth modules, we connect all the commands through our remote. This
power is transmitted to the rear wheel through gears. In this project it makes the
electric and mechanical systems share their power in efficient way. It reduces the
running cost of digging machine.
Features
Automatic grass cutter
Automatic seedling Sprinkling
Fertilizer Sprinkling
Irrigation &
Hydraulic cultivator
Solar power operated
Automated with remote
LIST OF EQUIPMENTS USED FOR AUTOMATION
Arduino Uno, MotorDrivers L298, DC MOTOR, 2-Bluetooth Module SC05, Battery(12volts), LED & Buzzer, Resistor(1kiloohm), Transmitter remote with switches, Solar Panel, 8 switches
WORKING OF MULTIPURPOSE AGROBOT
• The seeds and spraying the water with least changes in accessories with minimum
cost. This whole system of robot works with battery and the solar power.
• The basic frame is made for the robot with 4 wheels connected and the rear wheels are
connected with motor.
• At one end of the frame, cultivator is fitted which is also driven by DC motor and
design is made to dig the soil.
• Funnel is used to store the seeds and fertilizers, it flows through the funnel by drilled
hole on the shaft/anchor to the digged soil. On the end sprayer is fitted to spray water.
In front blades are set to cut the crops or grass.
• Solar is placed on the top of the robot and is connected to a battery for charging the
battery.
• Firstly, we can send data through our own remote that is developed by me, with the
help of Bluetooth connectivity.
• Bluetooth module receives the data according to our program that is in Arduino UNO.
Quality Assurance and Quality Control
• For quality control I have used solar power for the charging of the batteries it also
decreases the initial cost.
• For quality control purpose I have tested this agrobot in uneven field as it has to work
in farm areas.
ADVANTAGES
Machine is small and can be carried anywhere
It will cut the plants from roots
Maintenance cost is less
It could cut the tons of grains in a day
It reduces the manpower
It may become a great success if this project can be implemented throughout our country.
Are there any links or files you'd like to provide that support your project?
I have added this link where all code snippet of transmitter and receiver section is attached and all related documents are also attached.-: https://drive.google.com/open?id=1K1PMABZKO2UxA1gQCUWS1eLo8hruyouY
Your Project video: Please have a look at my video

Top Comments
-
a531016
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
a531016
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children