#badass Online Film Festival
  • Challenges & Projects
  • element14 presents
  • #badass Online Film Festival
  • More
  • Cancel
#badass Online Film Festival
Documents #badass Woman Project Entry - Akshita Gupta
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join #badass Online Film Festival to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 13 Apr 2020 2:51 PM Date Created
  • Last Updated Last Updated: 19 May 2020 4:16 PM
  • Views 4703 views
  • Likes 20 likes
  • Comments 33 comments
Related
Recommended

#badass Woman Project Entry - Akshita Gupta

Name: akshitagupta15june

Current home town:  Kanpur, Uttar Pradesh, India

Did you attend university?  Pranveer Singh Institute of Technology Kanpur, Bachelor of Technology in computer Science

Current Job: Undergraduate second year student

Your favorite electronics projects from element14 presents or youtube:

https://youtu.be/SdGtVfxwO9g

https://youtu.be/Dj-4U6VCHhM

 

Your project:

 

Under this lockdown i hope everyone is trapped in there home but due to the opportunity by element 14 i have got a great chance to show my project as a episode . It is first time making this project and recording such a long video so please pardon me if something is done wrong.

 

MULTIPURPOSE AGROBOT

Problem Statement / Purpose of Project

DESIGN COST EFFECTIVE BUSINESS SOLUTION WITH GOOD USE OF TECHNOLOGY AND MECHANISATION FOR SUSTAINABLE AND COOPERATIVE AGRICULTURE, FARMING.

Full Automatic MULTIPURPOSE AGROBOT using Internet of Things(IOT)

 The work is done by robot without any man power.

 Automation is used in all fields eg. automobiles , manufacturing fields.

 Automation is a illumination of human afford from the working field.

 The idea of applying robotic technology in agriculture is very new, the opportunities for robot enhanced productivity immense.

 The robots performing agriculture operations such as ploughing , seed sowing and water spraying.

 Allowing farmers to reduce the environmental impact, increase precision and efficiency, and manage individual plants in novel ways.

image

PRINCIPLE AND FEATURES OF AGROBOT

The main impact for our project has been to develop a solar operated digging

machine, which is solar powered. In this machine, we used a solar panel to

capture and convert solar energy into electrical energy which is used to charge a

5v battery. Which gives the necessary power to a DC motor. With the help of

Bluetooth modules, we connect all the commands through our remote. This

power is transmitted to the rear wheel through gears. In this project it makes the

electric and mechanical systems share their power in efficient way. It reduces the

running cost of digging machine.

Features

 Automatic grass cutter

 Automatic seedling Sprinkling

 Fertilizer Sprinkling

 Irrigation &

 Hydraulic cultivator

 Solar power operated

 Automated with remote

 

LIST OF EQUIPMENTS USED FOR AUTOMATION

Arduino Uno, MotorDrivers L298, DC MOTOR, 2-Bluetooth Module SC05, Battery(12volts), LED & Buzzer, Resistor(1kiloohm), Transmitter remote with switches, Solar Panel, 8 switches

 

WORKING OF MULTIPURPOSE AGROBOT

 

• The seeds and spraying the water with least changes in accessories with minimum

cost. This whole system of robot works with battery and the solar power.

• The basic frame is made for the robot with 4 wheels connected and the rear wheels are

connected with motor.

• At one end of the frame, cultivator is fitted which is also driven by DC motor and

design is made to dig the soil.

• Funnel is used to store the seeds and fertilizers, it flows through the funnel by drilled

hole on the shaft/anchor to the digged soil. On the end sprayer is fitted to spray water.

In front blades are set to cut the crops or grass.

• Solar is placed on the top of the robot and is connected to a battery for charging the

battery.

• Firstly, we can send data through our own remote that is developed by me, with the

help of Bluetooth connectivity.

• Bluetooth module receives the data according to our program that is in Arduino UNO.

 

Quality Assurance and Quality Control

• For quality control I have used solar power for the charging of the batteries it also

decreases the initial cost.

• For quality control purpose I have tested this agrobot in uneven field as it has to work

in farm areas.

ADVANTAGES

 Machine is small and can be carried anywhere

 It will cut the plants from roots

 Maintenance cost is less

 It could cut the tons of grains in a day

 It reduces the manpower

 

It may become a great success if this project can be implemented throughout our country.

 

 

 

Are there any links or files you'd like to provide that support your project?

I have added this link where all code snippet of transmitter and receiver section is attached and all related documents are also attached.-: https://drive.google.com/open?id=1K1PMABZKO2UxA1gQCUWS1eLo8hruyouY

 

 

 

Your Project video: Please have a look at my video

 

This video is unavailable.
You don't have permission to edit metadata of this video.

  • badass
  • badass women makers and engineers
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • KalebTheMaker
    KalebTheMaker over 6 years ago +3
    Nice mix of mechanical and electrical design! I have to agree with Dave on the "powerpointy" thought. Diagrams and documentation are great and necessary, but seeing more of you interacting with the robot…
  • alanmcdonley
    alanmcdonley over 6 years ago +3
    Nice "Proof of Concept (POC) Robot" combining many functions to one robot. A little scary to see unshielded cutters, but consistent with POC. Very creative engineering. Good job.
  • davedarko
    davedarko over 6 years ago in reply to akshitagupta15june +2
    It did Today A bit of feedback: it feels very "powerpointy", would have loved some more videos of it moving around and you showing / pointing at the parts you are talking about in the first bit. The block…
Parents
  • akshitagupta15june
    akshitagupta15june over 6 years ago

    kellyhensen when will this project release in official site and i hope u like it.

    Thankyou so much element 14 community for giving this awesome opportunity.

    element14 presents

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • davedarko
    davedarko over 6 years ago in reply to akshitagupta15june

    It did Today image

     

    A bit of feedback:

    it feels very "powerpointy", would have loved some more videos of it moving around and you showing / pointing at the parts you are talking about in the first bit. The block diagram was very helpful though, I sometimes regret that I forgot to add that to my videos. What were you using for editing the videos? Would have been great to see the cellphone shots integrated not vertically.

     

    You mentioned IoT somewhere, but I don't really see any internet integration - what are your plans for that?

    I do like the seed rattler thing - hope no ones feed where cut off by the razor blades though image

    I wonder if it gets easier through the dirt if it runs backwards, the orange rollers look like they might get stuck.

     

    Loved the presentation at the end! Super scary blades image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • akshitagupta15june
    akshitagupta15june over 6 years ago in reply to davedarko

    Thankyou so much for your feedbacks. As it was first long video making i will try to look at your feedback and will make changes in next one.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • akshitagupta15june
    akshitagupta15june over 6 years ago in reply to davedarko

    Thankyou so much for your feedbacks. As it was first long video making i will try to look at your feedback and will make changes in next one.