element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Blog The Ben Heck Show Needs Your Help!- Episode Live!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: element14Dave
  • Date Created: 31 Jul 2014 4:44 PM Date Created
  • Views 4641 views
  • Likes 0 likes
  • Comments 55 comments
  • crusher
  • ideas
  • ben_heck
  • heck
  • ben
  • can
Related
Recommended

The Ben Heck Show Needs Your Help!- Episode Live!

element14Dave
element14Dave
31 Jul 2014
image
image
Ben Heck home page
Ben's Top 5 Lifehacks
Ben's build kit

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


The  Can Crusher Buildhttp://www.element14.com/community/docs/DOC-24800/l/episode-3-ben-builds-an-automatic-can-crusher-or-does-he never turned out the way Ben and team wanted it to and is in need of an update. In an upcoming episode of The Ben Heck Show,  Ben and team will be creating "Can Crusher 2.0" and they need your help! Let Ben know your idea for what he should do for "Can Crusher 2.0"  by following the directions below.


Thanks for all of the wonderful ideas around "Can Crusher 2.0" Ben and team will be going through and evaluating the comments...check out how Ben used your ideas for the build!

Episode 153: Ben Heck’s Crowdsourced Can Crusher Part 1 Episode

 

 

Directions:


Step 1:  Log in or register on element14, it's easy and free.

 

Step 2: Post your suggestion in the comments section below. Videos, pictures and  text are all welcomed forms of submission. Comments or instructions should be limited to 200 words or less and contain no more than 2 diagrams.

 

Step 3:  Sit back, relax, and enjoy the show!  We will accept ideas until 12:01am Central Time  on August 18, 2014.  If you need something to do between now and then make sure to check out what is happening on This week on element14 Community, or watch more Ben Heck at element14.com/TBHS.


 

Important Notice:

  • By submitting an entry you will automatically start receiving notifications of other responses to this post. If you do not wish to receive notifications, select "Unfollow" at the top right of the post. If you have any questions, please let us know in our Feedback & Support area.
  • Sign in to reply

Top Comments

  • michaelwylie
    michaelwylie over 12 years ago +4
    Ben; I have two ideas, and they're more for the cool factor rather than practicality. 1. Use a solenoid with a plunger to catastrophically crush the can. 2. Use a vacuum system to suck the air from the…
  • Workshopshed
    Workshopshed over 12 years ago +2
    Oversized gear wheels with the can fitting between the teeth.
  • Kilohercas
    Kilohercas over 12 years ago +1
    i would use large capacitor and large coil,>20kj Or more simple idea, 2kW induction heater, all you need to do is to place can inside ceramic holder with large coil around, and it will melt in few seconds…
Parents
  • diamonddrake
    diamonddrake over 12 years ago

    For simplicity sake, Use a weight hung below or above the can to be crushed, the can goes in a crushing sliding housing similar to the one in the video. Use a geared motor with a screw system to slowly lift the heavy weight. This would allow for a lower powered motor to lift the heavy weight. then when actuated the weight would drop being allowed to pick up momentum that would be used to crush the can. As the weight system is reset the crushed can would be ejected.

     

    image

    I apologize for poor quality sketch.

    A turning screw shaft would go up the center of the weight and be spun by a motor. The weight would have rod guides to keep it sliding up and down. two solenoid actuated teeth would grab the screw shaft to lift it up and would be able to pull apart releasing the weight to slide down the guides and crush the can with momentum. The teeth would reengage and the motor would reset the weight.

     

    just a thought. I'm sure it would work but I don't know if it's the best way. I was leaning toward moderate size and low power consumption. What's the use of recycling if you have to waste tons of electricity running an air compressor for a pneumatic cylinder or the like. Potential energy for the win!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to diamonddrake

    It is certainly a great solution for using a low powered motor, but overall the can crushing rate is low and is limited by the power output of the motor (which is defined as energy per second (in this case we could even call it Work/seconds (as work is the change in energy(lets call it the amount of energy used to crush the can))(watts = joules/seconds). So while using a heavy weight can decrease the force required by the motor to crush the the can, it does not decrease the amount of work required to crush the can(work = force x displacement) because the displacement has been increased to compensate for a lower force. I love your outside the box thinking but effectively you have built a "force modifier device" such as a gearbox or lever.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to diamonddrake

    It is certainly a great solution for using a low powered motor, but overall the can crushing rate is low and is limited by the power output of the motor (which is defined as energy per second (in this case we could even call it Work/seconds (as work is the change in energy(lets call it the amount of energy used to crush the can))(watts = joules/seconds). So while using a heavy weight can decrease the force required by the motor to crush the the can, it does not decrease the amount of work required to crush the can(work = force x displacement) because the displacement has been increased to compensate for a lower force. I love your outside the box thinking but effectively you have built a "force modifier device" such as a gearbox or lever.