Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Blog Win a Raspberry Pi Media Center Kit - Winners Announced!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: element14Dave
  • Date Created: 14 May 2015 7:15 PM Date Created
  • Views 8882 views
  • Likes 8 likes
  • Comments 533 comments
  • past_contest
Related
Recommended

Win a Raspberry Pi Media Center Kit - Winners Announced!

element14Dave
element14Dave
14 May 2015

image

Ben Heck Home Page
Top 10 Builds of 2014
View All Episodes

 

 

Follow the instructions below and win! Terms and Conditions apply, see attached.



You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 


We're giving away 10 Rapsberry Pi Media Kits!


Kit includes:

1 Raspberry Pi Model B

1 Raspberry Pi branded case (black)

1 8 GB microSD card with Raspberry Pi branded adapter

 


Directions:


The winners are:

 

161915 gcorwin jwzumwalt viscount

AJKools sjames1958 publishedmeteor

rockinricky ufgatorsdm straitedge


I have sent the winners an email with further instruction. Let me know if you did not receive the message.



Step 1: Log in or register on element14, it's easy and free.

 

Step 2: In the comments section below, post what you would do with the kit or why you should be selected to receive the kit. Videos, pictures and  text are all welcomed forms of submission.

 

Step 3: Sit back, relax, and enjoy the show!  We will accept entries until 3:00pm CST  June 5, 2015  and announce our winners on June 9, 2015. If you need something to do between now and then make sure to check out what is happening This week on element14 Community.


Want to watch episodes of The Ben Heck Show on your Raspberry Pi? Learn How

 

 

Important Notice:

    By submitting an entry you will automatically start receiving notifications of other responses to this post. If you do not wish to receive notifications, select "Unfollow" at the top right of the post. If you have any questions, please let us know in our Feedback & Support area.


Terms and Conditions are Attached

Attachments:
imageTerms and Conditions_Media Center Giveaway_Ben Heck.pdf
  • Sign in to reply

Top Comments

  • clem57
    clem57 over 11 years ago +2
    I would like to win this to start builing a Raspberry Pi cluster! Go Super Pi <grin>
  • freddruppel
    freddruppel over 11 years ago +1
    I'd use this kit to learn linux, tinker around with the GPIO possibilities and, when I have enough knowledge to know what I'm doing, make a portable Raspberry Pi Linux computer !
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    I Would use this in my main tv since my current Media center takes up a lot of space , I used a lot of scrap parts to put this "half a laptop" together
  • e14 Contributor
    e14 Contributor over 11 years ago

    I would use it to experiment with cluster computing with mixtures of processor architectures.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    I would create a raspberry pi umpc. I would make a slide out keyboard and install a touchscreen. It would be wifi and bluetooth capable. It would have built in speakers and a headphone jack, as well as ported out hdmi. It would also as the name implies be ultra mobile.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wdfreemanjr
    wdfreemanjr over 11 years ago

    My project would be to complete my automated Tilapia Aeroponics System. It is a  90 sq/ft shed that contains 2 300 gallon fish tanks, a 192 sq/ft greenhouse and it completely powered by a 1440 watt solar system in a residential area the middle of a large city.

     

    A major benefit is that I have created a close-loop system wherein the dirty fish water is used to water and fertilize the vegetables in my greenhouse. The vegetables remove the excess nitrites/nitrates from the water which is then returned back to the fish tank cleansed. 


    A Wi-Fi fob sends/receives video/data from the PI to a local web server which then serves a web page that runs on any browser or smart phone anywhere in the world.  The web server can send/receive HTML/text messages/emails to alert me of critical situations or major changes in conditions.


    I started with a PI+A from a friend and in only two weeks, I am able to stream live video (USB Camera), monitor water temperature and turn on/off two relays. I use the camera to monitor the the fish, visually check for leaks/flooding and check the status of an LED panel to confirm that certain activities are in working. (It is primitive for feedback, but it works for now). I was able to quickly connect 2 GPIO wires to an Arduino for additional processing, distributed monitoring, sensing, A/D conversion and additional GPIO pins.

     

    If I am selected, I will use my PI+B to add additional cameras for inside the fish tanks, automate feeding, monitor water levels, internal/external ambient temperature, PH and O2 levels, as well as control inside lights, heater, air conditioner and solar panel output. 

     

    This project fascinates me due to the current drought conditions in California. This is a closed loop system that uses less than 60 gallons of water/month for the fish and the water usage for growing all of the vegetables is roughly 3%-6% of standard agricultural practices.


    I achieved all of this using a Raspberry PI and a few sensors all on a quarter acre lot.  I am no mathematician, but I know that 3%-6% of water consumption is the type of water savings California could use right now.

     

    Thank you for your consideration,

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bonitobird
    bonitobird over 11 years ago

    I would learn how to code computers (and maybe watch some stuff also). image I can't wait to get a Raspberry Pi and get started.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • samej71
    samej71 over 11 years ago

    I would really like to use it as a low-power/green hub for a smart home, being the gateway and primary decision maker when talking with smaller interactive units, such as Digistump Oaks andor some arduino-compatibles over the network. While this giveaway is media-centric, and it is certainly a common use for the Raspberry Pi, the case and memory card are essential for protecting and using the Pi, no matter what it is being used for. That said, it is also quite possible that it may perform smart-house duties in the background while acting as a media center. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>