Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Arduino controlled metal forge.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 42 subscribers
  • Views 527 views
  • Users 0 members are here
  • arduino
Related

Arduino controlled metal forge.

e14 Contributor
e14 Contributor over 10 years ago

I would like to see a ramped up micro controlled version of this metal smelter. It is a duel fuel setup which starts out with propane and after warming up converts over to waste oil. There are several things that could be automated or just monitored.

 

Monitoring:

Heat temp inside (very handy when dealing with different types of metal and saving fuel)

 

Air fuel mix (maybe a old sensor from a waste oil burner could do this)

 

Fan speed (There not only is a compressed air line running the burner for the waste oil suction but also a extra air source to help with the fuel mix)

 

Automation:

This could be setup to run off its own power using a thermoelectric generator and a startup battery.

 

Automatic fuel cut over: The propane side  is only to warm up the body of the torch and if you could monitor the temp of the torch (separate from the internal temp of the smelter) after it reaches operating temp it could shut off a valve and open the oil valve.

 

In a very advanced version with lots of research it could be setup to control the air/fuel mix. This could vary based of which fuel you want to monitor since the propane would mix differently than the oil. But since the oil is going to be the primary fuel during the melting process they I believe it would be the preferred choice.

 

Thanks for your time I know this is a little different than what the channel usually works with but maybe you could think of a way to incorporate the control side of this into something else without making it just for a metal forge.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +1
    I sorta made a low temp version of a automated metal melting/pouring machine: https://plus.google.com/+MarkMillerstuff/posts/TDiARuw6tha
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    I sorta made a low temp version of a automated metal melting/pouring machine:

    https://plus.google.com/+MarkMillerstuff/posts/TDiARuw6tha

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    I sorta made a low temp version of a automated metal melting/pouring machine:

    https://plus.google.com/+MarkMillerstuff/posts/TDiARuw6tha