Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Engine Management
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 48 subscribers
  • Views 6579 views
  • Users 0 members are here
Related

Engine Management

jack.chaney56
jack.chaney56 over 10 years ago

Hi Ben,

I am a programmer with a very small amount of skill with circuits, and am looking to create a platform for an engine management system, using an Arduino Mega 2560. I had done a bit of the coding, when I ran into some timing issues with the built in Arduino manager, so I switched over and started using AVR Studio and a programmer to go directly to the chip itself.  The code looks like it should work ok, but now I need some additional circuits to handle the energy levels of coils and injectors (Something like IGBTs). Sensors are being run through simple dividers (no protection yet), and cam and crank inputs are through a simple comparitor

 

Let me know what you think,

Jack

  • Sign in to reply
  • Cancel

Top Replies

  • jack.chaney56
    jack.chaney56 over 8 years ago +2
    Back again... After a bit of time away seeking enlightenment (and a steady paycheck), I am ready to get back to work on my project. I have continued to play around with the code and a number of components…
  • jack.chaney56
    jack.chaney56 over 8 years ago +2
    I want to start this thing right, so the shopping list for people that want to play along at home: Raspberry Pi - version is not significant if you don't mind a slow response when using Eclipse, but 3B…
  • jack.chaney56
    jack.chaney56 over 8 years ago +2
    Start off with two things. First, I forgot (neglected) to provide instruction on how to get the compiled code onto the Nano. Fault of familiarity; having done the process so many times, I had shifted to…
Parents
  • jack.chaney56
    jack.chaney56 over 8 years ago

    Back again...

    After a bit of time away seeking enlightenment (and a steady paycheck), I am ready to get back to work on my project. I have continued to play around with the code and a number of components. First, I wanted to have a more interesting development workstation, so I thought it would be fun to use a Raspberry Pi. After installing the latest version of Raspbian and getting all the updates, I loaded the AVR tool set, then Eclipse and the C/C++ components. Then adding the AVR plugin and whoopee I had a workstation.

     

    I also really wanted to use the Nano for a platform but had problems with adding controls for 8 cylinder coil on plug and still be able to have outputs for solenoids and idiot lights (shift, MIL, etc). Then I thought of using 4 of the port lines to control a 74LS138 and using a bunch of 74LS75s and some inverters, route the other 4 port lines available to create a multiplexed switch network. Got it to light LEDs and the scope signals look right too.  The last part of the puzzle for the Nano was since the 328p is limited for timers, I got inventive for some of the timing pieces (fueling is less time critical).

     

    So I created a dual path, with the majority of software files being shared between both platforms, only when hardware forces there to be a difference, the same code runs on both Mega2560 and Nano.  I will attempt to provide all the how-to for the development workstation, the Nano setup and programming, and source code with design theory.

     

    Since much stuff has been refined over the course of time, I will probably be redoing a bunch of stuff and there will probably be a bunch of  repeat.  For anyone interested, it is possible to get a big dose of what is to follow by looking over the early work at Engine Management project

     

    I am now in the throws of developing the UI to provide the calibration in a more comfortable way. Again, trying to stay with using a Raspberry Pi as the UI platform too.

     

    Jack

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 8 years ago in reply to jack.chaney56

    Hi Jack,

     

    I've just come into this thread but see it is over two years old and someone initially told you it couldn't be done....well my philosophy in life is that if someone else managed to make X in the past then it should be possible to make one myself (sometimes this doesn't work due to limited finances, time, materials, legality or equipment; but in theory nothing should hold you back).

     

    Look forward to your updates now you are back on track.

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • 14rhb
    14rhb over 8 years ago in reply to jack.chaney56

    Hi Jack,

     

    I've just come into this thread but see it is over two years old and someone initially told you it couldn't be done....well my philosophy in life is that if someone else managed to make X in the past then it should be possible to make one myself (sometimes this doesn't work due to limited finances, time, materials, legality or equipment; but in theory nothing should hold you back).

     

    Look forward to your updates now you are back on track.

     

    Rod