Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Engine Management
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 48 subscribers
  • Views 6569 views
  • Users 0 members are here
Related

Engine Management

jack.chaney56
jack.chaney56 over 10 years ago

Hi Ben,

I am a programmer with a very small amount of skill with circuits, and am looking to create a platform for an engine management system, using an Arduino Mega 2560. I had done a bit of the coding, when I ran into some timing issues with the built in Arduino manager, so I switched over and started using AVR Studio and a programmer to go directly to the chip itself.  The code looks like it should work ok, but now I need some additional circuits to handle the energy levels of coils and injectors (Something like IGBTs). Sensors are being run through simple dividers (no protection yet), and cam and crank inputs are through a simple comparitor

 

Let me know what you think,

Jack

  • Sign in to reply
  • Cancel

Top Replies

  • jack.chaney56
    jack.chaney56 over 8 years ago +2
    Back again... After a bit of time away seeking enlightenment (and a steady paycheck), I am ready to get back to work on my project. I have continued to play around with the code and a number of components…
  • jack.chaney56
    jack.chaney56 over 8 years ago +2
    I want to start this thing right, so the shopping list for people that want to play along at home: Raspberry Pi - version is not significant if you don't mind a slow response when using Eclipse, but 3B…
  • jack.chaney56
    jack.chaney56 over 8 years ago +2
    Start off with two things. First, I forgot (neglected) to provide instruction on how to get the compiled code onto the Nano. Fault of familiarity; having done the process so many times, I had shifted to…
Parents
  • jack.chaney56
    jack.chaney56 over 10 years ago

    Additional information...

    I can provide a bit of background on engine management strategy, and what goes into making of engine controller code. The timing operations, and what needs to happen when. How to work with single coil or coil on plug. Using normally aspirated, throttle body or direct injection of fuel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jack.chaney56
    jack.chaney56 over 10 years ago

    Additional information...

    I can provide a bit of background on engine management strategy, and what goes into making of engine controller code. The timing operations, and what needs to happen when. How to work with single coil or coil on plug. Using normally aspirated, throttle body or direct injection of fuel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to jack.chaney56

    Dear me, The gauntlet has been dropped. I was telling a friend about my idea and what I was using, and got the response I was hoping to hear. He was telling a third party that does work for a "major auto manufacturer" and was told the idea it was preposterous, and it would never work.

     

    So now I have a problem, what do I do with code that can take input from potentiometers acting as MAP, ECT, and IAT, and simulated cam (single pulse, half moon, VVT, and Mopar 4,6, and 8) and crank signals (4x to 60-2), and provides timing for up to 8 cylinders (single, dual, or coil on plug) from 150 up to 10000RPM using an Arduino Nano.  Unless, he thought I needed more hardware, like IGBTs or a CD charge pump or something, because I do need that part.  But from what I got from my friend, the third party didn't think the Nano was up to the task. We shall see.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to jack.chaney56

    Jack keep updating us on your interesting work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to e14 Contributor

    Hi Gary,

    Thank you for the encouragement. I will be publishing a short series in the documents section that covers elements of engine management. The current engine controllers use a "just in time" kind of methodology, which sometimes has to play catch up, and can get a little confused. My method operates off a different process, what messed up a friend was when I said my process can use a 4x wheel to run a 6 cylinder motor, as long as I can detect TDC0, everything else is just more detail.

     

    Jack.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to e14 Contributor

    Hi Gary,

    I posted the start of my first article, for lack of a better location, in the Arduino section.  I used a Mega 2560 for my initial platform.

     

    Jack

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to jack.chaney56

    Hello Jack,

     

    I can't find that article - can you give us a link.

     

    It's  a long time since I worked on automotive and even then it was never directly on engine management although controllers I built had to talk to engine management systems and I haven't totally lost touch.  There is no way an Arduino nano can replicate current, legislation compliant, engine management systems - since not only do you need to control the engine and emissions (or fake it like VW) but you need to detect and log misfires and faults. The tiny processor in the nano doesn't have enough ROM for a basic map and certainly doesn't have the processing power to calculate it on the fly.

     

    You might be able to replicate a traditional distributor and centrifugal advance system with a nano - but why bother ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to michaelkellett

    Hi Michael,

    The article is still in draft status, which requires me to add you to the list of collaborators. I should have that today. If I run into any problems, I will be contacting you.

     

    Jack