Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Build Idea: A soldering iron that extrudes it's own solder
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 45 subscribers
  • Views 1598 views
  • Users 0 members are here
  • build
  • suggested
Related

Build Idea: A soldering iron that extrudes it's own solder

e14 Contributor
e14 Contributor over 11 years ago

The lack of extra hands is always very frustrating when soldering. Wouldn't it be nice if the soldering iron could extrude solder like the hot end of a 3d printer? You'd press a button on the iron and a small amount of solder would be extruded out of the tip. You'd gain an entire extra hand! Would love to see you guys tackle this idea :-)

 

Eli V.

  • Sign in to reply
  • Cancel

Top Replies

  • Problemchild
    Problemchild over 11 years ago in reply to mcb1 +2
    Yeah I had a go with a feeder mechanism once and I found it much harder than to feed it through manually because you can control the feed and angle manually and it's always right when you practice
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +1
    Yes I know, like this: http://www.cybermarket.co.uk/shop/tools/soldering-irons-stations/soldering-gun-with-automatic-497690.html?utm_source=google&utm_medium=base&utm_campaign=H7Media&gclid=CjwKEAiAh7WkBRCQj…
  • jw0752
    jw0752 over 11 years ago +1
    Hi Eli, Part of the problem would be retention of the flux that is inherent in the solder. If the solder was preheated and pumped through the tip this flux would not be where and when it is needed. I do…
Parents
  • michaelkellett
    michaelkellett over 11 years ago

    This isn't  a new idea - I think there was a post about such a thing on E14 a couple of years ago.

    There is some information here:

     

    http://www.solidsmack.com/design/solder-buddy-keeps-the-hot-solder-aflowin/

     

    And of course you can buy an iron with a built in feeder for £14.94.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelkellett

    Hi Michael,

    Thanks for your reply. I've looked at your link, and while that's a handy tool, it's not what I'm describing. The link you posted would still require you to use your second hand to hold the solder. What I'm referring to is that the solder iron ITSELF is the extruder, so that the solder feeds into the hot tip of the iron thereby freeing up your left hand.

    Eli V.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor

    Yes I know, like this:

    http://www.cybermarket.co.uk/shop/tools/soldering-irons-stations/soldering-gun-with-automatic-497690.html?utm_source=google&utm_medium=base&utm_campaign=H7Media&gclid=CjwKEAiAh7WkBRCQj-_zwZvk52ISJADj7z8C-13TyIV83t1Fv1JSaJSDKZT7IubNtqeWxjMFSnfkXBoCOnDw_wcB

     

    Just use some clips, wire, whatever to fix the solder buddy to the standard iron.

     

    I'll mention, in passing, that I've been soldering for slightly over 50 years and never felt the need for such a thing !

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor

    Yes I know, like this:

    http://www.cybermarket.co.uk/shop/tools/soldering-irons-stations/soldering-gun-with-automatic-497690.html?utm_source=google&utm_medium=base&utm_campaign=H7Media&gclid=CjwKEAiAh7WkBRCQj-_zwZvk52ISJADj7z8C-13TyIV83t1Fv1JSaJSDKZT7IubNtqeWxjMFSnfkXBoCOnDw_wcB

     

    Just use some clips, wire, whatever to fix the solder buddy to the standard iron.

     

    I'll mention, in passing, that I've been soldering for slightly over 50 years and never felt the need for such a thing !

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelkellett

    oh, i see now. Looks a little clunky to really use comfortably. I guess this is more about convenience than necessity anyway!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to michaelkellett

    I'll mention, in passing, that I've been soldering for slightly over 50 years and never felt the need for such a thing !

    Not quite the same time, but after 40 or so years I've become very handy at holding the solder and the part as well.

     

     

    I wonder if the issue you are trying to solve is more to do with technique.

    Lately I've been teaching pupils to solder and they can make it very awkward for themselves, which makes it very hard, and once shown a good technique improve and relax much more.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to mcb1

    Yeah I had a go  with a feeder mechanism once and I found it much harder than to feed it through manually because you can control the feed and angle manually and it's always right when you practice