Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Current limitting power supply
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 42 subscribers
  • Views 325 views
  • Users 0 members are here
Related

Current limitting power supply

e14 Contributor
e14 Contributor over 11 years ago

I think it would be useful to have a power supply with variable voltage and current control for many projects. Also a readout of actual consumed current so you can tell if the limit is being used. It would allow the experimentation of circuits without as much risk of accidental over current. This would also be useful for charging batteries, but I would think additional circuitry would be needed to prevent overcharging.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    I use a Thurlby PL310 which has both voltage and current limiting and produce up to 30V at 1A, with digital readouts. You set the voltage/current with the unit output switched off and then if you overload the output when switched on the display flashes. You are also able to set up a virtual earth (0V) to have dual based supply as well. If I remember rightly it cost me about £100 a few years back and has proved to good.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    I use a Thurlby PL310 which has both voltage and current limiting and produce up to 30V at 1A, with digital readouts. You set the voltage/current with the unit output switched off and then if you overload the output when switched on the display flashes. You are also able to set up a virtual earth (0V) to have dual based supply as well. If I remember rightly it cost me about £100 a few years back and has proved to good.