Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Arduino powered system for electric guitar pickup selection.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 45 subscribers
  • Views 3322 views
  • Users 0 members are here
  • arduino
Related

Arduino powered system for electric guitar pickup selection.

QuantumAberrant
QuantumAberrant over 11 years ago

Electric guitars uses switches to select which pickups are activated at a time. Most designs though do not allow for all possible combinations of pickups. Also there are alternative ways of wiring a guitar, series/parallel wiring changes the tone. Also reversing the phase (polarity) gives you other sounds. Almost no guitar gives the option of selecting all of these options because the wiring becomes too complex. I would like to challenge Ben to create a system by which an Arduino can be used to select any of the different combinations.

 

Here are the wiring diagrams to give you a idea.

 

Series/parallel switching.

http://www.premierguitar.com/articles/Adding_Series_Switching_To_Your_Strat

 

In-Pase./out of phase

Wiring Diagram

 

Current mods to help add pickup combinations include:

 

Wiring Diagram

 

If you put all these ideas together you get something like what Brian May from Queen built. http://www.premierguitar.com/articles/21307-mod-garage-inside-brian-mays-red-special

 

Still there is more, pickups with two coils, called "humbuckers" can be "coil tapped" to be single coils, making one more set of switches one might want.

 

I have a Music Man 'Steve Morse' guitar. http://www.music-man.com/instruments/guitars/steve-morse.html

 

It has 4 pickups, and switching between them is crazy complicated all by itself. Here is the diagram: http://imgur.com/r5As604

 

Finally another guitar mod is know as a 'kill switch'. It's basically just a momentary button used to cut the signal to the amplifier, but when used by people like buckethead uses https://www.youtube.com/watch?v=NM8DuJKYlqE

A micro-controller would automate a killswitch and have lots of selectable patterns.

 

Can you help me Ben? Can all of this be built on to one circuit board controlled by a microcontroller? Possibly even with an LCD display that indicates what mode it's in?

  • Sign in to reply
  • Cancel

Top Replies

  • mayermakes
    mayermakes over 11 years ago +1
    its actually not that hard to do without any mcu Here is the DEIMOS CIV a guitar i have built myself about 6-8 years ago: 3 Pickups (2x Humbuckers) every combination possible is selectable, cut of switch…
  • QuantumAberrant
    QuantumAberrant over 11 years ago in reply to mayermakes +1
    That's a cool guitar but I think you vastly underestimate the space those wires takes up. As an example here is a circuit board used in modern Gibson guitars for volume and tone control. http://s1150.photobucket…
Parents
  • mayermakes
    mayermakes over 11 years ago

    its actually not that hard to do without any mcu

    Here is the DEIMOS CIV a guitar i have built myself about 6-8 years ago:

    3 Pickups (2x Humbuckers) every combination possible is selectable, cut of switch / out of phase/ single coil selectable for every combination.

    its complex wiring but mangable , here is my build:

     

    image

    notice REAL COW HORNS!!

    image

    The skulls are knobs for Volume and Tone for the selected pickup combination

     

    image

    it was a pretty tough fit inside the existing caverns of the guitar

     

    my concernes with the arduino-version:

     

    a mcu circuit could give you issues with interference, noise etc. there is also nearly no room for additional circuitry without cut opening the solid body-->may ruin the sound and give vibrating issues to the body itself.

    its overkill to run all the wires out to stomp-boxes and then to the amp(but possible) but this will / may create signal drop and even more noise. with active preamp and then messing around with the signal via arduino etc.. would be no different pickup selection but just a homemade effect box.

     

    greetings!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mayermakes
    mayermakes over 11 years ago

    its actually not that hard to do without any mcu

    Here is the DEIMOS CIV a guitar i have built myself about 6-8 years ago:

    3 Pickups (2x Humbuckers) every combination possible is selectable, cut of switch / out of phase/ single coil selectable for every combination.

    its complex wiring but mangable , here is my build:

     

    image

    notice REAL COW HORNS!!

    image

    The skulls are knobs for Volume and Tone for the selected pickup combination

     

    image

    it was a pretty tough fit inside the existing caverns of the guitar

     

    my concernes with the arduino-version:

     

    a mcu circuit could give you issues with interference, noise etc. there is also nearly no room for additional circuitry without cut opening the solid body-->may ruin the sound and give vibrating issues to the body itself.

    its overkill to run all the wires out to stomp-boxes and then to the amp(but possible) but this will / may create signal drop and even more noise. with active preamp and then messing around with the signal via arduino etc.. would be no different pickup selection but just a homemade effect box.

     

    greetings!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • QuantumAberrant
    QuantumAberrant over 11 years ago in reply to mayermakes

    That's a cool guitar but I think you vastly underestimate the space those wires takes up. As an example here is a circuit board used in modern Gibson guitars for volume and tone control.

     

    http://s1150.photobucket.com/user/vonserke/media/pcb_top.jpg.html

     

    It looks to me like there is room enough for at least an ATtiny85, and that's the hole through version. I bet with surface mount you could cram an entire ATMEGA32U4 or AT90USB1286 in there. The MCUs would not be processing the signal, just routing it from place to place probably using transistors or FETs or relays or something. Honestly, switches can be very noisy, which is why players tend not to play with them in the middle of a song. I think a transistor can be at least as quiet as a regular switch. It's possible that my dreams of a PWM controlled kill switch might be too much but believe the rest is possible and valuable.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 11 years ago in reply to QuantumAberrant

    this might work , but i think the signal will be corrupted by transistors and so on..there are concerns of musicians about using different WIRE than the original because of different resistance altering sound quality.

    there are people measuring the EXACT capacitance of replacement capacitators to match the original and then shout out to the world how they have been ripped off by soemone who sold them a 47nF Cap but it doesn´t sound like "the 47nF" before.

    I´have peronaly experimented with different parts in my guitars, now I think the best signal is the one with the less influence.

    But I hope you prove me wrong and build an awesome axe.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • QuantumAberrant
    QuantumAberrant over 11 years ago in reply to mayermakes

    I agree that there is plenty of superstition around guitars and a lack of scientific evidence around what actually makes something sound good. Thanks for the support. image I hope Ben can help me.