Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Unified Power Supply for PC and display
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 45 subscribers
  • Views 731 views
  • Users 0 members are here
  • Accessibility
Related

Unified Power Supply for PC and display

scorp8669
scorp8669 over 11 years ago

Hi Ben,

 

On my table there is a BRIX PC, a Display and a NAS. For each of them their own Power Supply and my work space if filled with them. Is there any way to make (or mod an ATX PSU) a PSU for all my devices?

I need an output of 19V 3.42A for PC, 19.5V 3.34A for Display, 12V 3A for NAS. An couple of additional USB ports for charging would be just great.

 

Thanks.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    So what you basically need is 20V at about 10A -15A power supply, 8A for the 19/20V and the rest for the 12V via a buck convertor from the 19/20 to 12V they can all share a common ground from what I am…
Parents
  • kidiccurus
    kidiccurus over 11 years ago

    Most atx PSUs only go up to 12v volts, so unless you use a boost regulator, ATX is out. Instead I recommend using a higher voltage supply (20v+) and several, seperate switching voltage regulators to reduce the voltage as appropriate for your various devices. USB could be obtained with a 5v regulator, plus's a few resistors to ensure fast charging works properly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scorp8669
    scorp8669 over 11 years ago in reply to kidiccurus

    I've seen on eBay a Step-down Power Converter Module such as this one: http://www.ebay.com/itm/LM2596-Buck-Step-down-Power-Converter-Module-DC-4-0-40-to-1-3-37V-LED-Voltmeter/400802470941

    I need something similar with 3.5A output that is going to be regulated independently and have an AC input and DC output.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scorp8669
    scorp8669 over 11 years ago in reply to kidiccurus

    I've seen on eBay a Step-down Power Converter Module such as this one: http://www.ebay.com/itm/LM2596-Buck-Step-down-Power-Converter-Module-DC-4-0-40-to-1-3-37V-LED-Voltmeter/400802470941

    I need something similar with 3.5A output that is going to be regulated independently and have an AC input and DC output.