Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum 3D Printer, CNC, Lasercutter All in one
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 44 subscribers
  • Views 930 views
  • Users 0 members are here
  • printer
  • 3d
  • build
  • cutter
  • cnc
  • heck
  • ben
  • laser
Related

3D Printer, CNC, Lasercutter All in one

e14 Contributor
e14 Contributor over 12 years ago

I want to be able to build an All in one machine to be able to 3d print, mill, and maybe laser cut (but its not 100% needed since the cnc can do most of the work). I have use for all 3 so I thought why not combine them?

I was thinking it would have interchangeable head pieces that would move on the XY axis and the base would move on the Z axis. I was thinking of making it big, something with a print/work area of about 50x50 cm (thats all I need anyway) and at that size it should still be small enough to not cause a big problem with its own weight). The base plate could also be interchangeable depending on the job.

It would have to be able to switch the type of job with buttons that change the commands in the boards automatically and maybe have some kind of safety so it doesn't work if for example the router head is on but the 3d printer plate is still attached.

 

My main problem would be how i'm going to setup the boards and the software, If I could use the same boards for the different jobs, how to program the software and calibrate it so it can work properly, how to get the cnc to start from the top not the bottom and basically work inverted etc etc. I'm a quick learner but iv'e never tried an electronic project like this before so I'm totally lost.

 

Would Ben be able to take a crack at it?

  • Sign in to reply
  • Cancel

Top Replies

  • turfgnome
    turfgnome over 12 years ago +1
    As with Samuel Doye said you have speed issues but you would also have a lot of quality control issues with a combo unit the dust from the router would play havoc with the 3d printer. The best combo for…
Parents
  • vd0gg1t
    0 vd0gg1t over 12 years ago

    to Samuel Doye's speed/torque point, would a two motor solution seem plausible?

    The old fashioned dental drills had high speed motors off to the side with cable link to the actual drill head. Then just employ a typical router motor setup for the high torque.


    Additional thoughts:

    Multi head: Drill/Router/Laser/Extruder: Microscope Lens. control the lens in use by rotating whole lens ensemble with the correct lens being directly inline and the other lens angled off and out of the way. Same idea to choose the proper head/extruder.

    image


    Laser: Ben's uses mirrors to transmit the laser light but if line of sight issues arise with the complexity of the various drill/laser/router/extruder heads could a fiber optic cable be employed to transmit the laser beam to the cutting source?


    cable harness: create a harness for the drill cables, the filament, and the fiber optics. (one for the laser, one for data)

     

    Carriage for Z travel: while keeping the board/printing surface (z plane) flat, attach a vertical carriage to the x and y control system and the drill/router/extruder to the vertical carriage system.

     

    ps. couldn't you have the laser 'melt' the filament for extrusion and also 'cut' supports off prints (post production)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vd0gg1t
    0 vd0gg1t over 12 years ago

    to Samuel Doye's speed/torque point, would a two motor solution seem plausible?

    The old fashioned dental drills had high speed motors off to the side with cable link to the actual drill head. Then just employ a typical router motor setup for the high torque.


    Additional thoughts:

    Multi head: Drill/Router/Laser/Extruder: Microscope Lens. control the lens in use by rotating whole lens ensemble with the correct lens being directly inline and the other lens angled off and out of the way. Same idea to choose the proper head/extruder.

    image


    Laser: Ben's uses mirrors to transmit the laser light but if line of sight issues arise with the complexity of the various drill/laser/router/extruder heads could a fiber optic cable be employed to transmit the laser beam to the cutting source?


    cable harness: create a harness for the drill cables, the filament, and the fiber optics. (one for the laser, one for data)

     

    Carriage for Z travel: while keeping the board/printing surface (z plane) flat, attach a vertical carriage to the x and y control system and the drill/router/extruder to the vertical carriage system.

     

    ps. couldn't you have the laser 'melt' the filament for extrusion and also 'cut' supports off prints (post production)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • kidiccurus
    0 kidiccurus over 12 years ago in reply to vd0gg1t

    Sorry but the speed is partly decided by the configuration for moving the head. A belt system gives speed and a screw system torque. The two can't be implemented on one machine. It would also be better to use a full extruder for safety and accuracy reasons. This idea comes up on the forums from time to time and I have yet to see a working solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vd0gg1t
    0 vd0gg1t over 12 years ago in reply to kidiccurus

    Hmm, quick change head function of the CEL Rebox RoadTest sounds interesting...

    http://www.element14.com/community/roadTests/1354?ICID=hp-3droboxrt-ban