Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum 3D Printer, CNC, Lasercutter All in one
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 44 subscribers
  • Views 930 views
  • Users 0 members are here
  • printer
  • 3d
  • build
  • cutter
  • cnc
  • heck
  • ben
  • laser
Related

3D Printer, CNC, Lasercutter All in one

e14 Contributor
e14 Contributor over 12 years ago

I want to be able to build an All in one machine to be able to 3d print, mill, and maybe laser cut (but its not 100% needed since the cnc can do most of the work). I have use for all 3 so I thought why not combine them?

I was thinking it would have interchangeable head pieces that would move on the XY axis and the base would move on the Z axis. I was thinking of making it big, something with a print/work area of about 50x50 cm (thats all I need anyway) and at that size it should still be small enough to not cause a big problem with its own weight). The base plate could also be interchangeable depending on the job.

It would have to be able to switch the type of job with buttons that change the commands in the boards automatically and maybe have some kind of safety so it doesn't work if for example the router head is on but the 3d printer plate is still attached.

 

My main problem would be how i'm going to setup the boards and the software, If I could use the same boards for the different jobs, how to program the software and calibrate it so it can work properly, how to get the cnc to start from the top not the bottom and basically work inverted etc etc. I'm a quick learner but iv'e never tried an electronic project like this before so I'm totally lost.

 

Would Ben be able to take a crack at it?

  • Sign in to reply
  • Cancel

Top Replies

  • turfgnome
    turfgnome over 12 years ago +1
    As with Samuel Doye said you have speed issues but you would also have a lot of quality control issues with a combo unit the dust from the router would play havoc with the 3d printer. The best combo for…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    TThere are a few of these on the market presently. The best and most affordable (meaning didn't sacrifice quality or integrity and is reasonably priced) in my opinion would be. boXZY

    CHECK IT OUT www.boxzy.com

    its a 3d printer, laser cutter, and CNC milling machine

     

    for $1999 you get to choose 2 out of 3 options

    Hardened Steel and Billet Aluminum form together to create the BoXZY Pick 2 Package! BoXZY Pick 2 includes everything you need to use 2 of BoXZY's amazing quick-change functionality: Pick from the The CNC Milling head, 3D printing head, or Laser Engraving head and add them to a ready to run fully assembled BoXZY CNC. This machine can mill an aluminum piston, Laser engrave a raw block of maple, or 3D print impossible shapes. Black Anodized finish. Includes BoXZY and 2 heads from these 3 choices: The CNC Milling head, 3D printing head, or Laser Engraving head


    THe he next option is $2900


    and the supreme deal is $3500

    When hardened steel and aluminum come together it's a great paring, add a large list of accessories and you have everything you need to utilize a machine to its full potential. BoXZY Supreme includes everything you need to use all 3 of BoXZY's amazing quick-change functionality: The CNC Milling head, 3D printing head, and Laser Engraving head come wrapped up with a ready to run fully assembled BoXZY CNC. This machine can mill an aluminum piston, Laser engrave a raw block of maple, or 3D print impossible shapes. But this BoXZY doesn't stop there. Check out the added list of accessories below, because it's impressive!

    • Magnetic enclosure panels (laser blocking, heat and debris trapping)
    • High grade carbide end mill set
    • Carbide Engraving bit set
    • Full clamp and jig set
    • 3 full rolls of colored filament (1kg each)
    • BoXZY tool kit

     

    I Don't work for the company but noticed this on kickstarted and got in when things were a little bit Cheaper. Delivery is scheduled for December of 2015. Hope this helps!!


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    TThere are a few of these on the market presently. The best and most affordable (meaning didn't sacrifice quality or integrity and is reasonably priced) in my opinion would be. boXZY

    CHECK IT OUT www.boxzy.com

    its a 3d printer, laser cutter, and CNC milling machine

     

    for $1999 you get to choose 2 out of 3 options

    Hardened Steel and Billet Aluminum form together to create the BoXZY Pick 2 Package! BoXZY Pick 2 includes everything you need to use 2 of BoXZY's amazing quick-change functionality: Pick from the The CNC Milling head, 3D printing head, or Laser Engraving head and add them to a ready to run fully assembled BoXZY CNC. This machine can mill an aluminum piston, Laser engrave a raw block of maple, or 3D print impossible shapes. Black Anodized finish. Includes BoXZY and 2 heads from these 3 choices: The CNC Milling head, 3D printing head, or Laser Engraving head


    THe he next option is $2900


    and the supreme deal is $3500

    When hardened steel and aluminum come together it's a great paring, add a large list of accessories and you have everything you need to utilize a machine to its full potential. BoXZY Supreme includes everything you need to use all 3 of BoXZY's amazing quick-change functionality: The CNC Milling head, 3D printing head, and Laser Engraving head come wrapped up with a ready to run fully assembled BoXZY CNC. This machine can mill an aluminum piston, Laser engrave a raw block of maple, or 3D print impossible shapes. But this BoXZY doesn't stop there. Check out the added list of accessories below, because it's impressive!

    • Magnetic enclosure panels (laser blocking, heat and debris trapping)
    • High grade carbide end mill set
    • Carbide Engraving bit set
    • Full clamp and jig set
    • 3 full rolls of colored filament (1kg each)
    • BoXZY tool kit

     

    I Don't work for the company but noticed this on kickstarted and got in when things were a little bit Cheaper. Delivery is scheduled for December of 2015. Hope this helps!!