Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum How to modify a set top DVD/Blu Ray player for 12V operation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 45 subscribers
  • Views 1372 views
  • Users 0 members are here
  • Portables
Related

How to modify a set top DVD/Blu Ray player for 12V operation

jaevans
jaevans over 10 years ago

That should say it all.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +2
    Do you have a schematic or datasheet for your DVD? Clem
  • william_hoffer
    william_hoffer over 10 years ago +1
    no it isn't, there are the questions like, why? I can buy a car dvd player with double screens for 89 dollars or 39 dollars for a dvd player and tv. So why try to convert a regulars dvd player to a vehicle…
  • jw0752
    jw0752 over 10 years ago in reply to jaevans +1
    From what I can see this is a quite simple SMPS and only has a single voltage output of 12 volts. If there is further voltage conversion being done it is on the other boards and probably as needed to power…
Parents
  • sunny94
    sunny94 over 9 years ago

    They are DVD systems that haven't been made with a GPS navigation system. Two groups can be found: The Gps navigation and also the no- GPS car DVD. They however produce other features the happen to be made with Bluetooth support.  This selection enables you to hear music and you may also receive calls.  The machine also has a radio and   music player. If you're searching for any more complex system, then your GPS DVD player may be the best brand out there.  It's been made with a GPS navigation feature along with a map.  Additionally, it arrives with a Bluetooth, radio receiver, stereo, and subwoofer, 3G Internet along with a USB and SD input.

     

     

    The motto of EinCar is Expert In Car electronics. Also, Eincar sells only top quality stuffs with global standards. Every EinCar’s goods are always reviewed by our experienced Qc team with proffessional rules. Under its strict tests and qc procedure, it's worldwide standards both in quality and safety.

     

     

    If you wish to reverse your vehicle from a automobile parking space, the thought of using of the car backup camera is a terrific way to make certain that you don't mistakenly hit anything. If you are using the interior mirror, they're most occasions not efficient particularly if you drive a truck or perhaps an Sports utility vehicle. These units are often available on greater finish models as well as, it is simple to have them in a retail store at significant prices. These cameras work by mounting to the back of the vehicle either around the license plate or around the rear bumper.

     

     

    Whenever a Bluetooth is met having a Bluetooth stereo, they've created an interaction around a network that is not just like a large one the thing is for Wireless and computers. Typically, it’s known as an individual area network and may hold a maximum of eight devices. Every one of these devices has one central hub (within this situation, the car stereo), and may pass information and data between one another to effectively use Bluetooth.

     

     

    Of car audio updates, this is often likely probably the most economical. Jacks are usually existing in nearly all car stereo systems-there's accessible, but generally, they are not used to their finest possible. Some vehicle proprietors disregard the truth these jacks may be used to produce audio or appear by utilizing outdoors sources just like a Personal stereo, an digital audio player, an I-pod, etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • sunny94
    sunny94 over 9 years ago

    They are DVD systems that haven't been made with a GPS navigation system. Two groups can be found: The Gps navigation and also the no- GPS car DVD. They however produce other features the happen to be made with Bluetooth support.  This selection enables you to hear music and you may also receive calls.  The machine also has a radio and   music player. If you're searching for any more complex system, then your GPS DVD player may be the best brand out there.  It's been made with a GPS navigation feature along with a map.  Additionally, it arrives with a Bluetooth, radio receiver, stereo, and subwoofer, 3G Internet along with a USB and SD input.

     

     

    The motto of EinCar is Expert In Car electronics. Also, Eincar sells only top quality stuffs with global standards. Every EinCar’s goods are always reviewed by our experienced Qc team with proffessional rules. Under its strict tests and qc procedure, it's worldwide standards both in quality and safety.

     

     

    If you wish to reverse your vehicle from a automobile parking space, the thought of using of the car backup camera is a terrific way to make certain that you don't mistakenly hit anything. If you are using the interior mirror, they're most occasions not efficient particularly if you drive a truck or perhaps an Sports utility vehicle. These units are often available on greater finish models as well as, it is simple to have them in a retail store at significant prices. These cameras work by mounting to the back of the vehicle either around the license plate or around the rear bumper.

     

     

    Whenever a Bluetooth is met having a Bluetooth stereo, they've created an interaction around a network that is not just like a large one the thing is for Wireless and computers. Typically, it’s known as an individual area network and may hold a maximum of eight devices. Every one of these devices has one central hub (within this situation, the car stereo), and may pass information and data between one another to effectively use Bluetooth.

     

     

    Of car audio updates, this is often likely probably the most economical. Jacks are usually existing in nearly all car stereo systems-there's accessible, but generally, they are not used to their finest possible. Some vehicle proprietors disregard the truth these jacks may be used to produce audio or appear by utilizing outdoors sources just like a Personal stereo, an digital audio player, an I-pod, etc.