Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum PS4 AND XBOX ONE PORTABLE ALL COMBINED IN TO ONE
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 42 subscribers
  • Views 426 views
  • Users 0 members are here
  • Console Builds
Related

PS4 AND XBOX ONE PORTABLE ALL COMBINED IN TO ONE

trentoncrowder0027
trentoncrowder0027 over 9 years ago

Well i got this ideas in my mind and well i thought why not make a PS4 AND XBOX ONE AKA PSX AS IN WLL YOUR KNOW basycle make it so bothe system work on the same power sourc and the same video cable oh yha you can you make a self for you best prochect ot not thanks bye image

  • Sign in to reply
  • Cancel
  • sneb
    sneb over 9 years ago

    Hi,

     

     

    It would be hard with out certain devices such a switching power supply for the different input voltages and amps, you might  struggle to put the video cable into all in one because I don't think Xbox One or PS4 can switch the display sources. ( if it was possible it would probably require two graphic chips on board.) Or thinking about it the only other way i can think of is having the  Sony's PS4 hardware (processors and etc.) on the same motherboard of the Microsoft Xbox One.

     

     

    hope this help's with your Question

    Ben

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • malloc
    malloc over 9 years ago

    Hey Trenton,

     

    I've worked on video game consoles for a long time as part of my job, and I've gotten a pretty good look at the insides of an PS4 and an Xbox One.

     

    This would require...A lot of work. However, I think it's technically possible depending on how crazy you're willing to get with it.

     

    The biggest problem, easily, is the "portable" part. The PS4 and Xbone generate too much heat and draw too much power to be portable without a lot of modifications; putting both of them in the same physical housing is pretty much begging to accidentally burn your house down. At the very least, it won't live very long without a lot of pretty complicated cooling solutions, which would likely draw more power, which would mean a bigger battery, which would add more head and weight, etc.

     

    Now, if we ditch the idea of "portable" and just go with a combo PS4 and Xbone? That actually wouldn't be too horrifically difficult. You just pull the guts of a PS4 and an Xbone and arrange them in a computer case so that they fit without colliding with each other or shorting out, get splitters for the power and disc drives, plus an internal switch for the Ethernet cable so you just have one cable extending out of the unit (or just go wireless on both).

     

    This is way more difficult than I'm making it sound, but we had test kits at work for both those consoles and all they really are is mental boxes with a bunch of test equipment bolted on to them. The motherboards are pretty robust and should still operate okay if they're given sufficient space for cooling.

     

    Downsides: You'd need two disc drives since as far as I know, the two systems cannot share a drive or even talk to the same one. Honestly it wouldn't really be a "hybrid" system, just a box holding two consoles together in the same place. You could probably rig them up to share USB ports but that's about it, and honestly I'd have to try this myself to confirm, I'm just speculating.

     

    Feel free to ask any questions though and I'll answer as best I can.