Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum My dream device made real
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 42 subscribers
  • Views 535 views
  • Users 0 members are here
Related

My dream device made real

e14 Contributor
e14 Contributor over 10 years ago

I would love to see a small system like a raspberry pi or similar fitted into a Psion 5mx case. with either same screen or a colour screen fitted, network capabilities and original Psion keyboard. Running from the same battery pack would also be great or fitted with a new one.

  • Sign in to reply
  • Cancel
Parents
  • toxxn
    toxxn over 10 years ago

    This would be a neat little way to turn the Raspberry Pi into a Handheld Portable Pi Laptop. With the size of the Psion 5mx, I don't think there would be a problem fitting a Pi into the case, might have to remove some things, but possible. I would assume that the driver components for the 5mx's lcd are on board, meaning that an external LCD roughly the same size as the original LCD with a separate driver board would need to be used and then fit to the case. I believe the hardest part of a project as such would be incorporating the original keyboard to work with the Pi, unless it has some sort of port to connect the keyboard to an external source.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • toxxn
    toxxn over 10 years ago

    This would be a neat little way to turn the Raspberry Pi into a Handheld Portable Pi Laptop. With the size of the Psion 5mx, I don't think there would be a problem fitting a Pi into the case, might have to remove some things, but possible. I would assume that the driver components for the 5mx's lcd are on board, meaning that an external LCD roughly the same size as the original LCD with a separate driver board would need to be used and then fit to the case. I believe the hardest part of a project as such would be incorporating the original keyboard to work with the Pi, unless it has some sort of port to connect the keyboard to an external source.