Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Super 8/8mm Film Converter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 42 subscribers
  • Views 4015 views
  • Users 0 members are here
  • 3d pritning
  • image processing
  • Mechanical
  • arduino:
  • analog-to-digital converters
  • camera.
  • Single Board Computer
  • image sensor
  • sbc
  • raspberry pi
Related

Super 8/8mm Film Converter

mglafond
mglafond over 9 years ago

As I envision it, the idea for a film converter screams for the use of an Arduino or Raspberry Pi to automate the process, some mechanical engineering to figure out film transport, 3D printing to create the "sprockets" that precisely advance the film, and image capture capabilities.  My idea is to create what is called a telecine converter that would automate the digital capture of each frame of the film as an image, and then allow those images to be strung together at the proper frame rate to create a digital copy of the film.

 

A little background:

 

I have a box full of 8 mm and Super 8 movie film that my parents shot of my brother and sisters when we were kids. Though I do have a projector, fiddling with it is always tricky, and you end up watching 3-5 minutes of film before you have to rewind it, and load the next roll. Needless to say, I never pull it out to watch the film.

 

There are commercially available systems, but the decent ones are prohibitively expensive, and the affordable ones are too low resolution to even bother spending your time doing the conversion. There are "devices" that allow you to project the film into one side, and then use a digital camera/video camera to capture the image from the other side in real time, but these systems suffer from incongruous display and capture rates, resulting in a "beat frequency" or "flicker" in the finished capture.  They also suffer from a hot spot in the center of the film image (and relatively poor illumination in the corners of the image) caused by the filament in the lamp on the projector. And projectors can't be stopped to capture a single frame without danger of melting the film with the heat of the lamp.

 

Commercial sites (WalMart, Costco, and others) will also transfer film for you, but they are expensive, usually in the $10 range for a 50' (3-5 minute) reel captured at Standard Def, and more for HD. If you have a sizable number of rolls, this quickly adds up, if you are even willing to let precious old home movies out of your possession for 3-5 weeks to a lab located who knows where.

 

Of course digitization would allow for color correction, scratch reduction, and various other types of repairs to the digitally captured copy of the original film. Also, though I don't have any film with sound, but I understand there are 8 mm films out there that do have an audio track, and that could also be captured and synchronized with the film. Converting the images to a movie, and post-processing (color correction, scratch reduction, etc.) could be an interested second phase to the project. Or maybe there is an open source or Linux based solution to do it on the fly at the time of capture?

 

I imagine an Arduino (or preferably a Raspberry Pi) using a stepper motor to advance the film one frame, and trigger a digital camera (or phone) to capture an image of the frame and save it to an SD card or computer (via USB, WiFi or Bluetooth). Most cameras and phones today have sensors that are 10 MP or bigger, which means the resulting film created from these captures should be 4K or better (I think). Of course we're limited to the quality of the original film, but why capture it at less than 4K?!?! Another option would be to use the Raspberry Pi camera, which has a resolution of 5MP, I believe, enough for 1080P but not 4K. I was thinking something like a Canon Powershot with CHDK installed would do nicely. Of course whichever capture solution is used, the optics have to be worked out to enlarge the film frame and focus the camera (maybe one of those clip on smart phone lenses... or an old slide projector lens used in reverse???). I also figure the frame could be evenly illuminated with an LED or LED array to provide a cool, even light source.

 

There are homebrew hacks described on the web where projectors have been retrofitted with LEDS, instrumentation to advance a single frame, and microswitches to trigger a camera, but it seems a complete solution using modern maker tools would be very much in Ben's wheelhouse!

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 9 years ago +2
    There was an 8mm telecine project done a while ago using a hacked Canon IXUS camera with a macro lens and an Arduino which may help generate some ideas : www.youtube.com/watch It is documented here…
  • spannerspencer
    spannerspencer over 9 years ago +1
    You know what this makes me think of? Those rigs people make for digitising books. They hold the book's pages flat, and there's an arm, or apparatus, that holds a digital camera (sometimes two) in place…
  • spannerspencer
    spannerspencer over 9 years ago

    You know what this makes me think of? Those rigs people make for digitising books. They hold the book's pages flat, and there's an arm, or apparatus, that holds a digital camera (sometimes two) in place to photograph the page. With lighting on the sides to give an even image, too.

     

    You also see those with smartphones instead of digital cameras these days too. And most smartphones now have high frame rate (120fps+) video recording.

     

    If you had this kind of rig (with a Pi or Arduino controlling the film spooling and speed, as you say) and recorded it at a high frame rate, I wonder if that'd work as a telecine device? Not sure what kind of quality you'd get, but as a homemade kit, it could be an interesting experiment!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago

    You are on the right sort of track, and with modern advances in LED lighting you can get a much more even, white light while reducing the temperature to almost zero.

     

    The issue you will have is that the 8mm film will need to be increased to fill the frame of the device capturing it.

    You can go to macro type lens.

     

     

    I seem to recall someone did something along the lines you're suggesting, and they used an old mouse (wired across one button) to interface into the software.

    It was a while ago and I have no idea where I would have saved it.

     

     

    most smartphones now have high frame rate (120fps+) video recording

    They do but at lower resolution, and you really don't want to lose anything.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago

    There was an 8mm telecine project done a while ago using a hacked Canon IXUS camera with a macro lens and an Arduino which may help generate some ideas :

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    It is documented here:

    The 8mm film scanner (Telecine) project, part 1 – Overview – Sabulo, Inc.

    The 8mm film scanner (Telecine) project, part 2 – Hacked camera – Sabulo, Inc.

    The 8mm film scanner (Telecine) project, part 3 – Printed parts – Sabulo, Inc.

    The 8mm film scanner (Telecine) project, part 4 – Arduino – Sabulo, Inc.

    The 8mm film scanner (Telecine) project, part 5 – Programming – Sabulo, Inc.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mglafond
    mglafond over 9 years ago in reply to beacon_dave

    That is a cool project... I hadn't seen that one.  At first glance, it looks very much like what I was describing above

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mglafond
    mglafond over 9 years ago in reply to mcb1

    @mcb1 I think I saw a YouTube video where someone had hacked a mouse to act as a microswitch to trigger the camera. Some of the rigs I've seen on YouTube are very inventive, but very convoluted and hardware specific.  Many come from Europe, so the projectors and other equipment they use isn't readily available in the States.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to mglafond

    mglafond

    Generally I avoided videos due to bandwidth and inability to easily got back, but it could be the same thing.

     

    My interest wasn't as much in what they were doing, it was the use of the miuse button to go to USB that I thought was clever.

     

     

     

    It's annoying me know so much that I'll probably spend three days cursing about disorganised and large hard drives.

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 3 years ago
    [deleted]
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to e14 Contributor

    Very poor quality AI spam.. reported

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mranton
    mranton over 3 years ago

    you may also want to check out this:

    https://hackaday.io/project/167426-8mm-film-scanner/discussion-186801