Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Ben's Home-Brew Solder Reflow Oven 2.0 Episode -- Episode 116
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 17 Jan 2014 3:24 PM Date Created
  • Last Updated Last Updated: 10 Jan 2014 8:24 AM
  • Views 7258 views
  • Likes 4 likes
  • Comments 39 comments
Related
Recommended

Ben's Home-Brew Solder Reflow Oven 2.0 Episode -- Episode 116

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Connect with TBHS
Featured Bonus Materials
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
Ben's fed-up with the difficulty of soldering surface-mount components by hand and builds a new reflow oven to keep in his shop. He transforms an inexpensive toaster over into a vital tool for electronics engineers and tinkerers. In this updated oven, he uses two thermal couples to ensure even heat distribution and effective reflow.
  • 116:
  • reflow
  • ben's
  • solder
  • episode
  • 2.0
  • oven
  • ben_heck
  • heck
  • ben
  • tbhs_ep
  • home-brew
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • colecago
    colecago over 12 years ago in reply to mazzmn +1
    I'm not sure, but I bet most IC sensors wouldn't work well inside an oven, too hot. As for the Thermocouple, you don't need the translation IC, you could just use an Op-amp and math if you know the specs…
  • Sabrina
    Sabrina over 12 years ago in reply to e14 Contributor +1
    Hi- You can see the details available for this show on Ben's blog- Episode 116 Project Files
  • bigdog1
    bigdog1 over 11 years ago in reply to clem57 +1
    thank you.
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Thanks to this video and a bunch of people I know that own DIY reflow ovens, I got my head around making my own!

    I bought a cheap mini oven : 14L, 2 heating elements on top and 2 on bottom for a total of 1300W (announced).

    I'm still waiting for the electronic parts to start the transformation from toaster to reflow.

     

    I really want it to be able to display the comparison of the profile and the actual temperature curve on its screen. So I'll have to use a small dot matrix screen.

    Obviously, it needs to be as accurate as possible for the temperature readings and the control of the heating elements.

     

    "Beta" version will be using :

    • an Arduino Uno R3
    • only one MAX6675 board with a thermocouple type K
    • a cheap lcd color display with SPI interface, probably the one with a SPI touch layer (if I get it to work)
    • a 25A SSR "noname" (hopefully it won't catch fire image )

     

    If it works well enough, it'll bake its own upgrade, as I plan on making my own reflow controller board.

    "Final" version :

    • for the mcu, a STM8 or a STM32 (I would like to start learning to use those arm cortex mcu)
    • two or three thermocouples interfaces, using either MAX6675 or 81855 (I got free samples from Maxim)
    • eventually a small fan to cool the controller board (I'll have to see if the "knob section" gets really hot or not)
    • maybe a large fan to improve the cooling speed
    • and probably a SD card reader to easily add thermal profiles without having to reprogram the mcu

     

    The color LCD screen that you can find everywhere (ebay, adafruit, ...) are mostly screens that were designed for old mobile phones. Most of the time, they're cheap and easy to use since there are many hobbyist made libraries for those screens.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 11 years ago

    Thanks to this video and a bunch of people I know that own DIY reflow ovens, I got my head around making my own!

    I bought a cheap mini oven : 14L, 2 heating elements on top and 2 on bottom for a total of 1300W (announced).

    I'm still waiting for the electronic parts to start the transformation from toaster to reflow.

     

    I really want it to be able to display the comparison of the profile and the actual temperature curve on its screen. So I'll have to use a small dot matrix screen.

    Obviously, it needs to be as accurate as possible for the temperature readings and the control of the heating elements.

     

    "Beta" version will be using :

    • an Arduino Uno R3
    • only one MAX6675 board with a thermocouple type K
    • a cheap lcd color display with SPI interface, probably the one with a SPI touch layer (if I get it to work)
    • a 25A SSR "noname" (hopefully it won't catch fire image )

     

    If it works well enough, it'll bake its own upgrade, as I plan on making my own reflow controller board.

    "Final" version :

    • for the mcu, a STM8 or a STM32 (I would like to start learning to use those arm cortex mcu)
    • two or three thermocouples interfaces, using either MAX6675 or 81855 (I got free samples from Maxim)
    • eventually a small fan to cool the controller board (I'll have to see if the "knob section" gets really hot or not)
    • maybe a large fan to improve the cooling speed
    • and probably a SD card reader to easily add thermal profiles without having to reprogram the mcu

     

    The color LCD screen that you can find everywhere (ebay, adafruit, ...) are mostly screens that were designed for old mobile phones. Most of the time, they're cheap and easy to use since there are many hobbyist made libraries for those screens.