Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Ben Heck’s Intel Edison Laser Harp Part 1: Design Episode -- Episode 253
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 1 Sep 2016 8:23 PM Date Created
  • Last Updated Last Updated: 26 Aug 2016 7:24 AM
  • Views 1578 views
  • Likes 4 likes
  • Comments 4 comments
Related
Recommended

Ben Heck’s Intel Edison Laser Harp Part 1: Design Episode -- Episode 253

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Connect with TBHS
Featured Bonus Content
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Ben works on a Laser Harp using lasers and a photoresistor while Felix sets up the intel Edison with VST: virtual studio technology MIDI music driver to play music on it. How would you use technology to discover a new way for the world to enjoy music? Let us know in the comments below!

Episode 254: Ben Heck’s Intel Edison Laser Harp Part 2: Assembly

 

Inspired by Music Tech Fest in Berlin, Ben and Felix create a Laser Harp using an Intel Edison single board computer and VST: virtual studio technology. The Intel Edison is a single board computer from Intel that includes a dual core atom processor x86 with built in RAM, Flash, WiFi, and Bluetooth. Ben does tests for the laser harp using a breadboard, a bench power supply and an individual laser pointer element.  The laser element has a current limiting resistor built in so he just attaches a voltage rail.  The photoresistor is analog, the more light you give it or take from it, there will be a different rating however if that voltage level goes past a certain amount in an integrated circuit it will either go high or low which will allow them to use it as a digital switch. He uses a photoresistor because it works well with individual light.

 

After he gets a laser he hooks it up to NOT logic gate. The NOT gate has a voltage at which it will switch from 0 to 1. Knowing this value allows them to dial in their photoresistor circuit. The input and output are at different voltages allowing a 5V signal to be converted to a 1.8 V signal.  Felix lays out everything on a protoboard and sets up a VST MIDI music driver on the Edison to allow it to play music. He takes the GPIO signal and maps it to a virtual MIDI device. He reconfigures the kernel and adds the virtual MIDI device to enable it. 12 notes per octave, chromatic scale (includes sharps and flats). The different lengths of harp strings create different notes. The top of the harp has 24 lasers for 24 notes which is two octaves. Ben builds the top half of the harp with all the emitters and lines them up.

  • musicmakerch
  • hack
  • episode 253: ben heck’s intel edison laser harp part 1:
  • Design
  • heck
  • ben
  • tbhs_ep
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 10 years ago +1
    Not sure that "The Intel Edison is a new single board computer from Intel" statement is quite true here ? The Intel Edison was released toward the end of 2014 http://www.intel.com/buy/us/en/product/emergingtechnologies…
Parents
  • atillad
    atillad over 10 years ago

    you could always use visable green lasers and a defuser on the bottom too read the laser

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • atillad
    atillad over 10 years ago

    you could always use visable green lasers and a defuser on the bottom too read the laser