Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Ben Heck’s TI Launchpad Plant Booster Episode -- Episode 256
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 22 Sep 2016 7:51 PM Date Created
  • Last Updated Last Updated: 16 Sep 2016 7:24 AM
  • Views 2285 views
  • Likes 3 likes
  • Comments 7 comments
Related
Recommended

Ben Heck’s TI Launchpad Plant Booster Episode -- Episode 256

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Connect with TBHS
Featured Bonus Content
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Ben builds a light compensator to supply indoor plants light when the sun isn’t able to provide enough light for them.  He uses a Texas Instrument MSP430 Launchpad Development Board, a TI BOOST-AD7042, a DS1307 real time clock, and a grow light. Have you ever done any projects revolving around energy efficiency?  Let us know in the comments below!

Bonus Content: TI Plant Booster Update

 

Supporting Files

Click Herefor access to all the supporting files you will need to replicate this build!

 

 

Ben gets his hands on a Texas Instrument MSP430Texas Instrument MSP430 Launchpad Microcontroller Development Board with a TI BOOST ADS7042TI BOOST ADS7042 booster pack  BOOST-ADS7042BOOST-ADS7042 is a high-speed low powered ADC analog-to-digital converter Karen suggests making a light array that gives supplemental light to plants only when they need it suggest as in the winter time Texas Instrument MSP430 Launchpads have top and bottom headers making it easy to stack many BoosterPacks With this in mind they add a DS1307DS1307 real time clock via the I2C bus so they know what time of day it is. This is important because it gives plants a start time and an end time as well as resting points for receiving light. If the sun is not bright enough then a supplemental light will be activated to help the plant.  DS1307DS1307 RTC is very common and there are many examples online to get you started.

 

The booster pack has a light sensor on it which will allow the device to know how much light is needed. The booster pack includes an LCD and three buttons that you can use to program it. One button is used to set the default amount of light. The other two buttons are used to set the start and end time to cycle through the hours. The light box is controlled by an SSR controlled by the MSP430 so the microcontroller can turn on an alternating current device. Ben adds a header for a DS1307DS1307 real time clock via the 12C bus. Ben populates the board and wires up to the booster pack to the MSP430.

 

He also handles all the coding to make the real time clock work. Ben introduces us to rudimentary electrics on wiring a USA mains plug and using a solid state relay to turn it on and off, and then guides us through using Code Composer Studio and Energia to compile code for the TI MSP430 with boosterpack. The growlight lights up red and blue. Plants are green so they do not care about the color green. He uses a solid state relay because it’s able to control alternating current loads with very low level logic.

  • hack
  • eejournal
  • solarpwrdevicesch
  • episode 256: ben heck’s ti launchpad plant booster
  • heck
  • ben
  • tbhs_ep
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • makerkaren
    makerkaren over 10 years ago in reply to DAB +1
    Yes, we ended up getting plant lights from a neighbor that does plant research. Initially, we were looking for LEDs in the right red and blue spectrum that are ideal for growing plants. My friend Roger…
  • beacon_dave
    beacon_dave over 10 years ago in reply to makerkaren +1
    Might need to add a menu option in the user interface "how do you like your designer plants ? stocky & full / tall & lean"
Parents
  • beacon_dave
    beacon_dave over 10 years ago

    How about finishing it off with some sort of a clear lid that fits over the microcontroller / boosterpack and attaches to the top of the relay enclosure ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to beacon_dave

    Might need to incorporate a plant pot rotator into the design as well, as the plants will likely grow toward the direct sunlight whilst the LED grow lights are off.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 10 years ago in reply to beacon_dave

    Might need to incorporate a plant pot rotator into the design as well, as the plants will likely grow toward the direct sunlight whilst the LED grow lights are off.