Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Ben Heck’s Multi-System Retro Controller Episode -- Episode 260
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 20 Oct 2016 9:20 PM Date Created
  • Last Updated Last Updated: 14 Oct 2016 7:24 AM
  • Views 1855 views
  • Likes 3 likes
  • Comments 7 comments
Related
Recommended

Ben Heck’s Multi-System Retro Controller Episode -- Episode 260

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Connect with TBHS
Featured Bonus Content
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The team builds the ultimate retro gaming controller using an ESP8266 WiFi Module, a transmitter controller, and a receiver on the game console. Universal support includes Nintendo, Super Nintendo, Sega, and Atari. What game consoles would you use on your controller?  Let us know in the below!

 

Supporting Files

Click Here

for access to all the supporting files you will need to replicate this build!

 

To make the universal controller wireless they use the inexpensive ESP8266 WiFi Module. It runs on NodeMCU firmware which can be programmed using LUA. Once you write the script in LUA and NodeMCU executes it the controller module and the console module can talk to each other. The controller module is the transmitter and the console module is the receiver.

The plan is to build a custom controller with two shift registers in it. The shift registers are used to read the buttons.  Each shift register has 8 bits for total of 16 bits. 16 bits are used as there will not be more than 16 buttons. The controller module can shift the data out of the shift registers and into itself which is similar to how a Nintendo controller actually works. Because it reads in 16 bits it does not care what the buttons are for each console, it just gets the data.

The custom controller then transmits a 16 bit package in one word to the receiver unit. The receiver takes that data and recreates it on its side with two more shift registers. These would be output registers which would be 74HC595 shift registers. Once again each shift register has 8 bits total for 16 bits, and they are going to be 0 or 1. From that point they connect up the console plugs. The way they connect the plugs to these shift depends on what the buttons actually do. After wiring everything up they use a multimeter to determine what button are being pressed.

They then wire up their controllers to match. Each controller is different.  In the case of the Nintendo and Super Nintendo there is going to be input shift registers to connect to the output shift registers. For the Sega Genesis they’ll need to take apart an old Sega Genesis and hook the pads beyond the chip directly to the output shift registers. One bank of output shift registers, 3 different console inputs.

The ultimate game controller includes the WiFi module, a battery, a charge jack for the batter, and is self-contained.  The receiver unit is powered off of the console because all consoles have 5V somewhere on their plug. They begin by working on the console controller.  Once they have that working they build the receiver and test it on the consoles.

Ben maps out the parts to make the video game console on a board using a 3.3 power regulator and a server module that plugs into the74HC595 shift registers. Shift registers are needed to translate as consoles run at 5V while WiFi works at 3V. The 74HC595 input shift registers are the same as the ones used on the controller and they will be used to plug into the Nintendo and the Super Nintendo. He also uses some 74157 quad muxes for the Sega and Atari. Turns out it’s much easier to just hack a 6 button controller.

After a lot of testing, soldering, and hacking apart a Sega controller, the team puts together the ultimate gaming controller!

  • episode 260: ben heck’s multi-system retro controller
  • hack
  • heck
  • ben
  • tbhs_ep
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • king_horror
    king_horror over 10 years ago +1
    Will you be posting this to Github?
  • makerkaren
    makerkaren over 10 years ago in reply to king_horror +1
    It will make it there. When Felix finds time to take a break from hacking.
  • DAB
    DAB over 10 years ago in reply to makerkaren +1
    That is why I watch the BHS. You just never know what you can learn when you watch people make stuff. In engineering, it is not the end product that is of importance as much as it is the technology and…
Parents
  • DAB
    DAB over 10 years ago

    I am not a gamer, but it was still and interesting episode on how to interface controllers using a wireless board.

     

    Well done.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 10 years ago in reply to DAB

    Glad you liked it! I'm always happy to hear people find something for themselves in the episodes with topics that may not be of interest to them normally.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • makerkaren
    makerkaren over 10 years ago in reply to DAB

    Glad you liked it! I'm always happy to hear people find something for themselves in the episodes with topics that may not be of interest to them normally.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 10 years ago in reply to makerkaren

    That is why I watch the BHS.

     

    You just never know what you can learn when you watch people make stuff.

     

    In engineering, it is not the end product that is of importance as much as it is the technology and skills needed to make it.

     

    I always find subjects of interest in unusual places.

     

    DAB