Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Logic Gate Board Game 01: Project Planning -- Episode 282
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 23 Mar 2017 7:57 PM Date Created
  • Last Updated Last Updated: 17 Mar 2017 8:24 AM
  • Views 4629 views
  • Likes 4 likes
  • Comments 24 comments
Related
Recommended

Logic Gate Board Game 01: Project Planning -- Episode 282

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Logic Gate Board Game
Featured Bonus Content
See All Episodes

 

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The Ben Heck Team begin mapping out the Logic Gate Game by considering its purpose, areas for improvement, reducing costs to build to scale, and materials to be used.  Ben uses a PIC microcontroller with plenty of I/O, wires up a breadboard, and uses ChipKit to quickly roll out code.  The team needs your help deciding on an LCD screen and a microcontroller with enough IO to connect with all the plugs!

 

Ben and Karen begin by mapping out a plan for their prototype using a diagram from a previous build.  They get rid of FLIP-FLOP, COUNTER, NAND, and NOR and keep AND, OR, XOR, and NOT. They can make NAND and NOR using the NOT gates. Each game set will come with 10-20 jumper wires to keep costs reasonable.  Ben and Karen offer different perspectives on how best to set up a learning game and who their target audience will be.

Next, it’s time to Ben and Felix to make a test circuit. Ben takes out a PIC32 starter kit with plenty of IO on it.  You program these with Microchip’s MPLB X IDE which can be found online. If they’re able to find a microcontroller with enough I/O they could conceivably simulate all the logic gates.  The other option would be to use an external I/O expander.  The idea is to use a line of female headers and another line of male headers to crudely simulate their logic gate connections and then trying to do a state machine loop MPlab to get it to simulate what they want.

Before going for it with MPlab, Ben first uses the Arduino ChipKit IDE to make things easier so he can roll out a quick example.  The ChipKit uses a PIC32MX795F512L which has plenty of I/O to test.  Ben wires up the breadboard and writes some code.  They’re writing the logic gates in code instead of using IC’s.

  • episode 282: logic board game 01: project planning
  • hack
  • logic_gate
  • logic_board_game
  • heck
  • ben
  • logic_gate_board_game
  • stem projects
  • tbhs_ep
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 9 years ago +4
    makerkaren - A compromise might be to make the magnetic connectors stackable so as to be able to bus the connectors together that way. (A bit like the stackable banana plugs from school physics.) Alternatively…
  • COMPACT
    COMPACT over 9 years ago +2
    Back in 1971 I learned digital logic at Infants school (6-7 years old) using nothing more than; A pair of Scissors, some cards, and Knitting needles. And Set theory using; a few cane hoops and wooden blocks…
  • chdabre
    chdabre over 9 years ago +1
    Hey Guys, I had a crazy idea about the gate layout: Instead of using a number of fixed gates printed on the board, you could try a modular approach with multiple small lcd displays (like the old cheap…
Parents
  • tm14
    tm14 over 9 years ago

    Who is your target audience for this product?  Find a group of them and get their feedback.  Size up the potential demand by asking them if they would buy it?  How can the product be changed to increase demand and reduce costs?

     

    Ben seems to want to keep the wires and make it small.  So consider hacking a breadboard.  You can use regular wires, you have buses, and you can take it apart and connect the electronics from behind.  Or you can make your own breadboard if you can figure out how to make all the little bent pieces that go inside the breadboard.  I don't like exposed wires carrying electrical power.  Remember the game Operation.  The original version had a wire and a buzzer.  If your fingers were damp, you could give yourself a shock.  You have to consider passing safety certifications when you have exposed wiring, right?  Better to use a LCD display (as suggested above) or make long slide switches that can connect to any other input by sliding or rotary switches (single pole, many throws) or use a potentiometer and A2D to get position (but this would mean the logic would have to be all software emulated) .

     

    Felix was in the background, listening and watching.  It would have been nice to know what he was thinking with a speech balloon like "I can't get any work done until those two agree on something", "I know it's going to come down to a bunch of code I'll have to write", or "I wonder if big Ben would mind if I nicked a can of diet Pepsi from the fridge."

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gordiegii
    gordiegii over 9 years ago in reply to tm14

    I was thinking of a pegboard cross-point switch but it has some potential problems and I realized your idea of slide switches has a lot of potential, especially if there is a way to make it look like a circuit diagram.

     

    The way I see it, there would be a slide switch for each input to select the signal source.  Sources could be one of the four data inputs or any of the gates outputs.

    Of course the four output lights would each have a slide (or rotary) switch to select its source.

    Multiple gate inputs could connect to the same source by setting them to the same position, and it's impossible to connect outputs to each other.

     

    The slide switches could be purchased but it would probably be cheaper to make 3D printed bits that slide across pads on the circuit board (built into the case) and the number of positions wouldn't be limited to what's available in stores. Of course you could use a bunch of slide pots but you would need a bunch of analog inputs. Or, digressing even further from the visceral jumper wire concept, you could have a bunch of LEDs (charlie-plexed of course) to indicate the position of virtual slide switches which could all be adjusted with just two rotary encoders.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • gordiegii
    gordiegii over 9 years ago in reply to tm14

    I was thinking of a pegboard cross-point switch but it has some potential problems and I realized your idea of slide switches has a lot of potential, especially if there is a way to make it look like a circuit diagram.

     

    The way I see it, there would be a slide switch for each input to select the signal source.  Sources could be one of the four data inputs or any of the gates outputs.

    Of course the four output lights would each have a slide (or rotary) switch to select its source.

    Multiple gate inputs could connect to the same source by setting them to the same position, and it's impossible to connect outputs to each other.

     

    The slide switches could be purchased but it would probably be cheaper to make 3D printed bits that slide across pads on the circuit board (built into the case) and the number of positions wouldn't be limited to what's available in stores. Of course you could use a bunch of slide pots but you would need a bunch of analog inputs. Or, digressing even further from the visceral jumper wire concept, you could have a bunch of LEDs (charlie-plexed of course) to indicate the position of virtual slide switches which could all be adjusted with just two rotary encoders.