Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Super Glue Gun 03: Ungluing the Great Glue Gun -- Episode 289
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 11 May 2017 8:50 PM Date Created
  • Last Updated Last Updated: 5 May 2017 7:24 AM
  • Views 1867 views
  • Likes 4 likes
  • Comments 6 comments
Related
Recommended

Super Glue Gun 03: Ungluing the Great Glue Gun -- Episode 289

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Super Glue Gun
Featured Bonus Content
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The team gets back to work on the Super Glue Gun. Previously they worked on controlling the heating element with a triac and controlling the motor while extruding the glue through it. The team gets help from a community member who returns a previous super glue gun build to Ben.

 

Check out more Super Glue Gun Episodes

Super Glue Gun Ideas

The Motor on the previous glue gun build is smaller than some of the other motors they tried. It uses a SN754410E Quadruple Half-H Driver. The Mains go straight to the heater core. The 12V adapter goes to a 5V stepdown for the microcontroller. The glue gun has a temperature sensor on it so if it’s not warm enough the motor will not extrude. The motor driver is driven at 12 V.  Ben demonstrates the control the glue gun gives him by writing in cursive with the glue gun.  A design flaw of the previous glue gun is that the heat from the motor is causing the glue that held the motor in place to fall off.

Ben rigs up an extrusion test. He 3D prints a part to test the motor with a larger bearing. After testing the extrusion its determined that the glue gun needs a tougher base plate.  Adding a plate prevents the idler-wheel from being pushed out with the force, keeping all the force on the glue stick, allowing it to extrude. Unlike the original glue gun, this glue gun isn’t spring loaded meaning it’s easier to build.  Finally, they refine the form using foamcore and are able to get the glue gun to extrude glue using a fairly small DC gear motor.

Disclaimer

  • hack
  • episode 289: super glue gun 03: ungluing the great glue
  • heck
  • ben
  • tbhs_ep
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • tm14
    tm14 over 9 years ago

    The metal parts may be overkill for job and their weight will add to shipping costs of the final product.

     

    Instead of bearing, why not use a simple post and a sleeve.  They used to use these in VCRs as tape guides.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 9 years ago in reply to tm14

    It would still need to spin. Are you suggesting that the metal bearing basically get replaced by a plastic bearing with a silicone or rubber covering for grip? Or a plastic post to brace against that doesn't spin, but offers a small enough amount of friction to work well enough?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • makerkaren
    makerkaren over 9 years ago in reply to tm14

    It would still need to spin. Are you suggesting that the metal bearing basically get replaced by a plastic bearing with a silicone or rubber covering for grip? Or a plastic post to brace against that doesn't spin, but offers a small enough amount of friction to work well enough?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • tm14
    tm14 over 9 years ago in reply to makerkaren

    A VCR tape guide is built a bit different, but the concept is the same as the following.

     

    I think all you need is a nylon cylinder with a hole in the middle and a pin or something that is smooth and can hold the cylinder in place.   This replaces the metal bearing.   The following is not the correct size, but you'll get the idea from this picture:

     

    PC Board Spacer 0.25" Nylon #4 Hole 100 Pcs. | 94F9907 | Distributed By MCM

     

    You probably even have them in the shop.

     

    If you just use a bolt with threads and with a wide pan head, I think the wide head may help keep the glue stick in bounds, but the threads may add friction and chew up the inside shaft of the spacer.  If you can find a bolt with threads at the very bottom only and a smooth shaft, that would work the best.  Or get a rod and use a tap and dye set to add only the amount of threads you need to mount it and screw a nut on the top and glue with super glue to keep it in place.

     

    If this method works, it should cut the cost significantly.