Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Logic Gate Board Game 04: LCD's Driving Me Crazy -- Episode 293
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: randogless
  • Date Created: 8 Jun 2017 9:13 PM Date Created
  • Last Updated Last Updated: 2 Jun 2017 7:24 AM
  • Views 4095 views
  • Likes 2 likes
  • Comments 17 comments
Related
Recommended

Logic Gate Board Game 04: LCD's Driving Me Crazy -- Episode 293

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Logic Gate Board Game
Featured Bonus Content
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In this week's episode the team considers a library from Microchip and how the game will work. Microchip has a library that allows you to drive an LCD glass with just a microcontroller, no need for an external controller or extra RAM.  They also discuss gamification, make some diagrams of how they want to space up the screen, what goes on the screen, where to put the plugs, and figure out how the puzzle is going to work on the screen. Have advice on how gamification will work?  Let us know in the comments below!

 

 

Ben attempts to use the PIC32 MZ starter kit as a mass storage device with a computer.  Acting as a mass storage device, more puzzles could be added just by dragging and dropping from a computer. There are multiple USB ports on the end; there’s one if it’s a device and one if it’s a host such as your computer.  Ben want’s the microcontroller to act as a device like a USB thumb drive.  There’s also a programming header and a UART with a USB converter.  The hope is that there will be a single USB port on the logic gate board game that can be used for charging as well as transferring data.

 

Ben goes over programming the microcontroller using MPLAB harmony, which includes a good number of examples in its library.  The problem is it doesn’t really tell you how to use them.  What they can do is set up an area of NVM non-volatile memory, the flash that holds the program, and set it up as a small file system.  This allows them to access it from within their program to get files. The USB could also use it as a file system so the user can put files there. Although, they may want to have separate file systems so there’s an area of memory that a person can’t destroy just plugging it into their computer. Getting examples to work isn’t that difficult, the real trick is combining them all.  This includes some kind of sound, LCD, USB, and file system.

 

After aligning the LCD screen he sets up another NOR gate using the MPLAB IDE. They need to do more work on the gamification and how the screen is going to be set up but if they can combine the schematic editor with a graphics driver and create a markup language that can store puzzles in as small space as possible, they’re at a good jumping off point.

 

Karen helps Ben with the gamification using Logic Gate pieces cut out to scale. The further they get away from the Hackmanjii concept, the more difficult it becomes to grasp the gamification.  They discuss giving the game the ability to drive real external devices. Karen slaps Ben with a reality check as things veer off course and they struggle to figure out a purpose for the game.

 

 

Disclaimer

  • lcd
  • episode 293: logic gate board game
  • hack
  • lcd's driving me crazy
  • heck
  • ben
  • stem projects
  • tbhs_ep
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 9 years ago in reply to tm14 +2
    Perhaps sounds a little bit like the 1970's 'Mastermind' game with the coloured pegs https://en.wikipedia.org/wiki/Mastermind_(board_game) However Mastermind is part guesswork, part logic so not ideal…
  • tm14
    tm14 over 9 years ago in reply to tm14 +1
    Another way to verify solution with sounds would be to step through each possible set of inputs at a fast speed (needed if you have more than 4 bits of inputs). At each step, if the result is correct,…
  • josefcs
    josefcs over 9 years ago +1
    I thought of the following, please see (and excuse) attached crude drawings. In general, on the left hand side, there is a row of LEDs. In the middle, there ist the LCD screen. On the right hand side,…
Parents
  • greywolfzx
    greywolfzx over 9 years ago

    Near the end of the episode, if I understood correctly, I think Karen had a good point about just moving the wires from place to place till you get it right becoming tedious.  I don't see any motivation to learn in that scenario.  A kid would just try things until they got it right or got bored.  I guess this would all be dependent on the failure states.  Is the game just timed? Do you have a limited number of guesses?  What this reminded me of was trying to diffuse a bomb or hack a security system.  I think you might be able to get better engagement if the product had a fun theme with an ulterior motive of learning.  What I mean is, Logic Gate Puzzle Game does not sound as cool as Spy Security Door Hacking Game even though they are functionally the same game.  This would allow for a failure state to be that you were detected by the enemy agents.  Your puzzles could have a correct solution that disables the lock and an incorrect solution that triggers the alarm.  The fear of failure, getting caught, I feel would be a powerful motivator to learn the gates and prohibit the tendency to just enter solutions until it works.

     

    I do have to agree with Ben in that if you want your product to be a success, you build something you would want.  But, then it becomes difficult to complete a project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • greywolfzx
    greywolfzx over 9 years ago

    Near the end of the episode, if I understood correctly, I think Karen had a good point about just moving the wires from place to place till you get it right becoming tedious.  I don't see any motivation to learn in that scenario.  A kid would just try things until they got it right or got bored.  I guess this would all be dependent on the failure states.  Is the game just timed? Do you have a limited number of guesses?  What this reminded me of was trying to diffuse a bomb or hack a security system.  I think you might be able to get better engagement if the product had a fun theme with an ulterior motive of learning.  What I mean is, Logic Gate Puzzle Game does not sound as cool as Spy Security Door Hacking Game even though they are functionally the same game.  This would allow for a failure state to be that you were detected by the enemy agents.  Your puzzles could have a correct solution that disables the lock and an incorrect solution that triggers the alarm.  The fear of failure, getting caught, I feel would be a powerful motivator to learn the gates and prohibit the tendency to just enter solutions until it works.

     

    I do have to agree with Ben in that if you want your product to be a success, you build something you would want.  But, then it becomes difficult to complete a project.