Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Help Ben Create an Automatic Can Crusher -- Episode 3
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: bluescreen
  • Date Created: 24 Oct 2010 11:24 PM Date Created
  • Last Updated Last Updated: 8 Oct 2010 7:24 AM
  • Views 5291 views
  • Likes 2 likes
  • Comments 18 comments
Related
Recommended

Help Ben Create an Automatic Can Crusher -- Episode 3

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Connect with TBHS
Featured Bonus Materials
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
Ben's friend The Longhorn Engineer challenges him to build an automatic, domestic can crusher. Ben also starts building the case for the Xbox 360 laptop.

 

Check out the Ben Heck BOM ListCheck out the Ben Heck BOM ListCheck out the Ben Heck BOM List
  • hack
  • an
  • automatic
  • he?
  • episode
  • 3:
  • does
  • quest
  • ben_heck
  • builds
  • heck
  • ben
  • crusher...
  • can
  • or
  • tbhs_ep
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Wow, I came into this late so I'm guessing the can crusher project was scrapped. But, just to throw in my 2 cents, I would suggest a windshield wiper motor and an Hbridge high power servo board to actuate and control the can crusher. Car windshield wiper motors are pre built with a worm gear, can operate at 5-12 Vcc, and have (usually) 2 or more connectors to operate at different speeds, plus they have MONSTER torque! This can be made into a hi power servo by linking the motor to an Hbridge circuit from Parallax.com which is around 15 bucks. A wiper motor is about the same price (15 bucks) new, but pulled from grandmas car (she refuses to drive in the rain anyways, right?) you can get it for free. The challenge would be mounting a 5V POT to the rotation shaft of the motor for position feedback to whatever servo controller board you choose. You could even use a remote control model airplane controller to make the servo work, or you could ditch the whole servo idea altogether and take advantage of the parking feature that SOME windshield wiper motors already come with. This means that the wiper motor shaft will return to the original position after one rotation of the shaft and would allow the motor to be actuated with a simple relay. Just a thought.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 15 years ago

    Wow, I came into this late so I'm guessing the can crusher project was scrapped. But, just to throw in my 2 cents, I would suggest a windshield wiper motor and an Hbridge high power servo board to actuate and control the can crusher. Car windshield wiper motors are pre built with a worm gear, can operate at 5-12 Vcc, and have (usually) 2 or more connectors to operate at different speeds, plus they have MONSTER torque! This can be made into a hi power servo by linking the motor to an Hbridge circuit from Parallax.com which is around 15 bucks. A wiper motor is about the same price (15 bucks) new, but pulled from grandmas car (she refuses to drive in the rain anyways, right?) you can get it for free. The challenge would be mounting a 5V POT to the rotation shaft of the motor for position feedback to whatever servo controller board you choose. You could even use a remote control model airplane controller to make the servo work, or you could ditch the whole servo idea altogether and take advantage of the parking feature that SOME windshield wiper motors already come with. This means that the wiper motor shaft will return to the original position after one rotation of the shaft and would allow the motor to be actuated with a simple relay. Just a thought.