• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum CNC Router Designs
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 35 subscribers
  • Views 2863 views
  • Users 0 members are here
Related

CNC Router Designs

benheck
benheck over 16 years ago

Attached are my designs for the CNC Router we did in Episode 2. There are certainly things I would do differently now, but it did function. I used PVC plastic, but MDF is a popular material for this as well.

 

You may need to modify it depending on the physical size of the stepper motors. I don't like when I see homemade CNC machines with motors hanging off the ends, so I made mine in-line. The side effect is the design and spacing is more aggressively tight, so a larger motor might not fit.

 

The cutting motor is a Porter Cable Laminate router. You can get one at Farm & Fleet for around $100.

 

I'll post the designs for the Xbox 360 laptop probably in Episode 6. Also, will offer the plans for Portable Work Bench whenever it shows up, probably episode 4.

Attachments:
CNC.zip
  • Sign in to reply
  • Cancel

Top Replies

  • ckraft
    ckraft over 15 years ago in reply to e14 Contributor +1
    The SparkFun steppers won't be enough. For a CNC type machine you need lots of torque because you have to push a cutting tip around the material. NEMA 23's at a minimum. Something with lots of torque,…
  • weekendranger
    weekendranger over 12 years ago +1
    Ben, I wanted to find out what you are using to cut the plywood. I know you are using a laser cutter but I wanted to know what model or at lest the model of the laser that you use if you home brewed your…
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago
    I see you are using Artpath to route parts for the CNC. I have to work with that @#%@^@! everyday:(
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • benheck
    benheck over 16 years ago in reply to e14 Contributor

    Ah yes Gerber. Great hardware, crappy software.

     

    Remember when it took them almost 6 years to make a 32-bit version of their software after Windows 95 came out?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to benheck
    "Advanced Nesting features...." image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to benheck
    "Advanced Nesting features...." image