• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Viewer Challenge (Multi-System.....System)
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 29 subscribers
  • Views 609 views
  • Users 0 members are here
Related

Viewer Challenge (Multi-System.....System)

e14 Contributor
e14 Contributor over 15 years ago

Hello, I am young viewer of the show and and challenging Ben Heck to try his abilities and to make a system that can play games from more than one system (ex. PS2, XBOX) but the real challenge is to choose from the examples and to add either DS or PSP capabilities.

 

 

                                                                                                                                                                                   Fan,

                                                                                                                                                                                      LongHairedFinley      

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    There are a few options, such as gutting several systems and incorporating them in one case like a large computer case. A PC can run a program called an emulator to siumulate many older game systems, a tv tuner or video capture card could be used to pickup the hardware game systems video outputs. Depending on how many devices installed it might be nessacary to use some kind of switching device to change inputs since most video capture devices only support one input. Only down side I can see is that depending on how many devices you install in a single case the number of fans required to keep it all cool could become quite noisy. Would be an interesting project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    There are a few options, such as gutting several systems and incorporating them in one case like a large computer case. A PC can run a program called an emulator to siumulate many older game systems, a tv tuner or video capture card could be used to pickup the hardware game systems video outputs. Depending on how many devices installed it might be nessacary to use some kind of switching device to change inputs since most video capture devices only support one input. Only down side I can see is that depending on how many devices you install in a single case the number of fans required to keep it all cool could become quite noisy. Would be an interesting project.