• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Episode Idea
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 32 subscribers
  • Views 722 views
  • Users 0 members are here
  • portable
  • hardware
  • giveaway
  • contest
  • build_challenge
  • idea
  • viewer_challenge
  • challenge
  • lessons
  • ben_heck
  • arduino
  • show_idea
Related

Episode Idea

AniGeek
AniGeek over 14 years ago

heres an idea since youve already talked about the Raspberry Pi and have Sponsored Rev3 episodes that involved the RPi, how about building a 22 inch laptop using these minimum specs:

 

Monitor:

Asus VE228H 21.5-Inch Full-HD LED Monitor with Integrated Speakers

http://www.amazon.com/Asus-VE228H-21-5-Inch-Integrated-Speakers/dp/B00413PHDM/ref=sr_1_2?ie=UTF8&qid=1349558416&sr=8-2&keywords=Asus+ML228H+21.5%22+Full+HD+LCD+Monitor

 

Raspberry Pi board

 

Any form of linux (hopefully either mint or gnome will work)

 

at least 6-8 USB ports for attachments such as wifi dongle, external hard drives, wireless mouse, external burn/read disc drive etc

 

power supply with surface push button switch or toggle switch to power on the system

 

built in keyboard with direct line to raspberry pi or secondary (arduino or pcb board to interface with raspberry pi)

 

1 or 2 micro fans to make sure everything stays cool on the case

 

total thickness of case and monitor closed around 1 1/2 inches

 

lightweight materials

 

I hope this build gets done because i want to learn how to do it myself because i know only about half of what i need to do to build it

 

thanks for all you do Ben its good to see those out there inovating the world around us

  • Sign in to reply
  • Cancel
Parents
  • COMPACT
    COMPACT over 14 years ago

    This can be done straight out of the box with a Raspberry Pi. 

    Raspberry Pi has HDMI output that can be directly connect to the HDMI of your monitor.

    The Raspberry Pi USB port can be connected to a multiport USB Hub to provide access to your 8 or more USB ports.

    For the keyboard and mouse you can use some of the USB ports.

     

    If the power supply of the monitor is sufficient, you could power the Raspberry Pi and peripherals with it too.

    Then you can use your monitor power switch for everything.

     

    If the power supply is not sufficient which is most likely the case, then you can use one a master sensing power board.

    You can connect your LCD monitor to the master socket and have the Raspberry Pi Power supply driven from a Slave socket.

    Be very very careful if you are dealing with High voltages! Make sure all safety precautions are met to guard against electric shock.

     

    Once you have it all working then you can encapsulate the "Notebook" with your own custom designed box.

     

    If you want to use a wireless mouse and keyboard, just connect a wireless keyboard/mouse dongle to one of the USB ports.

     

    I foresee this project mainly consisting of a lot of wire harnessing work.

     

     

    I hope this helps you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • COMPACT
    COMPACT over 14 years ago

    This can be done straight out of the box with a Raspberry Pi. 

    Raspberry Pi has HDMI output that can be directly connect to the HDMI of your monitor.

    The Raspberry Pi USB port can be connected to a multiport USB Hub to provide access to your 8 or more USB ports.

    For the keyboard and mouse you can use some of the USB ports.

     

    If the power supply of the monitor is sufficient, you could power the Raspberry Pi and peripherals with it too.

    Then you can use your monitor power switch for everything.

     

    If the power supply is not sufficient which is most likely the case, then you can use one a master sensing power board.

    You can connect your LCD monitor to the master socket and have the Raspberry Pi Power supply driven from a Slave socket.

    Be very very careful if you are dealing with High voltages! Make sure all safety precautions are met to guard against electric shock.

     

    Once you have it all working then you can encapsulate the "Notebook" with your own custom designed box.

     

    If you want to use a wireless mouse and keyboard, just connect a wireless keyboard/mouse dongle to one of the USB ports.

     

    I foresee this project mainly consisting of a lot of wire harnessing work.

     

     

    I hope this helps you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • AniGeek
    AniGeek over 14 years ago in reply to COMPACT

    it does a little bit but id like to see it done because i dont know the first thing about using a cnc machine and i cant afford classes for it right nowand i cant afford to buy a cnc right now. so i want to figure out how i can do it with mundane items i found out theres a wifi module for the RPi so i got the wifi figured out but i want to be able to intergrate the keyboard so that its attached as an onboard instead of using a wireless one i already plan on using a wireless mouse that i have but i wanna figure out how to take a modern wired keyboard and wire it to the system and shortening the cord kinda like a keyboard on our current laptops. for the power supply i was going to use his block form that he did on one episode that harnesses multiple power cables but a smaller version to handle just the powering for the RPi and the hubs and then an outlet for the monitor because the one i presented in the link has a small powercord i found out from a buddy who has one of them. but for the case ive got some parts stripped from a printer i had that had tactile switch and the main panel that i can mod to not have the other controls on it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AniGeek
    AniGeek over 14 years ago in reply to COMPACT

    oh and on a side note i would love to be an apprentice of ben's so that i can learn everything he knows be it for modding or on pinball, etc.