• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum PS2 Media PC Case mod
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 32 subscribers
  • Views 568 views
  • Users 0 members are here
Related

PS2 Media PC Case mod

e14 Contributor
e14 Contributor over 13 years ago

Hey Ben and crew,

     I have an old first generation Play Station 2 that broke down a long time ago and I never had the heart to throw it away. I was thinking today, maybe I can build a media center pc and gaming system out of it. I looked for a motheboard small enough to fit in the case and could not find one. I want more power than the Rasbery Pi can handle. So Ben, Do you think you could take on this challenge and help me out?

  • Sign in to reply
  • Cancel
Parents
  • RadioFreeRO
    RadioFreeRO over 13 years ago

    Why not use a mini-ITX motherboard? the Zotac brand makes a lot of PCs with these type of motherboards built in, however most ITX motherboards you can buy will not have that much power to them so you have to consider doing gaming or media center PC but not both unless you want constant lag. Also unless you buy from a manufacturer like Zotac or get a part out of a already built PC like the HP tower PC my friend has with a mini-ITX built in, you're not going to get a newer processor. The most mini-ITX processors go up to I've seen is 1.5 Ghz which isn't that much speed even in early 2000, but they do allow at least newer amounts of RAM you can fit on a board from today's standards like 4 GB to I've seen about 16 GB of RAM which is a factor to how fast it will be and what version of the OS you get. Anything below 4 GB you can use a 32-bit system and get the full speed that a 32-bit system will offer, anything at or above 4 GB you should get a 64-bit OS if you want good speed. If you go above 4 GB on a 32-bit system, there's a possibility of overload which will slow down the PC and on some systems will crash it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • RadioFreeRO
    RadioFreeRO over 13 years ago

    Why not use a mini-ITX motherboard? the Zotac brand makes a lot of PCs with these type of motherboards built in, however most ITX motherboards you can buy will not have that much power to them so you have to consider doing gaming or media center PC but not both unless you want constant lag. Also unless you buy from a manufacturer like Zotac or get a part out of a already built PC like the HP tower PC my friend has with a mini-ITX built in, you're not going to get a newer processor. The most mini-ITX processors go up to I've seen is 1.5 Ghz which isn't that much speed even in early 2000, but they do allow at least newer amounts of RAM you can fit on a board from today's standards like 4 GB to I've seen about 16 GB of RAM which is a factor to how fast it will be and what version of the OS you get. Anything below 4 GB you can use a 32-bit system and get the full speed that a 32-bit system will offer, anything at or above 4 GB you should get a 64-bit OS if you want good speed. If you go above 4 GB on a 32-bit system, there's a possibility of overload which will slow down the PC and on some systems will crash it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • benheck
    benheck over 13 years ago in reply to RadioFreeRO

    I used some AMD E-350 boards recently that would easily fit inside the PS2 case. Even the new slim one!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to benheck

    I looked at a lot of Mini ITX boards and they are too big for the case. I would have to modify the console to fit it or build a new case. Maybe I can figure out a way to use the CNC on campus to make a case that looks exactly like the PS2 case. Thanks for the suggestions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colecago
    colecago over 13 years ago in reply to e14 Contributor

    A Mini ATX board is too big to fit inside the old fat PS2?  That seems strange.

     

    Look into the PCDuino if you want a small form factor but a little more oomph than the Raspberry Pi.  There are plenty of small linux boards out there since the inception of the Pi.