Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 5v Amplifier for speakers
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 32 subscribers
  • Views 1220 views
  • Users 0 members are here
Related

5v Amplifier for speakers

e14 Contributor
e14 Contributor over 13 years ago

I was wondering if it was possible for me to make a circuit which would amplify a stereo audio signal for use with small speakers using a 5v current... I have a couple of speakers, a spare TDA2822 chip and I have access to other basic resources... I found a diagram (attached) except I don't know what the symbols and notation such as "C1 - 1uF" and "VR1 - 10K Lin" mean... Could you help me???

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    jvdberg@ieee.org over 13 years ago

    Will, TDA2822 can be used for this purpose. This circuit will work with supply voltages down to 3.3 Volt. At 4.5 Volt supply you will have 0.32 Watt per channel into a 4 Ohm speaker. 1 Watt output power is available when the IC is connected in a bridge configuration. (See the schematic in the datasheet.) In that case you need a TDA2822 for the left channel and a second TDA2822 for the right channel. At 5 Volt you will have a little more output power. The symbols and notation such as "C1 - 1uF are the external components you need to operate this IC. VR1 and VR2 are the volume control potmeters. You will probably need one stereo potmeter for VR1 and VR2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jvdberg@ieee.org

    Hi, thanks for the speedy reply,

     

    I do have a spare potmeter which clicks to turn the device on and has 3 furthur terminals for the volume control, however how would the 3 terminals wire up to the schematic so that I could adjust the volume? Would 5v provide enough power to provide an reasonable volume through two 4 Ohm / 1.5w speakers? I am also wondering if the TDA2822 capable at running at 12v also because that is my second option...


    It looks something like this:

    http://upload.wikimedia.org/wikipedia/commons/b/b5/Potentiometer.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bad_boy_y
    bad_boy_y over 13 years ago in reply to e14 Contributor

    for connect your potmeter the arrow is always the center pin and the other can be switch.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bad_boy_y

    So the rectangle isn't actually a resistor as I guessed it was?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bad_boy_y

    So the rectangle isn't actually a resistor as I guessed it was?