element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum capacitors with motor drive L293D
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 33 subscribers
  • Views 2693 views
  • Users 0 members are here
  • capacitor
  • l293d
  • drive
  • with
  • motor
Related

capacitors with motor drive L293D

e14 Contributor
e14 Contributor over 12 years ago

image

I'm expecting to use this circuit for my robot. But I'm supplying two PWM signals to Enable pin 1 and 2. I wanna know if adding these capacitors will affect the pwm signal which is essential for controlling motor speed.

  • Sign in to reply
  • Cancel
Parents
  • saurocksall
    saurocksall over 12 years ago

    Hi Sameera,

     

    Can you specify exactly which capacitors are you talking about ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • saurocksall
    saurocksall over 12 years ago

    Hi Sameera,

     

    Can you specify exactly which capacitors are you talking about ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to saurocksall

    i'm referring to the 0.1uF capacitors. Can you tell me what kind of modifications i can do with this circuit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colecago
    colecago over 12 years ago in reply to e14 Contributor

    The 0.1's are on the motors, doesn't have anything to do with your PWM signals.  It will make the motors respond slightly differently with them though.

     

    I'd lose the caps on the motors, maybe add some flyback diodes in their place.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to colecago

    Sameera

    The 0.1 caps are to stop the electrical Hash that brushed motors generate.

    Because of the low resistance and the motors inductance, they won't affect the performance.

    Don't try to drive the PWM at too high a frequency as you'll turn the motor into an audio noise generator.

     

    Generally you solder the 0.1 from the motor connection to the metal body, or you can simply add a single one between the two motor connections (at the motor).

    Fullscreen contentimage_176298.html Download
    <html><head><title>Jive SBS</title></head>
    <body><font face="arial,helvetica,sans-serif">
    <b>Error</b><br><font size="-1">
    Un error general ha ocurrido durante el procesamiento de su solicitud.
    </font></font></body></html>
    

     

    I would increase the capacitor value on Pin 8 (from the battery) to 1000uF and add a 0.1uf across it as well.

     

     

    Colecago

    The L293D already has flyback diodes, but some of the others variants don't

    image

     

    cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to mcb1

    From the TI datasheet the L293D has diodes and the L293 does not -  so use the L293D image

     

    MK