element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Telephone Rotary Dial relay control
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 31 subscribers
  • Views 1810 views
  • Users 0 members are here
  • rotary
  • control
  • telephone
  • dial
  • relay
Related

Telephone Rotary Dial relay control

e14 Contributor
e14 Contributor over 12 years ago

Hey Ben,

 

I'm new here to Element14.com and just made an account.  I came here by watching your videos and thought that I would check it out.  I have a challange for you.  I was wondering if there is some way to make an old telephone rotary dial activate 10 different relays.  Let me explain:

 

If for instance I dial a 2 on the rotary dial, it will activate relay two, dial a three and activates relay three, and so on.  I would need this to pulse the respective relay (turn the relay on for about 250ms then shut it off)  I know this is a bit obscure, but there is a method to my madness lol image

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 12 years ago in reply to shabaz +1
    You could check out this one. https://www.sparkfun.com/tutorials/51 I think there was a kit at one stage Mark
  • mcb1
    mcb1 over 12 years ago in reply to shabaz +1
    That must have looked very "James Bond"! :-) more 'Get Smart' If you want to see a really big dial, check out this one. http://www.thecoralsnake.com/History22 This one is in NZ now (less the dial). Had…
  • mcb1
    mcb1 over 12 years ago in reply to shabaz +1
    All outputs will ripple through one-by-one, so that may be undesirable for some scenarios Simply inhibit the voltage that drives the relay until until after x and problem gone. When you want the 'relay…
Parents
  • shabaz
    shabaz over 12 years ago

    This type of thing could be implemented with logic gates, but perhaps a quick way is to obtain an Arduino and connect it to the contacts on the rear of the rotary dialer, and count pulses (which begin to occur after you release the dial at a position). Use interrupts, possibly. Also you'll need to do a debounce, which is explained on the arduino.cc pages.

    There is a nice video about three-quarters of the way down the wikipedia page on rotary dialers which shows the electrical connection.

    If you wanted the action to occur once you've reached a position, then there are some other methods but would require some sensor or potentiometer or other method of interfacing to the dial, i.e. some mechanical work.

    All this assumes the telephone is not connected to the phone network. If it is connected, then the pulses could be detected from the phone line but is likely prohibited in most countries.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    Wow, thanks for all your replies image

     

    I have some dials laying around because I restore these old telephones and wanted to make something cool with the remaining dials.  I have restored a few of them to factory standards.  I already understand how the dials work, lol.

    I was wanting to use one as "let's say" a keypad or something.  Making it to where it can toggle the respective relay for the number dialed makes this a universal device I can impliment into any project I need.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    I have restored a few of them to factory standards.

    Nice.

    If you had a device to count the pulses, then you would know what 'number' has been dialled.

    Then use that to control the appropriate relay.

    If you use a litle hardware, you can reduce the outputs required, and drive the relays at the same time.

     

    Interesting concept ... dial a number to rurn on a relay.

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    I have restored a few of them to factory standards.

    Nice.

    If you had a device to count the pulses, then you would know what 'number' has been dialled.

    Then use that to control the appropriate relay.

    If you use a litle hardware, you can reduce the outputs required, and drive the relays at the same time.

     

    Interesting concept ... dial a number to rurn on a relay.

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 12 years ago in reply to mcb1

    I remember the 4017 was quite a useful thing, It is a decade counter with individual outputs, and a reset input. So if the reset could be arranged somehow using one pair of contacts on the rotary dial, and some debouncer (think a 555 can be used for that) for the count input should work. All outputs will ripple through one-by-one, so that may be undesirable for some scenarios. To prevent that, it could be latched using a register perhaps.

    Alternatively an arduino (but less fun ; ).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to shabaz

    All outputs will ripple through one-by-one, so that may be undesirable for some scenarios

    Simply inhibit the voltage that drives the relay until until after x and problem gone.

    When you want the 'relay' to stop, then the same timer arrangement drops the power, and they are off.

     

    Sometimes hardware solutions are simple ... but they are fixed.

     

    I'm thinking that a Digispark could easily provide the timer/control parts, while the 4017 selsinork suggests does the decoding.

     

    Mark