element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Raspberry Pi laptop/netbook?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 30 subscribers
  • Views 1812 views
  • Users 0 members are here
  • help
  • pls
  • need
  • rpi
  • help!
  • laptop
  • heck
  • ben
  • i
Related

Raspberry Pi laptop/netbook?

e14 Contributor
e14 Contributor over 11 years ago

Hi, I am wondering about what parts to use when making a RPi portable laptop, so as I can program, wherever I am.

the most important things are:

  1. Battery life, type and size.
  2. Battery voltage (needs to equal 5v, doesn't it?)
  3. The case
  4. it stays on when you charge it
  5. display size, (I was thinking 10.7 inch or below)
  6. ventilation
  7. an on/off button (will be used to turn on or off the 'RaspBook Pi' and to reset it, in the event that it freezes)
  8. keyboard (I prefer the mac- style keyboards, the keys are nicely spaced and are heaven to type on)
  9. touchpad (if possible)
  10. (in the event that a touch pad is unavailable for RPi) a trackball?
  11. speakers (I can't stand tinny sounding ones)
  12. that the RPi is left alone- no desoldering, I want to keep all the connectors on it, i want the Ethernet and HDMI out, but won't be using the composite, as nothing I own uses it, plus its broken on my B)
  13. SD card access
  14. the case should be universal with the B and B+ models.
  15. possible access to GPIO headers
  16. IT MUST NOT BE HANDHELD!
  17. a 'battery low' indicator light, maybe?

these are the main things that I think I need for this project!

I will need help with what materials to use, I may have access to a CNC machine, but i'm not too sure. I don't have access to a 3D printer either.

 

I will use a phone charger (probably iPhone or android, depends on what's easier to solder)

If you choose to help,

Thanks so very much!

Yours sincerely,

     Owen 'weeowey' D.

  • Sign in to reply
  • Cancel
  • shanesissons
    shanesissons over 11 years ago

    I do like the idea of a pi netbook what about making it in such a way that

    it can be used as a netbook what about relocating all the headers you will

    need onto the back of the screen that way you can enclose the pi but still

    use all of its features what would be the purpose of the netbook for you i

    think thats what u nees to know before you design the housing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shanesissons

    I would like to use it for programming and maybe even drawing, thanks for replying!

    I'm thinking of putting a powered hub in there so I can plug in a dvd drive without burning out the Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    at the minute, i'm just about to turn on the pi and experiment with the ps3 keypad, I may be able to use that as a trackpad/keyboard combo.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    and yes, I thing relocating the headers to the rear of the case would be cool, but how about putting them on the inside? they will be a lot more protected from shorting if I did that, plus, I could label them,or maybe make a retractable wire so that it isn't just stuck to the case. or put it on the side and put a sliding dust cover on it (like the USB port on the samsung galaxy ace)

    look;

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    I guess I COULD make my own speakers, I found a way to make them sound really great and make them REALLY thin. they do have a problem that it makes a flapping noise if you put a bassy song through them, but they do sound great (amazing bass response).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    PS3 keypad works! you can hover your finger over it and it senses your finger, too so this is a great application, plus the clip that holds it on the controller is broken!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    I believe it has a Synaptics chip in there too!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shanesissons
    shanesissons over 11 years ago

    for the headers you can make them recessed and ad a cover like you said the sliding cover sounds good but you have got to think about where the cover is going to slide depending on how large the case is this would work great

     

    quoting your first post these are what ideas i have that i can help you with

     

    1. Battery life, type and size.

    https://www.adafruit.com/product/1566

    quick search brought this up

    1. The case

    the case can be hand made from wood or acrylic with ease along as the design is simple enough

    1. ventilation

    in the case design you can add a small 1inch/2-3cm fan

    1. keyboard (I prefer the mac- style keyboards, the keys are nicely spaced and are heaven to type on)

    could use a modified external mac keyboard i know you can get mac style ones on amazon for a few pound

    1. touchpad (if possible)

    same as above

    1. speakers (I can't stand tinny sounding ones)

    small speakers are easy to come by from laptops online

    1. that the RPi is left alone- no desoldering, I want to keep all the connectors on it, i want the Ethernet and HDMI out, but won't be using the composite, as nothing I own uses it, plus its broken on my B)

    i like the idea of not messing with what you already know works

    1. SD card access

    the pi can sit to the edge if the case for access to the sd card

    1. the case should be universal with the B and B+ models.

    aslong as the case is built to fit them both you shouldn't have any problems

    1. possible access to GPIO headers

    these can be relocated for ease of access

    1. IT MUST NOT BE HANDHELD!

    so im presuming you would like something that isn't to big or to small

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shanesissons

    thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>