element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 3D Printer support
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 31 subscribers
  • Views 1568 views
  • Users 0 members are here
  • printer
  • 3d
  • stepper-motor
  • ramps
  • arduino
  • extruder
Related

3D Printer support

anej
anej over 11 years ago

Hello.

So i am planning on making a 3D printer. I know that i can buy a kit and all that but i really want to build my own.

Here are some of the parts i would use:

- Extruder head: http://www.ebay.com/itm/Geeetech-MK8-extruder-J-head-Print-ABS-PLA-for-3D-Printer-Reprap-Mendel-/390993481130?pt=LH_DefaultDomain_15&var=&hash=item5b09070daa

- 4X Stepper motor (one for X, one for Y and two for Z): http://www.ebay.com/itm/1pcs-Nema17-Stepper-Motors-2-Phase-Motor-for-3D-Printer-Prusa-Mendel-Makerbot-/191081254280?pt=LH_DefaultDomain_0&hash=item2c7d548d88

- Heated bed: http://www.ebay.com/itm/1-RepRap-3D-Printer-PCB-Heatbed-MK2a-Heat-Bed-for-Prusa-Mendel-/171275126930?pt=LH_DefaultDomain_0&hash=item27e0cb0892

- Controller: http://www.ebay.com/itm/Mega2560-R3-RAMPS-1-4-REPRAP-3D-Printer-CONTROLLER-A4988-Stepper-Motor-Driver-/131057008442?pt=LH_DefaultDomain_0&hash=item1e839b3f3a

Ok. So now I don't know if that arduino + ramps is everything i need. Does arduino connect to the computer and the data is transfered through arduino or ?

Are there any additional parts that i would need ?

Here is the design of how i am planing making it (not quite finnished yet but you get the idea...): http://prntscr.com/68ep96

EDIT: Shoud i use a display too ?

  • Sign in to reply
  • Cancel

Top Replies

  • kingrahl
    kingrahl over 11 years ago +1
    You've got some of the major necessities down. Judging from your picture, you'll need the pulleys, belts, linear rods, threaded rods, and nuts for threaded rods. Not to mention all the hardware, nuts,…
  • kingrahl
    kingrahl over 11 years ago in reply to anej +1
    I use 1.75mm. It seems to be becoming a standard amongst printers. Some people have strong opinions for either. Just like size of filament, the type (ABS, PLA, other) each have there advantages and disadvantages…
  • kingrahl
    kingrahl over 11 years ago in reply to anej +1
    Yes. It's friction is higher than ABS or PLA so sliding through a PTFE tube will be harder. Also since it is "softer" it can smash and bend inside the tube creating a bind.
Parents
  • kingrahl
    kingrahl over 11 years ago

    You've got some of the major necessities down. Judging from your picture, you'll need the pulleys, belts, linear rods, threaded rods, and nuts for threaded rods. Not to mention all the hardware, nuts, bolts, washers, bearings, cut frame pieces, wires, 12v psu, and any parts you might need 3d printed. Make sure you decide which filament you'll be buying when you choose your extruder. You wouldn't want to buy a 1.75mm nozzle and 3mm filament.

     

    If you haven't worked with a 3d printer before, I'd recommend just buying a kit as your first. It is usually cheaper.

    Everything on your list is coming from China anyway... http://www.ebay.com/itm/Geeetech-official-Unassembled-Full-Acrylic-Frame-Prusa-Mendel-I3-Sanguinololu-/331420680085?pt=LH_DefaultDomain_0&var=&hash=item4d2a363f95

     

    You can also buy a "bundle" and put it in any frame you build... http://www.ebay.com/itm/Geeetech-RepRap-kit-RAMPS1-4-2560-A4988-hoted-bed-MK2A-Hotend-stepper-motor-LCD-/331358205919?pt=LH_DefaultDomain_0&hash=item4d267cf7df or http://www.amazon.com/SainSmart-Ultimaker-Mega2560-LCD2004-Controller/dp/B00GJD7L3Q/ref=sr_1_13?ie=UTF8&qid=1424671462&sr=8-13&keywords=ultimaker

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • anej
    anej over 11 years ago in reply to kingrahl

    Thanks for response.

    Like I said, I would like to build my own. And I also watched a bunch of tutorials and I think i am capable to build one mysel image

    Ok, so that power supply I have a bunc of them from old PC's just how much current does it need to supply to the printer ?... I think i can get all the hardware stuff at my local hardware store so i don't think that is a problem. Also what fillament would you recommend me ? what thicknes should I use? And for the type I think i would use ABS - that one is stronger am I right?

    So that design that I did, would it be OK if i would put the stepper motor that pushes the fillament somewhere else and put just the hot end on the "moving part"(X,Z axis)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kingrahl
    kingrahl over 11 years ago in reply to anej

    I use 1.75mm. It seems to be becoming a standard amongst printers. Some people have strong opinions for either. Just like size of filament, the type (ABS, PLA, other) each have there advantages and disadvantages. And again, everyone usually has strong opinions for either. The strength of each material only matters by what you plan on making.

     

    Almost all computer psu's will have enough current so you shouldn't have any problems there.

     

    Mounting the extruder somewhere other than to the hot end would be utilizing a Bowden tube. Again, people have strong opinions on either. It will be less weight on the x-axis allowing for faster movements thus faster printing. Some people don't like them because of OOZEBANE. This means your retraction settings will need to be higher. If you ever want to print in NinjaFlex, you won't be able to use the Bowden tube.                                                        

     

    There are plenty of opinions and discussions on all these topics. Just visit http://forums.reprap.org/, The design you are going for may have already been built so you may get a shopping list for the things that may have been overlooked. Go ahead and read as much as you can about everything. I don't recommend asking any "what should I use?" questions. Either you may be ignored because those questions have been asked many times, or an argument will ensue because of their strong opinions.

     

    I wish you luck on your build.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • anej
    anej over 11 years ago in reply to kingrahl

    Thank you much image It helped me a LOT image

    Oh and that NinjaFlex - i am guessing that that filament is more like rubber and it would kinda get "stuck" in the Bowden tube or am i wrong image ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • anej
    anej over 11 years ago in reply to kingrahl

    Thank you much image It helped me a LOT image

    Oh and that NinjaFlex - i am guessing that that filament is more like rubber and it would kinda get "stuck" in the Bowden tube or am i wrong image ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kingrahl
    kingrahl over 11 years ago in reply to anej

    Yes. It's friction is higher than ABS or PLA so sliding through a PTFE tube  will be harder. Also since it is "softer" it can smash and bend inside the tube creating a bind.